This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'd like to communicate SSD through SATA. Usual SSD has 22-pin SATA connector.
However, there is only 7-pin SATA Conncetor in an OMAP-L138 LCDK.
If I connect SSD and LCDK board with 7pin to 22pin SATA Cable, do I share a power from provided 5V 3A adapter or use external adapter? If not, am I have to use a SMPS to share the power both SSD and LCDK?
As shown in first image, there are three different power, 3.3 V, 5 V, and 12 V. If I use properly, am I have to connect all?
Finally, I found 7 pin to 22 pin SATA cable below.
Is it OK to Communicate?
Thank you. :)
Hi user4566427,
In your first picture, the Harddisk has Power and Data connection interface....right? . Connect the power interface to the SMPS and connect the data interface to the LCDK board thorugh SATA. The SMPS will get power of 230V.