This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X: RGMII and RMII PHY configuration

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3358

Hi

I would like to know if the CPSW configuration support two different PHY mode on the same CPSW ?

Our Hardware engineer connected the Atheros 8031 and SMSC LAN8710 to our Sitara processor.

/var/log/dmesg:[    1.220301] davinci_mdio 4a101000.mdio: phy[2]: device 4a101000.mdio:02, driver SMSC LAN8710/LAN8720
/var/log/dmesg:[    1.220315] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver Atheros 8031 ethernet

I am trying to configure the DTS in order to have both PHY working, one on ETH0 and one on ETH1 but I dont know how to proceed.

I have reused the cpsw_emac section of the am335x-evm-sk and the Atheros started to work, but for the SMSC LAN8710 I used the cpsw_emac section of the bone-common.dtsi and I dont see link on eth1

is there some one which can guide me about those two questions ?

1. Is this design can work ?

2. if Yes, how the cpsw_emac DTS section should look like ?

3. How the pin definition cpsw_default: should look like ?

4. Is the dual_emac mode has to be enabled ?

thanks in advance

  • Hi,

    From your log file excerpt it seems that both PHYs register correctly on the MDIO. There are several things to check:
    1. The RMII interface needs external 50MHz clock.
    2. Pinmux configuration.
    3. eth1 needs to be brought up manually.
    4. Dual EMAC mode has to be enabled depending on your intended use case.
  • Yes thank you.

    Just for confirmation, you're saying thRGMII and RMII on the same CPSW,

    Actually I have this in my DTS:

    &mac {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&cpsw_default>;
        pinctrl-1 = <&cpsw_sleep>;
        dual_emac = <0>;
        status = "okay";
    };
    
    &davinci_mdio {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&davinci_mdio_default>;
        pinctrl-1 = <&davinci_mdio_sleep>;
        status = "okay";
    };
    
    &cpsw_emac0 {
        phy_id = <&davinci_mdio>, <4>;
        phy-mode = "rgmii-txid";
        dual_emac_res_vlan = <1>;
    };
    
    &cpsw_emac1 {
        phy_id = <&davinci_mdio>, <2>;
        phy-mode = "rgmii-txid";
        dual_emac_res_vlan = <2>;
    };
    

    and somehow things started to work.

    root@linux:~# mii-tool -v eth1
    eth1: negotiated 1000baseT-HD flow-control, link ok
      product info: vendor 00:01:f0, model 15 rev 1
      basic mode:   autonegotiation enabled
      basic status: autonegotiation complete, link ok
      capabilities: 1000baseT-HD 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
      advertising:  1000baseT-HD 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD flow-control
      link partner: 1000baseT-HD 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD flow-control
    root@linux:~# mii-tool -v eth0
    eth0: negotiated 100baseTx-FD, link ok
      product info: vendor 00:13:74, model 7 rev 4
      basic mode:   autonegotiation enabled
      basic status: autonegotiation complete, link ok
      capabilities: 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
      advertising:  100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
      link partner: 1000baseT-FD 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD flow-control

    And pinmux conf remaint the same:

        cpsw_default: cpsw_default {
            pinctrl-single,pins = <
                /* Slave 1 */
                0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
                0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxdv.rgmii1_rctl */
                0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
                0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
                0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
                0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
                0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
                0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxclk.rgmii1_rclk */
                0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxd3.rgmii1_rd3 */
                0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxd2.rgmii1_rd2 */
                0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxd1.rgmii1_rd1 */
                0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2)  /* mii1_rxd0.rgmii1_rd0 */
    
                /* Slave 2 */
                0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a0.rgmii2_tctl */
                0x44 (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a1.rgmii2_rctl */
                0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a2.rgmii2_td3 */
                0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a3.rgmii2_td2 */
                0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a4.rgmii2_td1 */
                0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a5.rgmii2_td0 */
                0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)  /* gpmc_a6.rgmii2_tclk */
                0x5c (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a7.rgmii2_rclk */
                0x60 (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a8.rgmii2_rd3 */
                0x64 (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a9.rgmii2_rd2 */
                0x68 (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a10.rgmii2_rd1 */
                0x6c (PIN_INPUT_PULLDOWN | MUX_MODE2)   /* gpmc_a11.rgmii2_rd0 */
            >;

    is it making sense ???

  • Well, this shows both ports in RGMII mode.
  • Hi,

    I am still stuck with this issue. My setup is as following:

    On ETH0 of the AM3358 I have the Atheros AR8031 and it works properly with no packet LOSS - connected in mode RGMII
    On ETH1 of the AM3358 I have SMSC LAN8710 connected in MII mode - with PACKET LOSS.

    - Can CPSW can handle two PHY working in different mode ? RGMII and MII ?
    - Secondly, in the SITARA Pinmux, I dont see a MII for ETH1, for example:
    PIN GMPC_A0 permits this mode: [GPMC_A0/GMII2_TXEN/RGMII2_TCTL/RMII2_TXEN/GPMC_A16/PR1_MII_MT1_CLK/EHRPWM1_TRIPZONE_INPUT/GPIO1_16].
    This PIN is connected to TXEN of the PHY, so the unique MII moe I can see is MODE1 meaning GMII2_TXEN, is it a correct assumption ?
    - Third, only when the PINs of SMSC are configured RGMII both PHY are working, but with PACKET LOSS on the SMSC, when I configure the cpsw_emac1 in phy-mode = "mii" no one of them is working, in term of Linux OS things seems to be OK, but no traffic is outgoing netheir incoming.

    So I am trying to figure out what is wrong in my configuration, why I select MII mode for cpsw_emac1, and why RGMII work for it (partly, since I am seeing some packet loss).


    Below my DTS:

    cpsw_default: cpsw_default {
    pinctrl-single,pins = <
    //RGMII Atheros
    /* Slave 1 */
    0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
    0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
    0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
    0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
    0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
    0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
    0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
    0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
    0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
    0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
    0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
    0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */

    //MII MODE with SMSC LAN 8710
    /* Slave 2 */
    0x78 ( PIN_INPUT | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
    0x70 ( PIN_INPUT | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
    0x74 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */

    0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a0.rgmii2_tctl */
    0x44 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a1.rgmii2_rctl */
    0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a2.rgmii2_td3 */
    0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a3.rgmii2_td2 */
    0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a4.rgmii2_td1 */
    0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a5.rgmii2_td0 */
    0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE1) /* gpmc_a6.rgmii2_tclk */
    0x5c (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a7.rgmii2_rclk */
    0x60 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a8.rgmii2_rd3 */
    0x64 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a9.rgmii2_rd2 */
    0x68 (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a10.rgmii2_rd1 */
    0x6c (PIN_INPUT_PULLDOWN | MUX_MODE1) /* gpmc_a11.rgmii2_rd0 */
    >;
    };


    &mac {
    pinctrl-names = "default", "sleep";
    pinctrl-0 = <&cpsw_default>;
    pinctrl-1 = <&cpsw_sleep>;
    dual_emac = <0>;
    status = "okay";
    };

    &davinci_mdio {
    pinctrl-names = "default", "sleep";
    pinctrl-0 = <&davinci_mdio_default>;
    pinctrl-1 = <&davinci_mdio_sleep>;
    status = "okay";
    };

    &cpsw_emac0 {
    phy_id = <&davinci_mdio>, <4>;
    phy-mode = "rgmii-txid";
    dual_emac_res_vlan = <1>;
    };

    &cpsw_emac1 {
    phy_id = <&davinci_mdio>, <5>;
    phy-mode = "mii";
    dual_emac_res_vlan = <2>;
    };




    thanks
  • Part Number: PROCESSOR-SDK-AM335X

    Tool/software: Linux

    Hi,

    I need help to debug my issue.

    I have read dozen of threads on configuring RGMII and MII on U-boot and DTS in the TI forum, I have tried all of them, nothing is helping.

    My issue is as following:

    Our board is based EVMSK for everything except the ETH1 which is SMSC LAN8710 (used in the design of BBB).

    My DTS is as following:

    cpsw_default: cpsw_default {
            pinctrl-single,pins = <
                /* Slave 1 */
                0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txen.rgmii1_tctl */
                0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxdv.rgmii1_rctl */
                0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txd3.rgmii1_td3 */
                0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txd2.rgmii1_td2 */
                0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txd1.rgmii1_td1 */
                0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txd0.rgmii1_td0 */
                0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)    /* mii1_txclk.rgmii1_tclk */
                0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxclk.rgmii1_rclk */
                0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxd3.rgmii1_rd3 */
                0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxd2.rgmii1_rd2 */
                0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxd1.rgmii1_rd1 */
                0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2)    /* mii1_rxd0.rgmii1_rd0 */

                0x78 ( PIN_INPUT | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
                0x70 ( PIN_INPUT | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
                0x74 ( PIN_INPUT | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */

                /* Slave 2 */
                0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a0.gmii2_tctl */
                0x44 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a1.gmii2_rctl */
                0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a2.gmii2_td3 */
                0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a3.gmii2_td2 */
                0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a4.gmii2_td1 */
                0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a5.gmii2_td0 */
                0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a6.gmii2_tclk */
                0x5c (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a7.gmii2_rclk */
                0x60 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a8.gmii2_rd3 */
                0x64 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a9.gmii2_rd2 */
                0x68 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a10.gmii2_rd1 */
                0x6c (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a11.gmii2_rd0 */
            >;
        };

    &mac {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&cpsw_default>;
        pinctrl-1 = <&cpsw_sleep>;
        dual_emac = <0>;
        status = "okay";
    };

    &davinci_mdio {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&davinci_mdio_default>;
        pinctrl-1 = <&davinci_mdio_sleep>;
        status = "okay";
    };

    &cpsw_emac0 {
        phy_id = <&davinci_mdio>, <4>;
        phy-mode = "rgmii-txid";
      };

    &cpsw_emac1 {
        phy_id = <&davinci_mdio>, <5>; //  the PHY IS 0x02 in the design, but we changed the PHY ADDR to 0x5 during our test
        phy-mode = "mii";
      };

    The result is that I see LINK UP on  eth1 but no ping and no traffic is getting out neither received and suddenly the KERNEL reports a WARNING which also made ETH0 not working anymore.

    [  632.563942] device eth0 entered promiscuous mode
    [  632.612187] device eth0 left promiscuous mode
    [  640.634085] device eth1 entered promiscuous mode
    [  648.024063] ------------[ cut here ]------------
    [  648.024160] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:303 dev_watchdog+0x2a4/0x2c8()
    [  648.024185] NETDEV WATCHDOG: eth0 (cpsw): transmit queue 0 timed out
    [  648.024204] Modules linked in: bluetooth ipv6 omap_rng rng_core rtc_omap omap_wdt uio_pdrv_genirq uio vs88ut_fpga(O)
    [  648.024312] CPU: 0 PID: 0 Comm: swapper Tainted: G           O    4.1.19-kramer-bone20-tisdk_vs88ut-001 #30
    [  648.024333] Hardware name: Generic AM33XX (Flattened Device Tree)
    [  648.024351] Backtrace:
    [  648.024417] [<c0012af8>] (dump_backtrace) from [<c0012d18>] (show_stack+0x18/0x1c)
    [  648.024437]  r7:c08225ec r6:0000012f r5:00000009 r4:00000000
    [  648.024501] [<c0012d00>] (show_stack) from [<c063fd80>] (dump_stack+0x20/0x28)
    [  648.024553] [<c063fd60>] (dump_stack) from [<c0036704>] (warn_slowpath_common+0x7c/0xb4)
    [  648.024593] [<c0036688>] (warn_slowpath_common) from [<c0036774>] (warn_slowpath_fmt+0x38/0x40)
    [  648.024613]  r8:ffffffff r7:c08eb6eb r6:c08baad0 r5:00000000 r4:c08225b0
    [  648.024675] [<c0036740>] (warn_slowpath_fmt) from [<c058a934>] (dev_watchdog+0x2a4/0x2c8)
    [  648.024695]  r3:cd9bf800 r2:c08225b0
    [  648.024719]  r4:cd9bf800
    [  648.024769] [<c058a690>] (dev_watchdog) from [<c00766dc>] (call_timer_fn+0x2c/0xa4)
    [  648.024788]  r9:c08baad0 r8:00200200 r7:00000000 r6:c08ade38 r5:c058a690 r4:00000101
    [  648.024858] [<c00766b0>] (call_timer_fn) from [<c0076b68>] (run_timer_softirq+0x234/0x2d4)
    [  648.024877]  r6:c08ade38 r5:c0900b40 r4:cd9bfa38
    [  648.024935] [<c0076934>] (run_timer_softirq) from [<c0039668>] (__do_softirq+0xec/0x218)
    [  648.024953]  r10:00000101 r9:40000001 r8:c08eed80 r7:c08ac000 r6:c08eed84 r5:00000001
    [  648.024999]  r4:00000000
    [  648.025038] [<c003957c>] (__do_softirq) from [<c0039a3c>] (irq_exit+0xa8/0x100)
    [  648.025057]  r10:00000001 r9:c08ae110 r8:cd806000 r7:00000001 r6:00000000 r5:c08c4954
    [  648.025102]  r4:00000000
    [  648.025149] [<c0039994>] (irq_exit) from [<c0068874>] (__handle_domain_irq+0x58/0xb0)
    [  648.025167]  r5:c08c4954 r4:00000000
    [  648.025210] [<c006881c>] (__handle_domain_irq) from [<c0009470>] (omap_intc_handle_irq+0xbc/0xcc)
    [  648.025228]  r9:c08ae110 r8:00000000 r7:00000044 r6:c08adf20 r5:c0916940 r4:c08c4bc0
    [  648.025300] [<c00093b4>] (omap_intc_handle_irq) from [<c0645240>] (__irq_svc+0x40/0x74)
    [  648.025323] Exception stack(0xc08adf20 to 0xc08adf68)
    [  648.025358] df20: 00000001 00000000 00000000 c001ffa0 c08ac000 c08ae110 00000000 00000000
    [  648.025392] df40: 00000000 c08ae110 00000001 c08adf74 c08adf78 c08adf68 c00101fc c0010200
    [  648.025414] df60: 60000013 ffffffff
    [  648.025430]  r7:c08adf54 r6:ffffffff r5:60000013 r4:c0010200
    [  648.025504] [<c00101c8>] (arch_cpu_idle) from [<c00603a0>] (cpu_startup_entry+0x194/0x214)
    [  648.025542] [<c006020c>] (cpu_startup_entry) from [<c063cbe4>] (rest_init+0x78/0x90)
    [  648.025560]  r7:c08ae000
    [  648.025611] [<c063cb6c>] (rest_init) from [<c0868c8c>] (start_kernel+0x354/0x3c4)
    [  648.025629]  r5:c08ee000 r4:c08ee050
    [  648.025675] [<c0868938>] (start_kernel) from [<80008078>] (0x80008078)
    [  648.025697] ---[ end trace c818a663baccaf67 ]---
    [  677.197982] device eth1 left promiscuous mode

    So, I need guidance to debug and how to check the validity of the PHY, it can be in u-boot or Linux, I have debugged the PHY register in both of them the issue remain the same.

    I almost sure the issue is somewhere in the hardware design, but I need your help to find the root cause.

    BTW, Strangely, when I declare "rgmii" for the ETH1, things starts to work but some packets are dropped..... very strange, the PHY is physically configured and connected using MII.....I am lost !

    Any direction, advice is welcome ,

    thank you very much in advance.

  • Reviewing the latest DTS file and pin mux it appears that everything is setup correctly. I will need to discuss with a HW apps team member about the schematic setup.

    Could you please post your current Linux boot log as an attachment?
    After a reboot do not use eth0, run a few ping commands and then please capture the following ethtool commands and post as an attachment:
    - ethtool eth1
    - ethtool -S eth1
    Which Linux SDK are you using?

    The kernel Warn you are seeing appears to be that eth1 is not able to send packets. Most likely the issue that eth0 is ceasing to function is that all the TX descriptors are blocked on eth1 waiting to be sent. Something looks to be blocking the packets from leaving the mac.

    Monday is a holiday here so please be aware a response may not come until at least tuesday.
  • We are using Ubuntu for ARM, and Kernel release 4.1.19-bone20 and also u-boot from the source of RobertNelson  for BBB.

    Below attached what you ask for, boot log + ethtool output + dmesg:

    Checking for: mmc 1:1 /uEnv.txt ...
    Checking for: /boot.scr ...
    Checking for: /boot/boot.scr ...
    Checking for: /boot/uEnv.txt ...
    918 bytes read in 34 ms (26.4 KiB/s)
    Loaded environment from mmc 1:1 /boot/uEnv.txt
    Checking if uname_r is set in /boot/uEnv.txt...
    Running uname_boot ...
    loading /boot/vmlinuz-4.1.19--bone20-tisdk_ ...
    3305464 bytes read in 229 ms (13.8 MiB/s)
    loading /boot/dtbs/4.1.19--bone20-tisdk_/am335x-evmsk.dtb ...
    58189 bytes read in 84 ms (675.8 KiB/s)
    debug: [console=ttyO0,115200n8 ksupport root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait oops=panic panic=-1] ...
    debug: [bootz 0x82000000 - 0x88000000] ...
    Kernel image @ 0x82000000 [ 0x000000 - 0x326ff8 ]
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Using Device Tree in place at 88000000, end 8801134c
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.1.19--bone20-tisdk_-001 (sweiss@ubuntu-obelix) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #30 PREEMPT Thu Feb 16 16:10:40 IST 2017
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine model:  AM335x VS-88UT 3.59t
    [    0.000000] cma: Reserved 24 MiB at 0x8e800000
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] AM335X ES2.1 (sgx neon )
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 64960
    [    0.000000] Kernel command line: console=ttyO0,115200n8 ksupport root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait oops=panic panic=-1
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 225364K/262144K available (6403K kernel code, 255K rwdata, 2168K rodata, 272K init, 233K bss, 12204K reserved, 24576K cma-reserved, 0K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc08670ac   (8573 kB)
    [    0.000000]       .init : 0xc0868000 - 0xc08ac000   ( 272 kB)
    [    0.000000]       .data : 0xc08ac000 - 0xc08ebd68   ( 256 kB)
    [    0.000000]        .bss : 0xc08ee000 - 0xc0928778   ( 234 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Additional per-CPU info printed with stalls.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [    0.000018] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
    [    0.000040] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
    [    0.000052] OMAP clocksource: timer1 at 24000000 Hz
    [    0.000243] Console: colour dummy device 80x30
    [    0.000271] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.000277] This ensures that you still see kernel messages. Please
    [    0.000283] update your kernel commandline.
    [    0.000302] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
    [    0.089087] pid_max: default: 32768 minimum: 301
    [    0.089191] Security Framework initialized
    [    0.089245] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.089256] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.089967] Initializing cgroup subsys blkio
    [    0.089994] Initializing cgroup subsys memory
    [    0.090040] Initializing cgroup subsys devices
    [    0.090057] Initializing cgroup subsys freezer
    [    0.090072] Initializing cgroup subsys perf_event
    [    0.090101] CPU: Testing write buffer coherency: ok
    [    0.090519] Setting up static identity map for 0x80008200 - 0x80008270
    [    0.092401] devtmpfs: initialized
    [    0.108527] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    0.120905] omap_hwmod: tptc0 using broken dt data from edma
    [    0.121059] omap_hwmod: tptc1 using broken dt data from edma
    [    0.121185] omap_hwmod: tptc2 using broken dt data from edma
    [    0.126004] omap_hwmod: debugss: _wait_target_disable failed
    [    0.181062] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.183482] pinctrl core: initialized pinctrl subsystem
    [    0.184845] NET: Registered protocol family 16
    [    0.187177] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.209080] cpuidle: using governor ladder
    [    0.239068] cpuidle: using governor menu
    [    0.241969] omap_gpio 44e07000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio0_cpld_cs_pins_default, deferring probe
    [    0.242282] omap_gpio 4804c000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_wl12xx_gpio, deferring probe
    [    0.242570] omap_gpio 481ac000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio2_jtag_pins_default, deferring probe
    [    0.242841] omap_gpio 481ae000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio3_fpga_rst_pins, deferring probe
    [    0.250758] No ATAGs?
    [    0.250793] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.288029] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
    [    0.291934] vgaarb: loaded
    [    0.292498] SCSI subsystem initialized
    [    0.293024] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
    [    0.293081] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c2_pins_default, deferring probe
    [    0.293209] media: Linux media interface: v0.10
    [    0.293281] Linux video capture interface: v2.00
    [    0.293333] pps_core: LinuxPPS API ver. 1 registered
    [    0.293341] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.293373] PTP clock support registered
    [    0.294091] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [    0.294387] Advanced Linux Sound Architecture Driver Initialized.
    [    0.295322] Switched to clocksource timer1
    [    0.306531] NET: Registered protocol family 2
    [    0.307423] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.307458] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.307487] TCP: Hash tables configured (established 2048 bind 2048)
    [    0.307571] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.307590] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.307762] NET: Registered protocol family 1
    [    0.308172] RPC: Registered named UNIX socket transport module.
    [    0.308188] RPC: Registered udp transport module.
    [    0.308194] RPC: Registered tcp transport module.
    [    0.308201] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.309161] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
    [    0.309209] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
    [    0.311128] futex hash table entries: 256 (order: -1, 3072 bytes)
    [    0.311221] audit: initializing netlink subsys (disabled)
    [    0.311289] audit: type=2000 audit(0.290:1): initialized
    [    0.319239] VFS: Disk quotas dquot_6.6.0
    [    0.319461] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.321711] NFS: Registering the id_resolver key type
    [    0.321787] Key type id_resolver registered
    [    0.321796] Key type id_legacy registered
    [    0.321867] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    [    0.324547] NET: Registered protocol family 38
    [    0.324621] io scheduler noop registered
    [    0.324636] io scheduler deadline registered
    [    0.324696] io scheduler cfq registered (default)
    [    0.325935] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
    [    0.328233] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.331936] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 26, base_baud = 3000000) is a 8250
    [    1.034054] console [ttyS0] enabled
    [    1.038498] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 27, base_baud = 3000000) is a 8250
    [    1.048258] [drm] Initialized drm 1.1.0 20060810
    [    1.064055] brd: module loaded
    [    1.072458] loop: module loaded
    [    1.076841] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    1.088910] mousedev: PS/2 mouse device common for all mice
    [    1.094628] i2c /dev entries driver
    [    1.100035] omap_hsmmc 481d8000.mmc: unable to get vmmc regulator -517
    [    1.106992] ledtrig-cpu: registered to indicate activity on CPUs
    [    1.113320] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
    [    1.120383] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
    [    1.126370] omap-sham 53100000.sham: initialization failed.
    [    1.132014] omap-sham: probe of 53100000.sham failed with error -22
    [    1.140477] oprofile: using arm/armv7
    [    1.144534] Initializing XFRM netlink socket
    [    1.149087] NET: Registered protocol family 17
    [    1.153601] NET: Registered protocol family 15
    [    1.158272] Key type dns_resolver registered
    [    1.162861] omap_voltage_late_init: Voltage driver support not added
    [    1.169688] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
    [    1.178523] cpu cpu0: cpu0 clock notifier not ready, retry
    [    1.184248] ThumbEE CPU extension supported.
    [    1.188621] Registering SWP/SWPB emulation handler
    [    1.196451] OMAP GPIO hardware version 0.1
    [    1.204260] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
    [    1.225523] tps65910 0-002d: No interrupt support, no core IRQ
    [    1.254964] tps65910-rtc tps65910-rtc: IRQ is not free.
    [    1.260294] tps65910-rtc: probe of tps65910-rtc failed with error -22
    [    1.267022] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
    [    1.273901] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 400 kHz
    [    1.280289] omap_hsmmc 48060000.mmc: Got CD GPIO
    [    1.285381] vmmc: supplied by vbat
    [    1.326716] vmmc: Restricting voltage, 3300000-1950000uV
    [    1.332065] omap_hsmmc 481d8000.mmc: could not set regulator OCR (-22)
    [    1.375672] vdd_mpu: supplied by vbat
    [    1.379540] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1260000]:-22
    [    1.389788] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1260000]:-22
    [    1.449302] mmc1: MAN_BKOPS_EN bit is not set
    [    1.457406] mmc1: new high speed MMC card at address 0001
    [    1.463389] mmcblk0: mmc1:0001 MMC04G 3.60 GiB
    [    1.468025] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
    [    1.474149] davinci_mdio 4a101000.mdio: detected phy mask c780ffcf
    [    1.480575] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
    [    1.487034] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
    [    1.501600] libphy: 4a101000.mdio: probed
    [    1.505874]  mmcblk0: p1 p2 p3 p4 < p5 p6 p7 >
    [    1.510610] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver Atheros 8031 ethernet
    [    1.522844] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver SMSC LAN8710/LAN8720
    [    1.532141] davinci_mdio 4a101000.mdio: phy[16]: device 4a101000.mdio:10, driver unknown
    [    1.540323] davinci_mdio 4a101000.mdio: phy[17]: device 4a101000.mdio:11, driver unknown
    [    1.548522] davinci_mdio 4a101000.mdio: phy[18]: device 4a101000.mdio:12, driver unknown
    [    1.556676] davinci_mdio 4a101000.mdio: phy[19]: device 4a101000.mdio:13, driver unknown
    [    1.564803] davinci_mdio 4a101000.mdio: phy[20]: device 4a101000.mdio:14, driver unknown
    [    1.572946] davinci_mdio 4a101000.mdio: phy[21]: device 4a101000.mdio:15, driver unknown
    [    1.581088] davinci_mdio 4a101000.mdio: phy[22]: device 4a101000.mdio:16, driver unknown
    [    1.589229] davinci_mdio 4a101000.mdio: phy[27]: device 4a101000.mdio:1b, driver unknown
    [    1.597371] davinci_mdio 4a101000.mdio: phy[29]: device 4a101000.mdio:1d, driver unknown
    [    1.606429] cpsw 4a100000.ethernet: Detected MACID = ec:24:b8:d1:58:6d
    [    1.613967] cpsw 4a100000.ethernet: cpsw: Detected MACID = ec:24:b8:d1:58:6f
    [    1.622039] hctosys: unable to open rtc device (rtc0)
    [    1.627188] of_cfs_init
    [    1.629745] of_cfs_init: OK
    [    1.636898] lis3_reg: disabling
    [    1.640186] ALSA device list:
    [    1.643164]   No soundcards found.
    [    1.652536] EXT4-fs (mmcblk0p1): INFO: recovery required on readonly filesystem
    [    1.660099] EXT4-fs (mmcblk0p1): write access will be enabled during recovery
    [    2.699753] EXT4-fs (mmcblk0p1): recovery complete
    [    2.709060] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
    [    2.717407] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.
    [    2.725660] devtmpfs: mounted
    [    2.729587] Freeing unused kernel memory: 272K (c0868000 - c08ac000)
    Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory
    [    3.289234] random: init urandom read with 31 bits of entropy available
    [    3.666285] init: plymouth-upstart-bridge main process (83) terminated with status 1
    [    3.699028] init: plymouth-upstart-bridge main process ended, respawning
    [    3.838838] init: ureadahead main process (86) terminated with status 5
    [    3.859106] init: plymouth-upstart-bridge main process (94) terminated with status 1
    [    3.871591] init: plymouth-upstart-bridge main process ended, respawning
    [    4.330494] init: mounted-proc main process (110) terminated with status 1
     * Starting Mount filesystems on boot                                    [ OK ]
     * Stopping Send an event to indicate plymouth is up                     [ OK ]
     * Starting Populate and link to /run filesystem                         [ OK ]
     * Stopping Populate and link to /run filesystem                         [ OK ]
     * Stopping Track if upstart is running in a container                   [ OK ]
     * Starting Initialize or finalize resolvconf                            [ OK ]
     * Starting set console keymap                                           [ OK ]
     * Starting Signal sysvinit that virtual filesystems are mounted         [ OK ]
     * Starting Signal sysvinit that virtual filesystems are mounted         [ OK ]
     * Starting Bridge udev events into upstart                              [ OK ]
     * Stopping set console keymap                                           [ OK ]
     * Starting Signal sysvinit that remote filesystems are mounted          [ OK ]
     * Starting device node and kernel event manager                         [ OK ]
     * Starting load modules from /etc/modules                               [ OK ]
     * Starting cold plug devices                                            [ OK ]
     * Starting log initial device creation                                  [ OK ]
     * Stopping load modules from /etc/modules                               [ OK ]
     * Stopping cold plug devices                                            [ OK ]
     * Starting Signal sysvinit that the rootfs is mounted                   [ OK ]
     * Stopping log initial device creation                                  [ OK ]
     * Starting configure network device security                            [ OK ]
     * Starting configure network device security                            [ OK ]
     * Starting set console font                                             [ OK ]
     * Starting configure network device                                     [ OK ]
     * Stopping set console font                                             [ OK ]
     * Starting userspace bootsplash                                         [ OK ]
     * Stopping userspace bootsplash                                         [ OK ]
     * Starting Send an event to indicate plymouth is up                     [ OK ]
     * Stopping Send an event to indicate plymouth is up                     [ OK ]
     * Starting Clean /tmp directory                                         [ OK ]
     * Starting configure network device security                            [ OK ]
     * Stopping Clean /tmp directory                                         [ OK ]
     * Starting configure network device                                     [ OK ]
     * Starting Mount network filesystems                                    [ OK ]
     * Stopping Read required files in advance (for other mountpoints)       [ OK ]
     * Stopping Mount network filesystems                                    [ OK ]
     * Starting Signal sysvinit that local filesystems are mounted           [ OK ]
     * Starting configure network device security                            [ OK ]
     * Stopping Mount filesystems on boot                                    [ OK ]
     * Starting D-Bus system message bus                                     [ OK ]
     * Starting flush early job output to logs                               [ OK ]
     * Starting System V initialisation compatibility                        [ OK ]
     * Starting configure network device                                     [ OK ]
     * Stopping flush early job output to logs                               [ OK ]
     * Starting NetBIOS name server                                          [ OK ]
     * Stopping System V initialisation compatibility                        [ OK ]
     * Starting system logging daemon                                        [ OK ]
     * Starting configure virtual network devices                            [ OK ]
     * Starting System V runlevel compatibility                              [ OK ]
     * Starting deferred execution scheduler                                 [ OK ]
     * Starting regular background program processing daemon                 [ OK ]
     * Starting ACPI daemon                                                  [ OK ]
     * Starting save kernel messages                                         [ OK ]
     * Stopping save kernel messages                                         [ OK ]
     * Loading cpufreq kernel modules...                                     [ OK ]
     * Starting OpenSSH server                                               [ OK ]
     * Starting mDNS/DNS-SD daemon                                           [ OK ]
     * CPU0...                                                               [ OK ]  * Starting Reload cups, upon starting avahi-daemon to make sure remote queues are populated
     * CPUFreq Utilities: Setting ondemand CPUFreq governor...        * Start[fail]load cups, upon starting avahi-daemon to make sure remote queues are populated
                                                                             [ OK ]
    udhcpd: Disabled. Edit /etc/default/udhcpd to enable it.
     * Starting NTP server ntpd                                              [ OK ]
     * Starting Bridge file events into upstart                              [ OK ]
    Starting  Tech Support Mode
    serial start/running, process 781
     * Stopping System V runlevel compatibility                              [ OK ]
    
      ttyS0
    Ubuntu 14.04.3 LTS
     login: root
    Password:
    Last login: Mon Sep  7 21:40:37 UTC 2015 on ttyS0
    Welcome to  Electronics LTD
    root@:~# ifconfig
    eth1      Link encap:Ethernet  HWaddr ec:24:b8:d1:58:6f
              inet addr:203.0.113.50  Bcast:203.0.113.255  Mask:255.255.255.0
              inet6 addr: fe80::ee24:b8ff:fed1:586f/64 Scope:Link
              UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
              RX packets:320 errors:0 dropped:0 overruns:0 frame:0
              TX packets:50 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000
              RX bytes:39057 (39.0 KB)  TX bytes:6535 (6.5 KB)
    
    lo        Link encap:Local Loopback
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:65536  Metric:1
              RX packets:0 errors:0 dropped:0 overruns:0 frame:0
              TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:0
              RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
    
    root@:~# ping 203.0.113.52
    PING 203.0.113.52 (203.0.113.52) 56(84) bytes of data.
    ^C
    --- 203.0.113.52 ping statistics ---
    3 packets transmitted, 0 received, 100% packet loss, time 1999ms
    
    root@:~# ethtool eth1
    Settings for eth1:
            Supported ports: [ TP MII ]
            Supported link modes:   10baseT/Half 10baseT/Full
                                    100baseT/Half 100baseT/Full
            Supported pause frame use: Symmetric Receive-only
            Supports auto-negotiation: Yes
            Advertised link modes:  10baseT/Half 10baseT/Full
                                    100baseT/Half 100baseT/Full
            Advertised pause frame use: Symmetric Receive-only
            Advertised auto-negotiation: Yes
            Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                                 100baseT/Half 100baseT/Full
            Link partner advertised pause frame use: Symmetric
            Link partner advertised auto-negotiation: Yes
            Speed: 100Mb/s
            Duplex: Full
            Port: MII
            PHYAD: 5
            Transceiver: external
            Auto-negotiation: on
            Supports Wake-on: d
            Wake-on: d
            Current message level: 0x00000000 (0)
    
            Link detected: yes
    root@:~# ethtool -S eth1
    NIC statistics:
         Good Rx Frames: 1391
         Broadcast Rx Frames: 391
         Multicast Rx Frames: 994
         Pause Rx Frames: 0
         Rx CRC Errors: 0
         Rx Align/Code Errors: 0
         Oversize Rx Frames: 0
         Rx Jabbers: 0
         Undersize (Short) Rx Frames: 0
         Rx Fragments: 0
         Rx Octets: 262196
         Good Tx Frames: 0
         Broadcast Tx Frames: 0
         Multicast Tx Frames: 0
         Pause Tx Frames: 0
         Deferred Tx Frames: 0
         Collisions: 0
         Single Collision Tx Frames: 0
         Multiple Collision Tx Frames: 0
         Excessive Collisions: 0
         Late Collisions: 0
         Tx Underrun: 0
         Carrier Sense Errors: 0
         Tx Octets: 0
         Rx + Tx 64 Octet Frames: 272
         Rx + Tx 65-127 Octet Frames: 320
         Rx + Tx 128-255 Octet Frames: 589
         Rx + Tx 256-511 Octet Frames: 197
         Rx + Tx 512-1023 Octet Frames: 11
         Rx + Tx 1024-Up Octet Frames: 2
         Net Octets: 262196
         Rx Start of Frame Overruns: 0
         Rx Middle of Frame Overruns: 0
         Rx DMA Overruns: 0
         Rx DMA chan: head_enqueue: 1
         Rx DMA chan: tail_enqueue: 454
         Rx DMA chan: pad_enqueue: 0
         Rx DMA chan: misqueued: 0
         Rx DMA chan: desc_alloc_fail: 0
         Rx DMA chan: pad_alloc_fail: 0
         Rx DMA chan: runt_receive_buf: 0
         Rx DMA chan: runt_transmit_buf: 0
         Rx DMA chan: empty_dequeue: 0
         Rx DMA chan: busy_dequeue: 766
         Rx DMA chan: good_dequeue: 391
         Rx DMA chan: requeue: 0
         Rx DMA chan: teardown_dequeue: 0
         Tx DMA chan: head_enqueue: 53
         Tx DMA chan: tail_enqueue: 0
         Tx DMA chan: pad_enqueue: 0
         Tx DMA chan: misqueued: 0
         Tx DMA chan: desc_alloc_fail: 0
         Tx DMA chan: pad_alloc_fail: 0
         Tx DMA chan: runt_receive_buf: 0
         Tx DMA chan: runt_transmit_buf: 3
         Tx DMA chan: empty_dequeue: 978
         Tx DMA chan: busy_dequeue: 0
         Tx DMA chan: good_dequeue: 53
         Tx DMA chan: requeue: 53
         Tx DMA chan: teardown_dequeue: 0
    root@:~# ethtool -S eth1
    NIC statistics:
         Good Rx Frames: 1700
         Broadcast Rx Frames: 468
         Multicast Rx Frames: 1224
         Pause Rx Frames: 0
         Rx CRC Errors: 0
         Rx Align/Code Errors: 0
         Oversize Rx Frames: 0
         Rx Jabbers: 0
         Undersize (Short) Rx Frames: 0
         Rx Fragments: 0
         Rx Octets: 319797
         Good Tx Frames: 0
         Broadcast Tx Frames: 0
         Multicast Tx Frames: 0
         Pause Tx Frames: 0
         Deferred Tx Frames: 0
         Collisions: 0
         Single Collision Tx Frames: 0
         Multiple Collision Tx Frames: 0
         Excessive Collisions: 0
         Late Collisions: 0
         Tx Underrun: 0
         Carrier Sense Errors: 0
         Tx Octets: 0
         Rx + Tx 64 Octet Frames: 329
         Rx + Tx 65-127 Octet Frames: 402
         Rx + Tx 128-255 Octet Frames: 714
         Rx + Tx 256-511 Octet Frames: 239
         Rx + Tx 512-1023 Octet Frames: 13
         Rx + Tx 1024-Up Octet Frames: 3
         Net Octets: 319797
         Rx Start of Frame Overruns: 0
         Rx Middle of Frame Overruns: 0
         Rx DMA Overruns: 0
         Rx DMA chan: head_enqueue: 1
         Rx DMA chan: tail_enqueue: 531
         Rx DMA chan: pad_enqueue: 0
         Rx DMA chan: misqueued: 0
         Rx DMA chan: desc_alloc_fail: 0
         Rx DMA chan: pad_alloc_fail: 0
         Rx DMA chan: runt_receive_buf: 0
         Rx DMA chan: runt_transmit_buf: 0
         Rx DMA chan: empty_dequeue: 0
         Rx DMA chan: busy_dequeue: 917
         Rx DMA chan: good_dequeue: 468
         Rx DMA chan: requeue: 0
         Rx DMA chan: teardown_dequeue: 0
         Tx DMA chan: head_enqueue: 53
         Tx DMA chan: tail_enqueue: 0
         Tx DMA chan: pad_enqueue: 0
         Tx DMA chan: misqueued: 0
         Tx DMA chan: desc_alloc_fail: 0
         Tx DMA chan: pad_alloc_fail: 0
         Tx DMA chan: runt_receive_buf: 0
         Tx DMA chan: runt_transmit_buf: 3
         Tx DMA chan: empty_dequeue: 1129
         Tx DMA chan: busy_dequeue: 0
         Tx DMA chan: good_dequeue: 53
         Tx DMA chan: requeue: 53
         Tx DMA chan: teardown_dequeue: 0
    root@:~# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.1.19--bone20-tisdk_-001 (sweiss@ubuntu-obelix) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #30 PREEMPT Thu Feb 16 16:10:40 IST 2017
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine model:  AM335x VS-88UT 3.59t
    [    0.000000] cma: Reserved 24 MiB at 0x8e800000
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] On node 0 totalpages: 65536
    [    0.000000] free_area_init_node: node 0, pgdat c08e9ca0, node_mem_map ce5ad000
    [    0.000000]   Normal zone: 576 pages used for memmap
    [    0.000000]   Normal zone: 0 pages reserved
    [    0.000000]   Normal zone: 65536 pages, LIFO batch:15
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] AM335X ES2.1 (sgx neon )
    [    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
    [    0.000000] pcpu-alloc: [0] 0
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 64960
    [    0.000000] Kernel command line: console=ttyO0,115200n8 ksupport root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait oops=panic panic=-1
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 225364K/262144K available (6403K kernel code, 255K rwdata, 2168K rodata, 272K init, 233K bss, 12204K reserved, 24576K cma-reserved, 0K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc08670ac   (8573 kB)
    [    0.000000]       .init : 0xc0868000 - 0xc08ac000   ( 272 kB)
    [    0.000000]       .data : 0xc08ac000 - 0xc08ebd68   ( 256 kB)
    [    0.000000]        .bss : 0xc08ee000 - 0xc0928778   ( 234 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Additional per-CPU info printed with stalls.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [    0.000018] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
    [    0.000040] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
    [    0.000052] OMAP clocksource: timer1 at 24000000 Hz
    [    0.000243] Console: colour dummy device 80x30
    [    0.000271] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.000277] This ensures that you still see kernel messages. Please
    [    0.000283] update your kernel commandline.
    [    0.000302] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
    [    0.089087] pid_max: default: 32768 minimum: 301
    [    0.089191] Security Framework initialized
    [    0.089245] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.089256] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.089967] Initializing cgroup subsys blkio
    [    0.089994] Initializing cgroup subsys memory
    [    0.090040] Initializing cgroup subsys devices
    [    0.090057] Initializing cgroup subsys freezer
    [    0.090072] Initializing cgroup subsys perf_event
    [    0.090101] CPU: Testing write buffer coherency: ok
    [    0.090519] Setting up static identity map for 0x80008200 - 0x80008270
    [    0.092401] devtmpfs: initialized
    [    0.108527] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    0.120905] omap_hwmod: tptc0 using broken dt data from edma
    [    0.121059] omap_hwmod: tptc1 using broken dt data from edma
    [    0.121185] omap_hwmod: tptc2 using broken dt data from edma
    [    0.126004] omap_hwmod: debugss: _wait_target_disable failed
    [    0.181062] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.183482] pinctrl core: initialized pinctrl subsystem
    [    0.184845] NET: Registered protocol family 16
    [    0.187177] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.209080] cpuidle: using governor ladder
    [    0.239068] cpuidle: using governor menu
    [    0.241969] omap_gpio 44e07000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio0_cpld_cs_pins_default, deferring probe
    [    0.242282] omap_gpio 4804c000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_wl12xx_gpio, deferring probe
    [    0.242570] omap_gpio 481ac000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio2_jtag_pins_default, deferring probe
    [    0.242841] omap_gpio 481ae000.gpio: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/gpio3_fpga_rst_pins, deferring probe
    [    0.250758] No ATAGs?
    [    0.250793] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.288029] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
    [    0.288540] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@0[0]'
    [    0.288865] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@1[0]'
    [    0.289362] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator@3[0]' - status (-517)
    [    0.291934] vgaarb: loaded
    [    0.292498] SCSI subsystem initialized
    [    0.293024] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
    [    0.293081] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c2_pins_default, deferring probe
    [    0.293209] media: Linux media interface: v0.10
    [    0.293281] Linux video capture interface: v2.00
    [    0.293333] pps_core: LinuxPPS API ver. 1 registered
    [    0.293341] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.293373] PTP clock support registered
    [    0.294091] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [    0.294387] Advanced Linux Sound Architecture Driver Initialized.
    [    0.295322] Switched to clocksource timer1
    [    0.306531] NET: Registered protocol family 2
    [    0.307423] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.307458] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.307487] TCP: Hash tables configured (established 2048 bind 2048)
    [    0.307571] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.307590] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.307762] NET: Registered protocol family 1
    [    0.308172] RPC: Registered named UNIX socket transport module.
    [    0.308188] RPC: Registered udp transport module.
    [    0.308194] RPC: Registered tcp transport module.
    [    0.308201] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.308241] PCI: CLS 0 bytes, default 64
    [    0.309161] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
    [    0.309209] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
    [    0.311128] futex hash table entries: 256 (order: -1, 3072 bytes)
    [    0.311221] audit: initializing netlink subsys (disabled)
    [    0.311289] audit: type=2000 audit(0.290:1): initialized
    [    0.319239] VFS: Disk quotas dquot_6.6.0
    [    0.319461] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.321711] NFS: Registering the id_resolver key type
    [    0.321787] Key type id_resolver registered
    [    0.321796] Key type id_legacy registered
    [    0.321867] jffs2: version 2.2. (NAND) (SUMMARY)  \xffffffc2\xffffffa9\xffffffa9 2001-2006 Red Hat, Inc.
    [    0.324547] NET: Registered protocol family 38
    [    0.324621] io scheduler noop registered
    [    0.324636] io scheduler deadline registered
    [    0.324696] io scheduler cfq registered (default)
    [    0.325935] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
    [    0.328233] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.331936] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 26, base_baud = 3000000) is a 8250
    [    1.034054] console [ttyS0] enabled
    [    1.038498] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 27, base_baud = 3000000) is a 8250
    [    1.048258] [drm] Initialized drm 1.1.0 20060810
    [    1.064055] brd: module loaded
    [    1.072458] loop: module loaded
    [    1.076841] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    1.088910] mousedev: PS/2 mouse device common for all mice
    [    1.094628] i2c /dev entries driver
    [    1.099367] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
    [    1.099390] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
    [    1.099423] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (-517)
    [    1.099436] omap_hsmmc 48060000.mmc: lookup for GPIO cd failed
    [    1.099639] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
    [    1.099652] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
    [    1.099664] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
    [    1.099675] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
    [    1.099685] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
    [    1.099695] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
    [    1.099708] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
    [    1.099718] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
    [    1.099727] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
    [    1.099737] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
    [    1.099746] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
    [    1.099756] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
    [    1.100035] omap_hsmmc 481d8000.mmc: unable to get vmmc regulator -517
    [    1.106992] ledtrig-cpu: registered to indicate activity on CPUs
    [    1.113320] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
    [    1.120383] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
    [    1.126370] omap-sham 53100000.sham: initialization failed.
    [    1.132014] omap-sham: probe of 53100000.sham failed with error -22
    [    1.140477] oprofile: using arm/armv7
    [    1.144534] Initializing XFRM netlink socket
    [    1.149087] NET: Registered protocol family 17
    [    1.153601] NET: Registered protocol family 15
    [    1.158272] Key type dns_resolver registered
    [    1.162861] omap_voltage_late_init: Voltage driver support not added
    [    1.169688] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
    [    1.178523] cpu cpu0: cpu0 clock notifier not ready, retry
    [    1.184248] ThumbEE CPU extension supported.
    [    1.188621] Registering SWP/SWPB emulation handler
    [    1.196236] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
    [    1.196451] OMAP GPIO hardware version 0.1
    [    1.200999] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
    [    1.201541] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
    [    1.202082] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
    [    1.202452] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator@3[0]' - status (0)
    [    1.204260] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
    [    1.225523] tps65910 0-002d: No interrupt support, no core IRQ
    [    1.231781] tps65910-gpio tps65910-gpio: ti,en-gpio-sleep not specified
    [    1.231800] gpiochip_find_base: found new base at 506
    [    1.231935] gpiochip_add: registered GPIOs 506 to 511 on device: tps65910
    [    1.254964] tps65910-rtc tps65910-rtc: IRQ is not free.
    [    1.260294] tps65910-rtc: probe of tps65910-rtc failed with error -22
    [    1.267022] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
    [    1.273901] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 400 kHz
    [    1.280211] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
    [    1.280228] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
    [    1.280260] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
    [    1.280289] omap_hsmmc 48060000.mmc: Got CD GPIO
    [    1.284932] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
    [    1.284942] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
    [    1.284953] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
    [    1.284965] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
    [    1.284974] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
    [    1.284985] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
    [    1.285381] vmmc: supplied by vbat
    [    1.326252] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
    [    1.326277] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
    [    1.326292] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
    [    1.326305] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
    [    1.326315] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
    [    1.326326] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
    [    1.326339] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
    [    1.326349] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
    [    1.326359] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
    [    1.326368] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
    [    1.326377] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
    [    1.326387] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
    [    1.326716] vmmc: Restricting voltage, 3300000-1950000uV
    [    1.332065] omap_hsmmc 481d8000.mmc: could not set regulator OCR (-22)
    [    1.375672] vdd_mpu: supplied by vbat
    [    1.379540] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1260000]:-22
    [    1.389788] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1260000]:-22
    [    1.449302] mmc1: MAN_BKOPS_EN bit is not set
    [    1.457406] mmc1: new high speed MMC card at address 0001
    [    1.463389] mmcblk0: mmc1:0001 MMC04G 3.60 GiB
    [    1.468025] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
    [    1.474149] davinci_mdio 4a101000.mdio: detected phy mask c780ffcf
    [    1.480575] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
    [    1.487034] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
    [    1.493886] Atheros 8031 ethernet 4a101000.mdio:04: GPIO lookup for consumer reset
    [    1.493906] Atheros 8031 ethernet 4a101000.mdio:04: using lookup tables for GPIO lookup
    [    1.493918] Atheros 8031 ethernet 4a101000.mdio:04: lookup for GPIO reset failed
    [    1.501600] libphy: 4a101000.mdio: probed
    [    1.505874]  mmcblk0: p1 p2 p3 p4 < p5 p6 p7 >
    [    1.510610] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver Atheros 8031 ethernet
    [    1.522844] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver SMSC LAN8710/LAN8720
    [    1.532141] davinci_mdio 4a101000.mdio: phy[16]: device 4a101000.mdio:10, driver unknown
    [    1.540323] davinci_mdio 4a101000.mdio: phy[17]: device 4a101000.mdio:11, driver unknown
    [    1.548522] davinci_mdio 4a101000.mdio: phy[18]: device 4a101000.mdio:12, driver unknown
    [    1.556676] davinci_mdio 4a101000.mdio: phy[19]: device 4a101000.mdio:13, driver unknown
    [    1.564803] davinci_mdio 4a101000.mdio: phy[20]: device 4a101000.mdio:14, driver unknown
    [    1.572946] davinci_mdio 4a101000.mdio: phy[21]: device 4a101000.mdio:15, driver unknown
    [    1.581088] davinci_mdio 4a101000.mdio: phy[22]: device 4a101000.mdio:16, driver unknown
    [    1.589229] davinci_mdio 4a101000.mdio: phy[27]: device 4a101000.mdio:1b, driver unknown
    [    1.597371] davinci_mdio 4a101000.mdio: phy[29]: device 4a101000.mdio:1d, driver unknown
    [    1.606429] cpsw 4a100000.ethernet: Detected MACID = ec:24:b8:d1:58:6d
    [    1.613967] cpsw 4a100000.ethernet: cpsw: Detected MACID = ec:24:b8:d1:58:6f
    [    1.622039] hctosys: unable to open rtc device (rtc0)
    [    1.627188] of_cfs_init
    [    1.629745] of_cfs_init: OK
    [    1.636898] lis3_reg: disabling
    [    1.640186] ALSA device list:
    [    1.643164]   No soundcards found.
    [    1.652536] EXT4-fs (mmcblk0p1): INFO: recovery required on readonly filesystem
    [    1.660099] EXT4-fs (mmcblk0p1): write access will be enabled during recovery
    [    2.699753] EXT4-fs (mmcblk0p1): recovery complete
    [    2.709060] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
    [    2.717407] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.
    [    2.725660] devtmpfs: mounted
    [    2.729587] Freeing unused kernel memory: 272K (c0868000 - c08ac000)
    [    3.289234] random: init urandom read with 31 bits of entropy available
    [    3.666285] init: plymouth-upstart-bridge main process (83) terminated with status 1
    [    3.699028] init: plymouth-upstart-bridge main process ended, respawning
    [    3.838838] init: ureadahead main process (86) terminated with status 5
    [    3.859106] init: plymouth-upstart-bridge main process (94) terminated with status 1
    [    3.871591] init: plymouth-upstart-bridge main process ended, respawning
    [    4.330494] init: mounted-proc main process (110) terminated with status 1
    [    5.732214] systemd-udevd[189]: starting version 204
    [    6.377072] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [    6.450393] omap_rtc 44e3e000.rtc: already running
    [    6.459906] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc1
    [    6.680821] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
    [    8.557762] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro
    [    9.005477] random: nonblocking pool is initialized
    [    9.585101] net eth1: initializing cpsw version 1.12 (0)
    [    9.588711] net eth1: phy found : id is : 0x7c0f1
    [    9.609360] net eth1: BQL enabled
    [   10.133062] EXT4-fs (mmcblk0p7): recovery complete
    [   10.136306] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: errors=remount-ro
    [   10.338679] EXT4-fs (mmcblk0p5): recovery complete
    [   10.338728] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: errors=remount-ro
    [   10.715983] EXT4-fs (mmcblk0p6): recovery complete
    [   10.719297] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: errors=remount-ro
    [   13.746161] cpsw 4a100000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx
    [   16.824119] NET: Registered protocol family 10
    [   17.982327] init: avahi-daemon main process (716) terminated with status 127
    [   17.982442] init: avahi-daemon main process ended, respawning
    [   18.261095] init: avahi-cups-reload main process (723) terminated with status 1
    [   19.697259] init: plymouth-upstart-bridge main process ended, respawning
    root@:~#

    thanks!

  • One of our HW engineer found my mistake: TCLK had to be defined as INPUT and not OUTPUT

    WRONG:  0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a6.gmii2_tclk */

    the right configuration is:
                0x58 (PIN_INPUT_PULLUP | MUX_MODE1)    /* gpmc_a6.gmii2_tclk */

    the full Pinmux for MIi2 is:


                0x78 ( PIN_INPUT | MUX_MODE1 ) /* (U18) gpmc_be1n.gmii2_col */
                            0x70 ( PIN_INPUT | MUX_MODE1 ) /* (T17) gpmc_wait0.gmii2_crs */
                            0x74 ( PIN_INPUT_PULLUP | MUX_MODE1 ) /* (U17) gpmc_wpn.gmii2_rxer */

                /* Slave 2 */
                0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a0.GMII2_TXEN */
                0x44 (PIN_INPUT_PULLUP | MUX_MODE1)    /* gpmc_a1.GMII2_RXDV */

                0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a2.gmii2_td3 */
                0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a3.gmii2_td2 */
                0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a4.gmii2_td1 */
                0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a5.gmii2_td0 */

                0x58 (PIN_INPUT_PULLUP | MUX_MODE1)    /* gpmc_a6.gmii2_tclk */
                0x5c (PIN_INPUT_PULLUP  | MUX_MODE1)    /* gpmc_a7.gmii2_rclk */

                0x60 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a8.gmii2_rd3 */
                0x64 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a9.gmii2_rd2 */
                0x68 (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a10.gmii2_rd1 */
                0x6c (PIN_INPUT_PULLDOWN | MUX_MODE1)    /* gpmc_a11.gmii2_rd0 */

    thanks for your help  !