Hi,
I'm having a decoder problem on my platform which runs version of Android. Sometimes i get errors like these while video playback through an android app is ongoing. Does anyone have an idea on what might be going on?
--------- beginning of main 12-20 19:43:28.244 3097-13831/? E/IMG_Gralloc: Frame count is : 1349500218 12-20 19:43:28.244 3097-13831/? E/IMG_Gralloc: Bytes consumed - 1349500218 12-20 19:43:28.246 3097-13831/? E/IMG_Gralloc: Process function returned an Error... 12-20 19:43:28.246 3097-13831/? E/IMG_Gralloc: Codec Extended - 0x506fbd3a 12-20 19:43:28.246 3097-13831/? E/IMG_Gralloc: Input Buffer Size provided to codec is : 1349500218 12-20 19:43:28.246 3097-13831/? E/IMG_Gralloc: Frame count is : 1349500218 12-20 19:43:28.246 3097-13831/? E/IMG_Gralloc: Bytes consumed - 1349500218 12-20 19:43:28.248 3097-13831/? E/IMG_Gralloc: Process function returned an Error... 12-20 19:43:28.248 3097-13831/? E/IMG_Gralloc: Codec Extended - 0x506fbd3a 12-20 19:43:28.248 3097-13831/? E/IMG_Gralloc: Input Buffer Size provided to codec is : 1349500218 12-20 19:43:28.248 3097-13831/? E/IMG_Gralloc: Frame count is : 1349500218 12-20 19:43:28.248 3097-13831/? E/IMG_Gralloc: Bytes consumed - 1349500218 12-20 19:43:28.250 3097-13831/? E/IMG_Gralloc: Process function returned an Error... 12-20 19:43:28.250 3097-13831/? E/IMG_Gralloc: Codec Extended - 0x506fbd3a 12-20 19:43:28.250 3097-13831/? E/IMG_Gralloc: Input Buffer Size provided to codec is : 1349500218