Hi all,
After successfully starting the EVM C6657 board in SPI boot mode, we tried to boot in SPI mode with our final board which integrates a C6655.
The configuration of clocks is normally the same as the one on EVM board (100 MHz for the core, 66.67 MHz for the DDR3). We therefore use the same boot table as for the EVM board.
The problem we have is that after having loaded the binary into the SPI flash (this part works well), and after resetting the component, the microcontroller remains at the address 0x20b0eb90. The PLLM and PLLEN registers are equal to 0.
Do you have any idea what might happen ?