Part Number: EVMK2H
Tool/software: Linux
Hi,
We want to figure out the real time DSP frequency while running the code on Linux. We are using MCSDK 3.1.4.7. There is a CSL function call
"CSL_tscRead()" that return clock cycle. However, to convert to real time, we need to know the real time frequency. Keystone 2 data sheet listed DSP can go up to 1.2GHz, and ARM can go up to
1.4GHz. These information are great, but we wish there is a function call from maybe Chip Support Library to get the real time frequency for the DSP. Could you help us?
Sincerely
Yoyo