This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5517: C5517 got all zero results from hwafft output

Part Number: TMS320C5517

Tool/software: Code Composer Studio

Dear there,

I am using TMS320C5517 DSP for a project. I got a BIG problem in using this chip. I need some help urgently.

The problem is that I always get all zero results from hwafft on c5517.

The attachment is a test project which using samples data of 1k sine wave at 48k FS as input for 1024 pts fft and then printf the output results of hwafft_1024pts().

The test project runs well on the my ezDsp5515 usbstk. However, I got all zero fft output on the c5517 board.

I am sure I was using the correct hwafft routines address in the CMD file.

Can anybody help me here?

HLNVPREG1.0.rar