This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hello TI Experts,
I have download the gst-plugin-dsp66 source code from http://git.ti.com/processor-sdk/gst-plugin-dsp66 and compiled it.
then I replace the same name file in AM5728 target board, and I input command "gst-inspect-1.0 dsp66videokernel", the system not found the element.
How to resolved this issue ? Please help me , thanks !
My compiled scripts is following and compiled it successed.
GST_MODULES="gstreamer gst-plugin-base gst-plugin-good gst-plugin-libav gst-plugin-dsp66" GST_CONF=("" "--disable-pango --disable-ivorbis" "--disable-libpng" "" "") LOG_PATH=$PWD/gst-log export PREFIX=$PWD/ARMInstall # AM5728 Enviroment export SDK_PATH_TARGET=$HOME/work_home/Source/am57xx_evm_3.0/linux-devkit/sysroots/cortexa15hf-neon-linux-gnueabi export TI_OCL_CGT_INSTALL=$SDK_PATH_TARGET/usr/share/ti/cgt-c6x export TARGET_ROOTDIR=$SDK_PATH_TARGET export DESTDIR=$PREFIX i=0 rm -rf $LOG_PATH/* for MODULE in $GST_MODULES; do cd $MODULE ./autogen.sh > $LOG_PATH/$MODULE.log 2>&1 PATH=$PREFIX/bin:$PATH PKG_CONFIG_PATH=$PREFIX/lib/pkgconfig ./configure CC=arm-linux-gnueabihf-gcc --build=i686-linux --host=arm-linux ${GST_CONF[i]} >> $LOG_PATH/$MODULE.log 2>&1 make clean >> $LOG_PATH/$MODULE.log 2>&1 && make -s -j4 >> $LOG_PATH/$MODULE.log 2>&1 && make install >> $LOG_PATH/$MODULE.log 2>&1 if [ $? -ne 0 ]; then echo "$MODULE make error"; exit; else echo "$MODULE make success"; fi let i+=1 cd - done