Dear TI guys
I have use C5509A for a walkie-talkie project, meet a power consumption issue.
when the core voltage is 1.6V, the frequency-power consumption is 0.6mA/Mhz in datasheet, but in face, when 5509A run at 96Mhz in our system, the core power consumption is 92.9mA.
when the core voltage is 1.2V, the frequency-power consumption is 0.45mA/Mhz in datasheet, but in face, when 5509A run at 96Mhz in our system, the core power consumption is 64.1mA.
could you kindly help to advise how can I do to reduce this power consumption?
thanks a lot!