This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
a cusotmer of mine makes telecommunication PBX (IP and normal Line).
They have an issue with OMAP-L138, and it seems that due to bug in silicon OMAP do not support SATA III.
As Drives with SATA II seems to run dry, suppliers switches to SATA III, and they need support on how to overcome this issue.
There is Errata available with “'port multiplier” although they asses this will be a very expensive solution for them.
They would like to get our feed if there might be any other solution to solve that issue (external chip).
any advice is more than welcome
thanks a lot in advance
KR
Vincenzo
Vincenzo,
Mukul is correct...this IP issue was discovered and fixed prior to AM571x PG and as such this device is not affected. Please refer to the AM571x Errata to ensure that this device meets the customer's needs.
-DK