Part Number: TMS320C6657
Hi all,
My customer used c6657 and it have DDR ECC chip on board.
we enabled the ECC function and set the ecc and address range as below.
Here is the summarize:
1, After ecc enabled DDR AUTO LEVELING failed.
2, ECC address range ddr read/write check failed. I used the 64bit aligned access to ddr , it can't pass the memory check.
3, DDR which not in the range of ecc check, it can pass memory check.
The similar code can be test on tci6614 board. It runs well, it can pass the ddr memory check after ecc enabled.
Here is my questions:
1, How to verify the 6657 ddr ecc function?
2, 6657 36bit ddr interface and tci6614 is 72 bit ddr interface. Are there any special setting is necessary for 6657?
3, Other advise?
thanks!
BR,
Denny