This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Pinmux for CPSW and PRU-ICSS

Part Number: AM5728
Other Parts Discussed in Thread: AM5718,

I have been told that the only way to get six ports is to use the AM5718 instead of the AM5728 because the AM5728 shares its Gb ethernet pins with the PRU1 MII pins.  However, would it be possible to use one Gb switch going to the A-15, and one MII going to the PRU1 MII port?  In this setup I would have the PRU1 port parsing an industrial protocol and the A-15 port connecting to the internet.  It seems possible in the pinmux tool but I wanted to confirm.