This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

4K Capture/Encode Streaming Application



Hello TI,

We are working on system which Capture/Encode video resolution upto 4k and streaming it. We found one of the TI EVM which support 4k Resution mentioned below.

http://www.ti.com/devnet/docs/catalog/endequipmentproductfolder.tsp?actionPerformed=productFolder&productId=18160

Can you please suggest where i can get software devlopment kit for this EVM? Do we need to purchase licence for it?


Thanks,
Devang

  • Hi Hiren,

    This Z3-DM8169-4K-RPS Video Encoder Starter Kit is supported by:

    Technical Support Contact
    Martin Burgos
    Business Development Director
    1-402-3251577-
    http://www.Z3technology.com
    burgos@z3technology.com

    Regards,
    Pavel
  • Hiren,

    Also some info:

    1. The DM8169 is not available. However, if you are interested in pursuing 4K DSP applications, we would suggest using the DM8168 DaVinci Video Processor.

    2. The DM8168 is the exact same hardware as the DM8169, and the only difference is that the DM8169 had an additional codec. This codec has no bearing on the ability of the processor itself to generate 4K video, as the codec was not related to video resolution. Therefore, the DM8169 would give you no advantage over the DM8168 in terms of 4K video.
    The other advantage is that the DM8168 is less expensive due to the fact that the DM8169 was priced at a premium due to this additional codec.

    3. We do not have any software to enable 4K video, and we will not be able to support this device moving forward.
    We would suggest reaching out to Z3 for support in regards to enabling 4K.

    Sales contact: sales@z3technology.com
    Technical Support contact: burgos@z3technology.com


    See also below e2e threads:

    e2e.ti.com/.../377027
    e2e.ti.com/.../247031
    e2e.ti.com/.../250193

    Regards,
    Pavel
  • Hi Devang (via Hiren Kumbhare),

    You can contact Z3 Technology at sales@z3technology.com or +1.402.323.0702 to discuss our 4K video offerings based upon the DM8169

    Thanks,
    Charles Flint III
    Z3 Technology, LLC