This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What version are you using of:
CCS?
BIOS?
What chip/platform are you using?
Hussen,
The best information about RTA in SYS/BIOS 6 is in the product's User Guide, which you can find in your installation's doc directory. See chapter 7 of the document.
There are a number of different parts to RTA in SYS/BIOS, including
Also, here is a block diagram that shows the overall architecture of the RTA tooling. Note that on the target side, one or more buffers need to be set up in order to collect the data. Since these buffers are finite in length, you'll need to think about how large they should be to collect the data that you want before the RTA data gets examined. At this point, you sould focus on just examining the RTA data in stop mode, since the full support for transporting RTA data over physical streams such as serial or Ethernet has not been fully rolled out for SYS/BIOS 6. Even in stop-mode, you can still use the RTA plug-in inside CCS to examine all the RTA data.
Hope that's enough to get you started.