Part Number: AM4376
If I want to boot from a NAND flash. At which Pin of the Sitara do I have to connect the Busy Pin from the Flash if I select with SYSBOOT[8] = 0 Wait mux option 0.
And at which Pin if I have selected SYSBOOT[8] = 1?
This is not clear from the datasheet because it doesn’t say what the Wait mux option 0 and 1 means. It could mean selecting the gpmc_wait0 or gpmc_wait1 pin or it could mean selecting Pin B12 or A2 for gpmc_wait0.