This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
We are using the AM4376 in our design, and have successfully implemented Parallel NOR FLASH and two FPGAs with SRAM interfaces the GPMC bus. All 3 devices use non muxed Address and Data lines. The processor boots from NOR FLASH.
We are considering replacing the NOR FLASH with NAND FLASH, and having the processor boot from NAND FLASH. The datasheet and user manual don't explicitly state it, but is it acceptable to include both muxed and non muxed devices on the GPMC bus? The extra pins required for NAND FLASH are not assigned to other functions, so that should not be an issue.
Thanks,
M