I just can't find a "big picture" anywhere. The closed I've come is on the wiki at http://processors.wiki.ti.com/index.php/When_to_use_and_when_not_to_use_Codec_Engine where a use case is given for "I want to build my own DSP-side applications(s)", but that's for OMAP-L138 and I want to use DM6467T.
Are there any bubble diagrams or something explaining how Linux, Codec Engine, and XDAIS Framework Components fit together? Do either of the latter two require Linux? Are the latter two related? Is there overview documentation for either of the latter two? I just can't find anything that covers the fundamental questions about them.
All I want to do is my video analytics on the DSP. I don't need a generic reconfigurable workhorse.
(I realize this is partially repeating another post. Unfortunately, I've been trying to get answers to these types of questions for a week and a half, getting no traction at all. So I'm both desperate as well as continuously discovering new points of view for rephrasing the question.)
Thanks very much,
Helmut