Tool/software: Linux
We have tried multiple vendors and we have eliminated 2 of them due to the slow speed issues. Some come up at 3Gb/s and some at 1.5GB/s. We can’t tolerate the 1.5GB/s rate due to the long bootup time and then sluggish system response. Our system only uses 1 SATA link (port 2) on the TI DSP.
This one memory is working great except at temperature of 65C it does not even get detected on a power cycle . The attached logs shows our sequence. On a power cycle of our main voltage we do not do a shutdown command and so our software detects this and requires a reboot. This second reboot continues until we power cycle the unit.
We found 1 vendor works from -35C to 65C on power cycles but has this occasional state of failure at 65C.
-
Power cycle at 65C and the system does not even recognize the MSATA.
-
Our system hangs 2 minutes and reboots.
-
Again the MSATA is not detected.
-
This repeats forever until we power cycle.
If we lower the temperature to 30C it still does not reboot on its own. We think the 65C temperature initiates the problem but lowering the temperature does not allow it to recover.
Here’s the startup sequence to compare with a good startup. On the left below shows the problem where ata2 is down. It is not detected for some reason. We do not have a ata 1 device.
You can compare the first 2 files. Left side is the teraterm WCS2 May 7…. And the right side is the teraterm May Virtium good.
This always occurs at ~1.35 seconds on power cycle as recorded by the kernel.