This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are trying to do software leveling with AM3352 and DDR3L.
While using the Ratio Seed spreadsheet I found out that DQS1 lengths if longer than the CLK and DQS0 is shorter than CLK.
So on one case I need to invert the clock on "1" and on the second case I have keep it "0 ".
Parameters | Comments | |||
DDR clock frequency | 400 | MHz | input maximum frequency you will use | |
PHY_INVERT_CLKOUT | 0 | If (DDR_CK length) < (DDR_DQS length), then use 1. If (DDR_CK length) > (DDR_DQS length), then use 0. | ||
Trace Length (inches) | ||||
Byte 0 | Byte 1 | |||
DDR_CK trace | 0.7906 | 0.7906 | input the average of DDR_CK and DDR_CKn traces. If you have two x8 memories, use the trace lengths for each corresponding byte. | |
DDR_DQSx trace | 0.727 | 0.9852 | x can be 0 or 1, corresponding to each byte. | |
Intermediate values (per byte lane) | ||||
WR DQS | 1 | FFFFFFFFFD | these are just used for the calculations below | |
RD DQS | 40 | 40 | these are just used for the calculations below | |
RD DQS GATE | 69 | 72 | these are just used for the calculations below |
How can we do software leveling in this layout?
Thanks,
Nadav
James,
we tried to run the script with the new radio seed while choosing invert.
it seems wrong because for some reason both DATA_PHY_RD_DQS_SLAVE_RATIO and DATA_PHY_WR_DQS_SLAVE_RATIO is 0.
we tried to use the optimum Value and as suspected it failed.
This is the log that I received
[CortxA8]
Enter the PHY_INVERT_CLKOUT value (0 or 1) from the spreadsheet
1
Enter the Seed RD_DQS_SLAVE_RATIO Value in Hex to search the RD DQS Ratio Window
40
Enter the Seed FIFO_WE_SLAVE_RATIO Value in Hex to search the RD DQS Gate Window
ED
Enter the Seed WR_DQS_SLAVE_RATIO Write DQS Ratio Value in Hex to search the Write DQS Ratio Window
7E
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x000 | 0x0e9 | 0x074 | 0xffffff17
DATA_PHY_WR_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DATA_SLAVE_RATIO 0x0f1 | 0x086 | 0x0bb | 0x06b
***************************************************************
rd_dqs_range = 0
fifo_we_range = 74
wr_dqs_range = 0
wr_data_range = bb
Optimal values not reached, rerunning program with new values...
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x000 | 0x0e9 | 0x074 | 0xffffff17
DATA_PHY_WR_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DATA_SLAVE_RATIO 0x0f1 | 0x086 | 0x0bb | 0x06b
***************************************************************
rd_dqs_range = 0
fifo_we_range = 0
wr_dqs_range = 0
wr_data_range = 0
Optimal values have been found!!
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x000 | 0x0e9 | 0x074 | 0xffffff17
DATA_PHY_WR_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DATA_SLAVE_RATIO 0x0f1 | 0x086 | 0x0bb | 0x06b
***************************************************************
===== END OF TEST =====
Ratio Seed values spreadsheet:
Parameters | Comments | |||
DDR clock frequency | 400 | MHz | input maximum frequency you will use | |
PHY_INVERT_CLKOUT | 1 | If (DDR_CK length) < (DDR_DQS length), then use 1. If (DDR_CK length) > (DDR_DQS length), then use 0. | ||
Trace Length (inches) | ||||
Byte 0 | Byte 1 | |||
DDR_CK trace | 0.7906 | 0.7906 | input the average of DDR_CK and DDR_CKn traces. If you have two x8 memories, use the trace lengths for each corresponding byte. | |
DDR_DQSx trace | 0.727 | 0.9852 | x can be 0 or 1, corresponding to each byte. | |
Intermediate values (per byte lane) | ||||
WR DQS | 81 | 7C | these are just used for the calculations below | |
RD DQS | 40 | 40 | these are just used for the calculations below | |
RD DQS GATE | E9 | F2 | these are just used for the calculations below | |
Seed values used in CCS code | ||||
DATAx_PHY_RD DQS_SLAVE_RATIO | 40 | |||
DATAx_PHY_FIFO_WE_SLAVE_RATIO | ED | |||
DATAx_PHY_WR DQS_SLAVE_RATIO | 7E | |||
Register value | ||||
CMDx_PHY_CTRL_SLAVE_RATIO | 100 |
Hi James,
We have ddr iniailization code in uboot, inside MLO, it is derived from the standard ti sdk uboot, we added a new board type (copied from a ti am335x). And in our new board type, we changed the ddr iniailization code.
After change the GEL with the values generated, I tried the DDR test scripts, and it failed.
Also when using the memory browser, I can see the memory is not stable.
Each time I hit enter on the address 0x80000000, I can see somwething has changed, returning either all 0 on certain address.
I think the memry test function, write A5 to these addresses. See below, each time the result is different, it is as if the data A5A5A5A5 is in the memory, but each time the read would fail and return 0x00000000 on random addresses.
Also the 0xFFFFFFFF, I think indicate write failure during the memtest, they behave more lide the A5A5A5A5 values, more likely the memtest failed to write the A5 into those locations.
0x80000000 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x80000014 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x80000028 A5A5A5A5 A5A5A5A5 00000000 A5A5A5A5 A5A5A5A5
0x8000003C A5A5A5A5 A5A5A5A5 FFFFFFFF A5A5A5A5 A5A5A5A5
0x80000050 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x80000064 FFFFFFFF A5A5A5A5 A5A5A5A5 A5A5A5A5 00000000
0x80000078 00000000 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x8000008C A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x800000A0 A5A5A5A5 A5A5A5A5 00000000 00000000 A5A5A5A5
0x800000B4 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x800000C8 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x800000DC A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x800000F0 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x80000104 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x80000118 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
0x8000012C A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5
Also here is our Gel modification.
#define CMD_PHY_CTRL_SLAVE_RATIO 0x100
#define CMD_PHY_INVERT_CLKOUT 0x1
#define DATA_PHY_RD_DQS_SLAVE_RATIO 0x40
#define DATA_PHY_FIFO_WE_SLAVE_RATIO 0xB2 //RD DQS GATE
#define DATA_PHY_WR_DQS_SLAVE_RATIO 0x82
#define DATA_PHY_WR_DATA_SLAVE_RATIO 0xBE //WRITE DATA
Jeff
Hi,
the MPN we are using is: MT41K256M16TW-107:P (MICRON).
see attached the spreadsheet from step 1 you mentioned.