Other Parts Discussed in Thread: TMS320C5504
Hello,
My customer needs to estimate the maximum value of the CVDD current. A sample value would be accepted. Could you please advise?
Condition:
* 1.3V
* Processing at Full load.
* 100MHz
From the DS p-56, we found 0.31mW/MHz(typ), that is 31mW@100MHz(typ). Then could you please add a sufficient margins to estimate a sample max value?