Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
We try to operate a USB 2.0 camera with minimun bandwidth requiment of 150 Mbps with an AM335x, Linux Debian powerd board (e.g.Beaglebone blue).
Although AM335x USB controller is reported to be capable as a host to handle USB devices in High speed mode (480 Mbit/s), according to Benchamarks the above throuput cannot be achieved.
Could the High speed rate be reached using some special Linux kernel modification ?