Tool/software: Linux
Hello All,
I'm trying to interface xilinx FPGA with am3359 via GPCM(CS1) on custom board based on AM3359 icev2.A nand flash is also connected to the GPMC(CS0).I added fpga and nand as the child nodes of gpmc in the device tree.Is the device tree configuration and enabling the respective fpga drivers enough to access the fpga?.Also I would like to write a .bin file to fpga from the user space.Is it possible?. The board is is the final phase of design.I'm looking for a head start.Any information would be really helpful.TIA
Regards,
Murugan S