Other Parts Discussed in Thread: DRA718, DRA72, DRA722, AM5728, TMDXIDK5718, , DRA71XEVM, DRA71, AM5718
Tool/software: Linux
Hi:
I have a custom AM5708 based board and want to use keyboard controller to handle a key pad.
I am working with SDK Linux RT 5.00.00.15.
Attached are the dts and config file for Linux
During Linux startup I get the following message:
[ 1.926557] omap4-keypad 4ae1c00000000080.keypad: no base address specified
[ 1.933577] omap4-keypad: probe of 4ae1c00000000080.keypad failed with error2
Billa 0576.bridge_linux.dts.txt
CONFIG_NO_HZ=y CONFIG_HIGH_RES_TIMERS=y CONFIG_BLK_DEV_INITRD=y CONFIG_PERF_EVENTS=y CONFIG_PARTITION_ADVANCED=y CONFIG_CMDLINE_PARTITION=y # CONFIG_ARCH_MULTI_V5 is not set # CONFIG_ARCH_MULTI_V4 is not set CONFIG_MACH_ARTPEC6=y CONFIG_MACH_ARMADA_370=y CONFIG_MACH_ARMADA_375=y CONFIG_MACH_ARMADA_38X=y CONFIG_MACH_ARMADA_39X=y CONFIG_MACH_ARMADA_XP=y CONFIG_MACH_DOVE=y CONFIG_SOC_SAMA5D2=y CONFIG_SOC_SAMA5D3=y CONFIG_SOC_SAMA5D4=y CONFIG_ARCH_BCM2835=y CONFIG_ARCH_BCM_63XX=y CONFIG_MACH_BERLIN_BG2=y CONFIG_MACH_BERLIN_BG2CD=y CONFIG_MACH_BERLIN_BG2Q=y CONFIG_SOC_IMX50=y CONFIG_SOC_IMX51=y CONFIG_SOC_IMX53=y CONFIG_SOC_IMX6Q=y CONFIG_SOC_IMX6SL=y CONFIG_SOC_IMX6SX=y CONFIG_SOC_IMX6UL=y CONFIG_SOC_IMX7D=y CONFIG_SOC_VF610=y CONFIG_SOC_LS1021A=y CONFIG_MACH_SPEAR1310=y CONFIG_MACH_SPEAR1340=y CONFIG_EXYNOS5420_MCPM=y CONFIG_ARCH_R8A7743=y CONFIG_ARCH_R8A7745=y CONFIG_ARCH_R8A7792=y CONFIG_MACH_HREFV60=y CONFIG_MACH_SNOWBALL=y CONFIG_TRUSTED_FOUNDATIONS=y CONFIG_PCI_HOST_GENERIC=y CONFIG_PCI_KEYSTONE=y CONFIG_PCI_MSI=y CONFIG_PCI_MVEBU=y CONFIG_PCI_TEGRA=y CONFIG_PCI_RCAR_GEN2=y CONFIG_PCIE_RCAR=y CONFIG_PCIEPORTBUS=y CONFIG_HIGHPTE=y CONFIG_CMA=y CONFIG_EFI=y CONFIG_CPU_FREQ_GOV_SCHEDUTIL=y CONFIG_ARM_IMX6Q_CPUFREQ=y CONFIG_ARM_ZYNQ_CPUIDLE=y CONFIG_ARM_EXYNOS_CPUIDLE=y CONFIG_PACKET=y CONFIG_UNIX=y CONFIG_IP_PNP=y CONFIG_IP_PNP_DHCP=y CONFIG_IP_PNP_BOOTP=y CONFIG_IP_PNP_RARP=y CONFIG_IPV6_ROUTER_PREF=y CONFIG_IPV6_OPTIMISTIC_DAD=y CONFIG_INET6_ESP=m CONFIG_IPV6_MIP6=m CONFIG_IPV6_MULTIPLE_TABLES=y CONFIG_NET_DSA=m CONFIG_NET_SWITCHDEV=y CONFIG_CAN_RAW=y CONFIG_CAN_BCM=y CONFIG_CAN_DEV=y CONFIG_CAN_AT91=m CONFIG_CAN_RCAR=m CONFIG_CAN_XILINXCAN=y CONFIG_CAN_MCP251X=y CONFIG_B53_SPI_DRIVER=m CONFIG_B53_MDIO_DRIVER=m CONFIG_B53_MMAP_DRIVER=m CONFIG_B53_SRAB_DRIVER=m CONFIG_CAN_SUN4I=y CONFIG_BT=m CONFIG_BT_MRVL=m CONFIG_BT_MRVL_SDIO=m CONFIG_CFG80211=m CONFIG_MAC80211=m CONFIG_RFKILL=y CONFIG_RFKILL_INPUT=y CONFIG_RFKILL_GPIO=y CONFIG_DMA_CMA=y CONFIG_OMAP_OCP2SCP=y CONFIG_SIMPLE_PM_BUS=y CONFIG_SUNXI_RSB=y CONFIG_MTD=y CONFIG_MTD_BLOCK=y CONFIG_MTD_M25P80=y CONFIG_MTD_NAND=y CONFIG_MTD_NAND_DENALI_DT=y CONFIG_MTD_NAND_ATMEL=y CONFIG_MTD_NAND_BRCMNAND=y CONFIG_MTD_NAND_VF610_NFC=y CONFIG_MTD_NAND_DAVINCI=y CONFIG_MTD_SPI_NOR=y CONFIG_SPI_FSL_QUADSPI=m CONFIG_MTD_UBI=y CONFIG_BLK_DEV_LOOP=y CONFIG_BLK_DEV_RAM=y CONFIG_BLK_DEV_RAM_SIZE=65536 CONFIG_VIRTIO_BLK=y CONFIG_AD525X_DPOT=y CONFIG_AD525X_DPOT_I2C=y CONFIG_ATMEL_TCLIB=y CONFIG_ICS932S401=y CONFIG_ATMEL_SSC=m CONFIG_QCOM_COINCELL=m CONFIG_APDS9802ALS=y CONFIG_ISL29003=y CONFIG_EEPROM_AT24=y CONFIG_BLK_DEV_SD=y CONFIG_BLK_DEV_SR=y CONFIG_SCSI_MULTI_LUN=y CONFIG_AHCI_BRCM=y CONFIG_AHCI_DM816=y CONFIG_AHCI_ST=y CONFIG_AHCI_IMX=y CONFIG_AHCI_SUNXI=y CONFIG_AHCI_TEGRA=y CONFIG_SATA_HIGHBANK=y CONFIG_SATA_MV=y CONFIG_SATA_RCAR=y CONFIG_NETDEVICES=y CONFIG_VIRTIO_NET=y CONFIG_HIX5HD2_GMAC=y CONFIG_SUN4I_EMAC=y CONFIG_MACB=y CONFIG_BGMAC_BCMA=y CONFIG_NET_CALXEDA_XGMAC=y CONFIG_GIANFAR=y CONFIG_MV643XX_ETH=y CONFIG_MVNETA=y CONFIG_PXA168_ETH=m CONFIG_KS8851=y CONFIG_R8169=y CONFIG_SH_ETH=y CONFIG_SMSC911X=y CONFIG_STMMAC_ETH=y CONFIG_STMMAC_PLATFORM=y CONFIG_DWMAC_DWC_QOS_ETH=y CONFIG_XILINX_EMACLITE=y CONFIG_AT803X_PHY=y CONFIG_SMSC_PHY=y CONFIG_REALTEK_PHY=y CONFIG_FIXED_PHY=y CONFIG_ROCKCHIP_PHY=y CONFIG_USB_SUPPORT=y CONFIG_USB=m CONFIG_USB_PEGASUS=y CONFIG_USB_RTL8152=m CONFIG_USB_NET_SMSC75XX=y CONFIG_BRCMFMAC=m CONFIG_RT2X00=m CONFIG_RT2800USB=m CONFIG_MWIFIEX=m CONFIG_MWIFIEX_SDIO=m CONFIG_INPUT_JOYDEV=y CONFIG_INPUT_EVDEV=y CONFIG_KEYBOARD_QT1070=m CONFIG_KEYBOARD_GPIO=y CONFIG_KEYBOARD_TEGRA=y CONFIG_KEYBOARD_SPEAR=y CONFIG_KEYBOARD_ST_KEYSCAN=y CONFIG_KEYBOARD_CROS_EC=m CONFIG_KEYBOARD_SAMSUNG=m CONFIG_KEYBOARD_OMAP4=y CONFIG_MOUSE_PS2_ELANTECH=y CONFIG_MOUSE_CYAPA=m CONFIG_MOUSE_ELAN_I2C=y CONFIG_INPUT_TOUCHSCREEN=y CONFIG_TOUCHSCREEN_ATMEL_MXT=m CONFIG_TOUCHSCREEN_MMS114=m CONFIG_TOUCHSCREEN_ST1232=m CONFIG_TOUCHSCREEN_STMPE=y CONFIG_TOUCHSCREEN_SUN4I=y CONFIG_TOUCHSCREEN_WM97XX=m CONFIG_INPUT_MISC=y CONFIG_INPUT_MAX77693_HAPTIC=m CONFIG_INPUT_MAX8997_HAPTIC=m CONFIG_INPUT_AXP20X_PEK=m CONFIG_INPUT_ADXL34X=m CONFIG_SERIO_AMBAKMI=y CONFIG_SERIAL_8250=y CONFIG_SERIAL_8250_CONSOLE=y CONFIG_SERIAL_8250_MT6577=y CONFIG_SERIAL_8250_UNIPHIER=y CONFIG_SERIAL_AMBA_PL011_CONSOLE=y CONFIG_SERIAL_ATMEL=y CONFIG_SERIAL_ATMEL_CONSOLE=y CONFIG_SERIAL_ATMEL_TTYAT=y CONFIG_SERIAL_BCM63XX=y CONFIG_SERIAL_BCM63XX_CONSOLE=y CONFIG_SERIAL_MESON=y CONFIG_SERIAL_MESON_CONSOLE=y CONFIG_SERIAL_SAMSUNG=y CONFIG_SERIAL_SAMSUNG_CONSOLE=y CONFIG_SERIAL_SIRFSOC=y CONFIG_SERIAL_SIRFSOC_CONSOLE=y CONFIG_SERIAL_TEGRA=y CONFIG_SERIAL_IMX=y CONFIG_SERIAL_IMX_CONSOLE=y CONFIG_SERIAL_SH_SCI=y CONFIG_SERIAL_SH_SCI_NR_UARTS=20 CONFIG_SERIAL_SH_SCI_CONSOLE=y CONFIG_SERIAL_SH_SCI_DMA=y CONFIG_SERIAL_MSM=y CONFIG_SERIAL_MSM_CONSOLE=y CONFIG_SERIAL_VT8500=y CONFIG_SERIAL_VT8500_CONSOLE=y CONFIG_SERIAL_OF_PLATFORM=y CONFIG_SERIAL_OMAP_CONSOLE=y CONFIG_SERIAL_XILINX_PS_UART_CONSOLE=y CONFIG_SERIAL_FSL_LPUART_CONSOLE=y CONFIG_SERIAL_CONEXANT_DIGICOLOR_CONSOLE=y CONFIG_SERIAL_ST_ASC_CONSOLE=y CONFIG_HVC_DRIVER=y CONFIG_VIRTIO_CONSOLE=y CONFIG_I2C_CHARDEV=y CONFIG_I2C_DAVINCI=y CONFIG_I2C_ARB_GPIO_CHALLENGE=m CONFIG_I2C_MUX_PCA954x=y CONFIG_I2C_MUX_PINCTRL=y CONFIG_I2C_DEMUX_PINCTRL=y CONFIG_I2C_AT91=m CONFIG_I2C_BCM2835=y CONFIG_I2C_CADENCE=y CONFIG_I2C_DIGICOLOR=m CONFIG_I2C_EMEV2=m CONFIG_I2C_EXYNOS5=y CONFIG_I2C_IMX=m CONFIG_I2C_MV64XXX=y CONFIG_I2C_RIIC=y CONFIG_I2C_S3C2410=y CONFIG_I2C_SH_MOBILE=y CONFIG_I2C_SIRF=y CONFIG_I2C_ST=y CONFIG_I2C_SUN6I_P2WI=y CONFIG_I2C_TEGRA=y CONFIG_I2C_UNIPHIER=y CONFIG_I2C_UNIPHIER_F=y CONFIG_I2C_RCAR=y CONFIG_I2C_CROS_EC_TUNNEL=m CONFIG_I2C_SLAVE_EEPROM=y CONFIG_SPI=y CONFIG_SPI_ATMEL=m CONFIG_SPI_BCM2835=y CONFIG_SPI_BCM2835AUX=y CONFIG_SPI_DAVINCI=y CONFIG_SPI_GPIO=m CONFIG_SPI_FSL_DSPI=m CONFIG_SPI_OMAP24XX=y CONFIG_SPI_ORION=y CONFIG_SPI_PL022=y CONFIG_SPI_RSPI=y CONFIG_SPI_S3C64XX=m CONFIG_SPI_SH_MSIOF=m CONFIG_SPI_SH_HSPI=y CONFIG_SPI_SIRF=y CONFIG_SPI_SUN4I=y CONFIG_SPI_SUN6I=y CONFIG_SPI_TEGRA114=y CONFIG_SPI_TEGRA20_SFLASH=y CONFIG_SPI_TEGRA20_SLINK=y CONFIG_SPMI=y CONFIG_PINCTRL_AS3722=y CONFIG_PINCTRL_PALMAS=y CONFIG_PINCTRL_BCM2835=y CONFIG_PINCTRL_APQ8064=y CONFIG_PINCTRL_APQ8084=y CONFIG_PINCTRL_IPQ8064=y CONFIG_PINCTRL_MSM8660=y CONFIG_PINCTRL_MSM8960=y CONFIG_PINCTRL_MSM8X74=y CONFIG_PINCTRL_MSM8916=y CONFIG_PINCTRL_QCOM_SPMI_PMIC=y CONFIG_PINCTRL_QCOM_SSBI_PMIC=y CONFIG_GPIO_DAVINCI=y CONFIG_GPIO_RCAR=y CONFIG_GPIO_ZYNQ=y CONFIG_GPIO_PCA953X_IRQ=y CONFIG_GPIO_TWL4030=y CONFIG_GPIO_PALMAS=y CONFIG_GPIO_SYSCON=y CONFIG_GPIO_TPS65910=y CONFIG_BATTERY_ACT8945A=y CONFIG_BATTERY_SBS=y CONFIG_BATTERY_MAX17040=m CONFIG_BATTERY_MAX17042=m CONFIG_CHARGER_MAX14577=m CONFIG_CHARGER_MAX77693=m CONFIG_CHARGER_MAX8997=m CONFIG_CHARGER_MAX8998=m CONFIG_CHARGER_TPS65090=y CONFIG_AXP20X_POWER=m CONFIG_POWER_RESET_AS3722=y CONFIG_POWER_RESET_GPIO=y CONFIG_POWER_RESET_GPIO_RESTART=y CONFIG_POWER_RESET_KEYSTONE=y CONFIG_POWER_RESET_RMOBILE=y CONFIG_POWER_RESET_ST=y CONFIG_POWER_AVS=y CONFIG_ROCKCHIP_IODOMAIN=y CONFIG_SENSORS_IIO_HWMON=y CONFIG_SENSORS_LM90=y CONFIG_SENSORS_LM95245=y CONFIG_SENSORS_NTC_THERMISTOR=m CONFIG_SENSORS_PWM_FAN=m CONFIG_SENSORS_INA2XX=m CONFIG_BRCMSTB_THERMAL=m CONFIG_ROCKCHIP_THERMAL=y CONFIG_RCAR_THERMAL=y CONFIG_ARMADA_THERMAL=y CONFIG_DAVINCI_WATCHDOG=m CONFIG_EXYNOS_THERMAL=m CONFIG_ST_THERMAL_MEMMAP=y CONFIG_DA9063_WATCHDOG=m CONFIG_ARM_SP805_WATCHDOG=y CONFIG_AT91SAM9X_WATCHDOG=y CONFIG_SAMA5D4_WATCHDOG=y CONFIG_ORION_WATCHDOG=y CONFIG_ST_LPC_WATCHDOG=y CONFIG_SUNXI_WATCHDOG=y CONFIG_IMX2_WDT=y CONFIG_TEGRA_WATCHDOG=m CONFIG_MESON_WATCHDOG=y CONFIG_DIGICOLOR_WATCHDOG=y CONFIG_BCM2835_WDT=y CONFIG_BCM47XX_WDT=y CONFIG_BCM_KONA_WDT=y CONFIG_MFD_ACT8945A=y CONFIG_MFD_AC100=y CONFIG_MFD_AXP20X_RSB=y CONFIG_MFD_QCOM_RPM=y CONFIG_MFD_SPMI_PMIC=y CONFIG_REGULATOR_ACT8945A=y CONFIG_REGULATOR_AB8500=y CONFIG_POWER_RESET_SYSCON=y CONFIG_REGULATOR_MAX8997=m CONFIG_REGULATOR_MAX8998=m CONFIG_REGULATOR_QCOM_RPM=y CONFIG_REGULATOR_QCOM_SMD_RPM=y CONFIG_REGULATOR_WM8994=m CONFIG_USB_GSPCA=y CONFIG_SOC_CAMERA=m CONFIG_SOC_CAMERA_PLATFORM=m CONFIG_VIDEO_RCAR_VIN=m CONFIG_VIDEO_ATMEL_ISI=m CONFIG_VIDEO_SAMSUNG_EXYNOS4_IS=m CONFIG_VIDEO_S5P_FIMC=m CONFIG_VIDEO_S5P_MIPI_CSIS=m CONFIG_VIDEO_EXYNOS_FIMC_LITE=m CONFIG_VIDEO_EXYNOS4_FIMC_IS=m CONFIG_VIDEO_SAMSUNG_S5P_JPEG=m CONFIG_VIDEO_SAMSUNG_S5P_MFC=m CONFIG_VIDEO_SAMSUNG_EXYNOS_GSC=m CONFIG_VIDEO_STI_BDISP=m CONFIG_VIDEO_STI_HVA=m CONFIG_VIDEO_STI_DELTA=m CONFIG_VIDEO_RENESAS_JPU=m CONFIG_VIDEO_RENESAS_VSP1=m CONFIG_V4L_TEST_DRIVERS=y CONFIG_VIDEO_ADV7180=m CONFIG_VIDEO_ML86V7667=m CONFIG_DRM_I2C_ADV7511_AUDIO=y # CONFIG_DRM_I2C_CH7006 is not set # CONFIG_DRM_I2C_SIL164 is not set CONFIG_DRM_DUMB_VGA_DAC=m CONFIG_DRM_EXYNOS_FIMD=y CONFIG_DRM_EXYNOS_MIXER=y CONFIG_DRM_EXYNOS_DPI=y CONFIG_DRM_EXYNOS_DSI=y CONFIG_DRM_EXYNOS_HDMI=y CONFIG_DRM_ROCKCHIP=m CONFIG_ROCKCHIP_ANALOGIX_DP=y CONFIG_ROCKCHIP_DW_HDMI=y CONFIG_ROCKCHIP_DW_MIPI_DSI=y CONFIG_ROCKCHIP_INNO_HDMI=y CONFIG_DRM_ATMEL_HLCDC=m CONFIG_DRM_RCAR_DU=m CONFIG_DRM_RCAR_LVDS=y CONFIG_DRM_SUN4I=m CONFIG_DRM_TEGRA=y CONFIG_DRM_PANEL_SAMSUNG_LD9040=m CONFIG_DRM_VC4=y CONFIG_FB_ARMCLCD=y CONFIG_FB_EFI=y CONFIG_FB_WM8505=y CONFIG_FB_SH_MOBILE_LCDC=y CONFIG_FB_SIMPLE=y CONFIG_FB_SH_MOBILE_MERAM=y CONFIG_BACKLIGHT_LCD_SUPPORT=y CONFIG_BACKLIGHT_CLASS_DEVICE=y CONFIG_LCD_PLATFORM=m CONFIG_BACKLIGHT_AS3711=y CONFIG_FRAMEBUFFER_CONSOLE=y CONFIG_FRAMEBUFFER_CONSOLE_ROTATION=y CONFIG_SND_DYNAMIC_MINORS=y CONFIG_SND_HDA_TEGRA=m CONFIG_SND_HDA_INPUT_BEEP=y CONFIG_SND_HDA_PATCH_LOADER=y CONFIG_SND_HDA_CODEC_REALTEK=m CONFIG_SND_HDA_CODEC_HDMI=m CONFIG_SND_USB_AUDIO=m CONFIG_SND_ATMEL_SOC_WM8904=m CONFIG_SND_ATMEL_SOC_PDMIC=m CONFIG_SND_BCM2835_SOC_I2S=m CONFIG_SND_SOC_ROCKCHIP=m CONFIG_SND_SOC_ROCKCHIP_SPDIF=m CONFIG_SND_SOC_ROCKCHIP_MAX98090=m CONFIG_SND_SOC_ROCKCHIP_RT5645=m CONFIG_SND_SOC_SAMSUNG=m CONFIG_SND_SOC_SAMSUNG_SMDK_WM8994=m CONFIG_SND_SOC_SMDK_WM8994_PCM=m CONFIG_SND_SOC_SNOW=m CONFIG_SND_SOC_SH4_FSI=m CONFIG_SND_SOC_RCAR=m CONFIG_SND_SIMPLE_SCU_CARD=m CONFIG_SND_SUN4I_CODEC=m CONFIG_SND_SOC_TEGRA=m CONFIG_SND_SOC_TEGRA20_I2S=m CONFIG_SND_SOC_TEGRA30_I2S=m CONFIG_SND_SOC_TEGRA_RT5640=m CONFIG_SND_SOC_TEGRA_WM8753=m CONFIG_SND_SOC_TEGRA_WM8903=m CONFIG_SND_SOC_TEGRA_WM9712=m CONFIG_SND_SOC_TEGRA_TRIMSLICE=m CONFIG_SND_SOC_TEGRA_ALC5632=m CONFIG_SND_SOC_TEGRA_MAX98090=m CONFIG_SND_SOC_SPDIF=m CONFIG_SND_SOC_STI=m CONFIG_USB_XHCI_HCD=y CONFIG_USB_XHCI_MVEBU=y CONFIG_USB_XHCI_RCAR=m CONFIG_USB_XHCI_TEGRA=m CONFIG_USB_XHCI_PLATFORM=m CONFIG_USB_EHCI_MSM=m CONFIG_USB_EHCI_EXYNOS=y CONFIG_USB_EHCI_TEGRA=y CONFIG_USB_EHCI_HCD_STI=y CONFIG_USB_EHCI_HCD_PLATFORM=y CONFIG_USB_ISP1760=y CONFIG_USB_OHCI_HCD=y CONFIG_USB_OHCI_HCD_STI=y CONFIG_USB_OHCI_HCD_PLATFORM=y CONFIG_USB_OHCI_EXYNOS=m CONFIG_USB_R8A66597_HCD=m CONFIG_USB_RENESAS_USBHS=m CONFIG_USB_STORAGE=y CONFIG_USB_MUSB_SUNXI=m CONFIG_USB_CHIPIDEA_UDC=y CONFIG_USB_CHIPIDEA_HOST=y CONFIG_AB8500_USB=y CONFIG_KEYSTONE_USB_PHY=y CONFIG_USB_GPIO_VBUS=y CONFIG_USB_ISP1301=y CONFIG_USB_MSM_OTG=m CONFIG_USB_MXS_PHY=y CONFIG_USB_FSL_USB2=y CONFIG_USB_RENESAS_USBHS_UDC=m CONFIG_MMC_BLOCK_MINORS=16 CONFIG_MMC_ARMMMCI=y CONFIG_MMC_SDHCI_OF_ARASAN=y CONFIG_MMC_SDHCI_OF_AT91=y CONFIG_MMC_SDHCI_OF_ESDHC=y CONFIG_MMC_SDHCI_ESDHC_IMX=y CONFIG_MMC_SDHCI_DOVE=y CONFIG_MMC_SDHCI_TEGRA=y CONFIG_MMC_SDHCI_PXAV3=y CONFIG_MMC_SDHCI_SPEAR=y CONFIG_MMC_SDHCI_S3C=y CONFIG_MMC_SDHCI_S3C_DMA=y CONFIG_MMC_SDHCI_BCM_KONA=y CONFIG_MMC_SDHCI_ST=y CONFIG_MMC_OMAP=y CONFIG_MMC_ATMELMCI=y CONFIG_MMC_SDHCI_MSM=y CONFIG_MMC_MVSDIO=y CONFIG_MMC_SDHI=y CONFIG_MMC_DW_PLTFM=y CONFIG_MMC_DW_EXYNOS=y CONFIG_MMC_DW_ROCKCHIP=y CONFIG_MMC_SH_MMCIF=y CONFIG_MMC_SUNXI=y CONFIG_MMC_BCM2835=y CONFIG_NEW_LEDS=y CONFIG_LEDS_CLASS_FLASH=m CONFIG_LEDS_GPIO=y CONFIG_LEDS_PWM=y CONFIG_LEDS_MAX77693=m CONFIG_LEDS_MAX8997=m CONFIG_LEDS_TRIGGERS=y CONFIG_LEDS_TRIGGER_TIMER=y CONFIG_LEDS_TRIGGER_ONESHOT=y CONFIG_LEDS_TRIGGER_HEARTBEAT=y CONFIG_LEDS_TRIGGER_BACKLIGHT=y CONFIG_LEDS_TRIGGER_CPU=y CONFIG_LEDS_TRIGGER_GPIO=y CONFIG_LEDS_TRIGGER_DEFAULT_ON=y CONFIG_LEDS_TRIGGER_TRANSIENT=y CONFIG_LEDS_TRIGGER_CAMERA=y CONFIG_EDAC_HIGHBANK_MC=y CONFIG_EDAC_HIGHBANK_L2=y CONFIG_RTC_CLASS=y CONFIG_RTC_DRV_AC100=y CONFIG_RTC_DRV_AS3722=y CONFIG_RTC_DRV_MAX8907=y CONFIG_RTC_DRV_MAX8998=m CONFIG_RTC_DRV_MAX8997=m CONFIG_RTC_DRV_MAX77686=y CONFIG_RTC_DRV_RK808=m CONFIG_RTC_DRV_ST_LPC=y CONFIG_RTC_DRV_DA9063=m CONFIG_RTC_DRV_EFI=m CONFIG_RTC_DRV_DIGICOLOR=m CONFIG_RTC_DRV_S5M=m CONFIG_RTC_DRV_S3C=m CONFIG_RTC_DRV_PL031=y CONFIG_RTC_DRV_AT91RM9200=m CONFIG_RTC_DRV_AT91SAM9=m CONFIG_RTC_DRV_VT8500=y CONFIG_RTC_DRV_SUN6I=y CONFIG_RTC_DRV_SUNXI=y CONFIG_RTC_DRV_MV=y CONFIG_RTC_DRV_TEGRA=y CONFIG_DMADEVICES=y CONFIG_DW_DMAC=y CONFIG_AT_HDMAC=y CONFIG_AT_XDMAC=y CONFIG_FSL_EDMA=y CONFIG_MV_XOR=y CONFIG_TEGRA20_APB_DMA=y CONFIG_SH_DMAE=y CONFIG_RCAR_DMAC=y CONFIG_RENESAS_USB_DMAC=m CONFIG_STE_DMA40=y CONFIG_SIRF_DMA=y CONFIG_TI_EDMA=y CONFIG_PL330_DMA=y CONFIG_IMX_SDMA=y CONFIG_IMX_DMA=y CONFIG_MXS_DMA=y CONFIG_DMA_BCM2835=y CONFIG_DMA_OMAP=y CONFIG_QCOM_BAM_DMA=y CONFIG_XILINX_DMA=y CONFIG_DMA_SUN6I=y CONFIG_ST_FDMA=m CONFIG_SENSORS_ISL29018=y CONFIG_SENSORS_ISL29028=y CONFIG_MFD_NVEC=y CONFIG_KEYBOARD_NVEC=y CONFIG_SERIO_NVEC_PS2=y CONFIG_NVEC_POWER=y CONFIG_NVEC_PAZ00=y CONFIG_BCMA=y CONFIG_BCMA_HOST_SOC=y CONFIG_BCMA_DRIVER_GMAC_CMN=y CONFIG_BCMA_DRIVER_GPIO=y CONFIG_QCOM_GSBI=y CONFIG_QCOM_PM=y CONFIG_QCOM_SMEM=y CONFIG_QCOM_SMD_RPM=y CONFIG_QCOM_SMP2P=y CONFIG_QCOM_SMSM=y CONFIG_QCOM_WCNSS_CTRL=m CONFIG_ROCKCHIP_PM_DOMAINS=y CONFIG_COMMON_CLK_QCOM=y CONFIG_QCOM_CLK_RPM=y CONFIG_STAGING_BOARD=y CONFIG_CROS_EC_CHARDEV=m CONFIG_COMMON_CLK_MAX77686=y CONFIG_COMMON_CLK_RK808=m CONFIG_COMMON_CLK_S2MPS11=m CONFIG_APQ_MMCC_8084=y CONFIG_MSM_GCC_8660=y CONFIG_MSM_MMCC_8960=y CONFIG_MSM_MMCC_8974=y CONFIG_HWSPINLOCK_QCOM=y CONFIG_ROCKCHIP_IOMMU=y CONFIG_TEGRA_IOMMU_GART=y CONFIG_TEGRA_IOMMU_SMMU=y CONFIG_ST_REMOTEPROC=m CONFIG_ARM_TEGRA_DEVFREQ=m CONFIG_MEMORY=y CONFIG_TI_AEMIF=y CONFIG_IIO=y CONFIG_IIO_SW_TRIGGER=y CONFIG_AT91_ADC=m CONFIG_AT91_SAMA5D2_ADC=m CONFIG_BERLIN2_ADC=m CONFIG_EXYNOS_ADC=m CONFIG_VF610_ADC=m CONFIG_XILINX_XADC=y CONFIG_MPU3050_I2C=y CONFIG_CM36651=m CONFIG_AK8975=y CONFIG_RASPBERRYPI_POWER=y CONFIG_IIO_HRTIMER_TRIGGER=y CONFIG_PWM=y CONFIG_PWM_ATMEL=m CONFIG_PWM_ATMEL_HLCDC_PWM=m CONFIG_PWM_ATMEL_TCB=m CONFIG_PWM_FSL_FTM=m CONFIG_PWM_RENESAS_TPU=y CONFIG_PWM_ROCKCHIP=m CONFIG_PWM_SAMSUNG=m CONFIG_PWM_SUN4I=y CONFIG_PWM_TEGRA=y CONFIG_PWM_VT8500=y CONFIG_PHY_HIX5HD2_SATA=y CONFIG_PWM_STI=y CONFIG_PWM_BCM2835=y CONFIG_PWM_BRCMSTB=m CONFIG_GENERIC_PHY=y CONFIG_OMAP_USB2=y CONFIG_TI_PIPE3=y CONFIG_PHY_BERLIN_USB=y CONFIG_PHY_BERLIN_SATA=y CONFIG_PHY_ROCKCHIP_DP=m CONFIG_PHY_ROCKCHIP_USB=y CONFIG_PHY_QCOM_APQ8064_SATA=m CONFIG_PHY_MIPHY28LP=y CONFIG_PHY_RCAR_GEN2=m CONFIG_PHY_STIH407_USB=y CONFIG_PHY_SUN4I_USB=y CONFIG_PHY_SUN9I_USB=y CONFIG_PHY_SAMSUNG_USB2=m CONFIG_PHY_TEGRA_XUSB=y CONFIG_PHY_BRCM_SATA=y CONFIG_NVMEM=y CONFIG_NVMEM_SUNXI_SID=y CONFIG_BCM2835_MBOX=y CONFIG_RASPBERRYPI_FIRMWARE=y CONFIG_EFI_VARS=m CONFIG_EFI_CAPSULE_LOADER=m CONFIG_BCM47XX_NVRAM=y CONFIG_BCM47XX_SPROM=y CONFIG_EXT4_FS=y CONFIG_AUTOFS4_FS=y CONFIG_MSDOS_FS=y CONFIG_VFAT_FS=y CONFIG_NTFS_FS=y CONFIG_TMPFS_POSIX_ACL=y CONFIG_UBIFS_FS=y CONFIG_TMPFS=y CONFIG_SQUASHFS=y CONFIG_SQUASHFS_LZO=y CONFIG_SQUASHFS_XZ=y CONFIG_PSTORE=y CONFIG_PSTORE_CONSOLE=y CONFIG_PSTORE_PMSG=y CONFIG_PSTORE_RAM=y CONFIG_NFS_FS=y CONFIG_NFS_V3_ACL=y CONFIG_NFS_V4=y CONFIG_ROOT_NFS=y CONFIG_NLS_CODEPAGE_437=y CONFIG_NLS_ISO8859_1=y CONFIG_NLS_UTF8=y CONFIG_PRINTK_TIME=y CONFIG_MAGIC_SYSRQ=y CONFIG_KEYSTONE_IRQ=y CONFIG_HW_RANDOM=y CONFIG_HW_RANDOM_ST=y CONFIG_CRYPTO_USER=m CONFIG_CRYPTO_USER_API_RNG=m CONFIG_CRYPTO_USER_API_AEAD=m CONFIG_CRYPTO_DEV_MARVELL_CESA=m CONFIG_CRYPTO_DEV_EXYNOS_RNG=m CONFIG_CRYPTO_DEV_S5P=m CONFIG_CRYPTO_DEV_SUN4I_SS=m CONFIG_CRYPTO_DEV_ROCKCHIP=m CONFIG_ARM_CRYPTO=y CONFIG_CRYPTO_SHA1_ARM=m CONFIG_CRYPTO_SHA1_ARM_CE=m CONFIG_CRYPTO_SHA2_ARM_CE=m CONFIG_CRYPTO_AES_ARM=m CONFIG_CRYPTO_AES_ARM_CE=m CONFIG_CRYPTO_CHACHA20_NEON=m CONFIG_CRYPTO_CRC32_ARM_CE=m CONFIG_CRYPTO_CRCT10DIF_ARM_CE=m CONFIG_CRYPTO_GHASH_ARM_CE=m CONFIG_CRYPTO_DEV_ATMEL_AES=m CONFIG_CRYPTO_DEV_ATMEL_TDES=m CONFIG_CRYPTO_DEV_ATMEL_SHA=m CONFIG_VIDEO_VIVID=m CONFIG_VIRTIO=y CONFIG_VIRTIO_PCI=y CONFIG_VIRTIO_PCI_LEGACY=y CONFIG_VIRTIO_MMIO=y # Add config flags here that only appear in the multi_v7_defconfig CONFIG_ARCH_ALPINE=n CONFIG_ARCH_ARTPEC=n CONFIG_ARCH_AT91=n CONFIG_ARCH_BCM=n CONFIG_ARCH_BCM_CYGNUS=n CONFIG_ARCH_BCM_NSP=n CONFIG_ARCH_BCM_5301X=n CONFIG_ARCH_BCM_281XX=n CONFIG_ARCH_BCM_21664=n CONFIG_ARCH_BRCMSTB=n CONFIG_ARCH_BERLIN=n CONFIG_ARCH_DIGICOLOR=n CONFIG_ARCH_HIGHBANK=n CONFIG_ARCH_HISI=n CONFIG_ARCH_HI3xxx=n CONFIG_ARCH_HIP01=n CONFIG_ARCH_HIP04=n CONFIG_ARCH_HIX5HD2=n CONFIG_ARCH_MESON=n CONFIG_ARCH_MXC=n CONFIG_ARCH_MEDIATEK=n CONFIG_ARCH_QCOM=n CONFIG_ARCH_MSM8X60=n CONFIG_ARCH_MSM8960=n CONFIG_ARCH_MSM8974=n CONFIG_ARCH_ROCKCHIP=n CONFIG_ARCH_SOCFPGA=n CONFIG_ARCH_SPEAR13XX=n CONFIG_ARCH_STI=n CONFIG_ARCH_EXYNOS=n CONFIG_ARCH_SHMOBILE_MULTI=n CONFIG_ARCH_EMEV2=n CONFIG_ARCH_R7S72100=n CONFIG_ARCH_R8A73A4=n CONFIG_ARCH_R8A7740=n CONFIG_ARCH_R8A7778=n CONFIG_ARCH_R8A7779=n CONFIG_ARCH_R8A7790=n CONFIG_ARCH_R8A7791=n CONFIG_ARCH_R8A7793=n CONFIG_ARCH_R8A7794=n CONFIG_ARCH_RENESAS=n CONFIG_ARCH_SH73A0=n CONFIG_ARCH_SUNXI=n CONFIG_ARCH_SIRF=n CONFIG_ARCH_TEGRA=n CONFIG_ARCH_TEGRA_2x_SOC=n CONFIG_ARCH_TEGRA_3x_SOC=n CONFIG_ARCH_TEGRA_114_SOC=n CONFIG_ARCH_TEGRA_124_SOC=n CONFIG_ARCH_UNIPHIER=n CONFIG_ARCH_U8500=n CONFIG_ARCH_VEXPRESS=n CONFIG_ARCH_VEXPRESS_TC2_PM=n CONFIG_ARCH_WM8850=n CONFIG_ARCH_ZYNQ=n CONFIG_ARCH_VIRT=n CONFIG_ARCH_MVEBU=n CONFIG_PLAT_SPEAR=n CONFIG_CHROME_PLATFORMS=n ################################################## # TI Baseport Config Options ################################################## # Kernel compression CONFIG_KERNEL_GZIP=n CONFIG_KERNEL_LZMA=y CONFIG_KERNEL_LZ4=n CONFIG_KERNEL_XZ=n CONFIG_KERNEL_LZO=n # Enable process accounting CONFIG_BSD_PROCESS_ACCT=y # Have some way to pick up kernel config later on # Always useful to look at /proc/config.gz CONFIG_IKCONFIG=y CONFIG_IKCONFIG_PROC=y # Add Bin2c CONFIG_BUILD_BIN2C=y # Add base Cgroups functions CONFIG_CGROUP_DEBUG=n CONFIG_CPUSETS=y CONFIG_PROC_PID_CPUSET=y CONFIG_PAGE_COUNTER=y CONFIG_MEMCG=y CONFIG_MEMCG_SWAP=y CONFIG_MEMCG_SWAP_ENABLED=y CONFIG_DEBUG_BLK_CGROUP=n CONFIG_CGROUP_WRITEBACK=y # Choose CONFIG_EMBEDDED CONFIG_EMBEDDED=y CONFIG_EXPERT=y CONFIG_ARM_PATCH_PHYS_VIRT=y # Enable all kernel symbols please CONFIG_KALLSYMS=y CONFIG_KALLSYMS_ALL=y # Enable AEABI CONFIG_AEABI=y # How do we want kernel Modules to work? CONFIG_BASE_FULL=y CONFIG_BASE_SMALL=0 CONFIG_MODULES=y CONFIG_MODULE_FORCE_LOAD=y CONFIG_MODULE_UNLOAD=y CONFIG_MODULE_FORCE_UNLOAD=y CONFIG_MODVERSIONS=y CONFIG_MODULE_SRCVERSION_ALL=y CONFIG_MODULE_SIG=n CONFIG_MODULE_COMPRESS=n CONFIG_MODULES_TREE_LOOKUP=y # Boot options CONFIG_USE_OF=y CONFIG_ATAGS=y CONFIG_DEPRECATED_PARAM_STRUCT=n CONFIG_ZBOOT_ROM_TEXT=0x0 CONFIG_ZBOOT_ROM_BSS=0x0 CONFIG_ARM_APPENDED_DTB=y CONFIG_ARM_ATAG_DTB_COMPAT=y CONFIG_ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER=y CONFIG_ARM_ATAG_DTB_COMPAT_CMDLINE_EXTEND=n CONFIG_CMDLINE="" CONFIG_CMDLINE_FROM_BOOTLOADER=y CONFIG_CMDLINE_EXTEND=n CONFIG_CMDLINE_FORCE=n CONFIG_ATAGS_PROC=y CONFIG_CRASH_DUMP=n CONFIG_AUTO_ZRELADDR=y # Mem allocator CONFIG_SLAB=n CONFIG_SLUB=y # Enable NEON CONFIG_VFP=y CONFIG_NEON=y CONFIG_KERNEL_MODE_NEON=y # POSIX Message queue CONFIG_POSIX_MQUEUE=y # No Multi Cluster systems in TI yet.. CONFIG_MCPM=n # Serial CONFIG_SERIAL_8250_OMAP=y CONFIG_SERIAL_8250_OMAP_TTYO_FIXUP=y CONFIG_SERIAL_8250_NR_UARTS=10 CONFIG_SERIAL_8250_RUNTIME_UARTS=10 CONFIG_SERIAL_8250_DMA=y CONFIG_SERIAL_OMAP=n CONFIG_SERIAL_8250_DW=n CONFIG_SERIAL_8250_EM=n CONFIG_SERIAL_AMBA_PL011=n CONFIG_SERIAL_XILINX_PS_UART=n CONFIG_SERIAL_FSL_LPUART=n CONFIG_SERIAL_CONEXANT_DIGICOLOR=n CONFIG_SERIAL_ST_ASC=n CONFIG_JUMP_LABEL=y # Disable Extra debug options CONFIG_TIMER_STATS=n CONFIG_DEBUG_SPINLOCK=n CONFIG_DEBUG_MUTEXES=n CONFIG_DEBUG_LOCK_ALLOC=n CONFIG_PROVE_LOCKING=n CONFIG_LOCKDEP=n CONFIG_STACKTRACE=n CONFIG_FTRACE=n CONFIG_ARM_UNWIND=n CONFIG_DEBUG_PREEMPT=n CONFIG_SLUB_DEBUG=n CONFIG_LOCKUP_DETECTOR=n CONFIG_DETECT_HUNG_TASK=n CONFIG_IRQ_DOMAIN_DEBUG=n CONFIG_DEBUG_BUGVERBOSE=n CONFIG_DEBUG_FS=y # Enable System V IPC CONFIG_SYSVIPC=y # Power management options CONFIG_SUSPEND_FREEZER=y CONFIG_SUSPEND_SKIP_SYNC=n CONFIG_HIBERNATION=n CONFIG_PM_SLEEP=y CONFIG_PM_SLEEP_SMP=y CONFIG_PM_AUTOSLEEP=n CONFIG_PM_WAKELOCKS=n CONFIG_PM=y CONFIG_PM_DEBUG=y CONFIG_APM_EMULATION=n CONFIG_PM_OPP=y CONFIG_PM_CLK=y CONFIG_PM_GENERIC_DOMAINS=y CONFIG_WQ_POWER_EFFICIENT_DEFAULT=n CONFIG_PM_GENERIC_DOMAINS_SLEEP=y CONFIG_PM_GENERIC_DOMAINS_OF=y CONFIG_CPU_PM=y CONFIG_ARCH_SUSPEND_POSSIBLE=y CONFIG_ARM_CPU_SUSPEND=y CONFIG_ARCH_HIBERNATION_POSSIBLE=y # Clock framework stuff we need CONFIG_CLKDEV_LOOKUP=y CONFIG_HAVE_CLK_PREPARE=y CONFIG_COMMON_CLK=y CONFIG_COMMON_CLK_SI5351=n CONFIG_COMMON_CLK_SI514=n CONFIG_COMMON_CLK_SI570=n CONFIG_COMMON_CLK_CDCE925=n CONFIG_CLK_TWL6040=n CONFIG_CLK_QORIQ=n CONFIG_COMMON_CLK_PALMAS=y CONFIG_COMMON_CLK_PWM=n CONFIG_COMMON_CLK_PXA=n CONFIG_COMMON_CLK_CDCE706=n CONFIG_CLKSRC_OF=y CONFIG_CLKSRC_PROBE=y CONFIG_CLKSRC_MMIO=y CONFIG_CLKSRC_TI_32K=y CONFIG_ARM_ARCH_TIMER=y CONFIG_ARM_ARCH_TIMER_EVTSTREAM=y CONFIG_ARM_GLOBAL_TIMER=n CONFIG_ARM_TIMER_SP804=n # Clock cleanup please CONFIG_OMAP_RESET_CLOCKS=y # CPU Idle CONFIG_CPU_IDLE_GOV_LADDER=y CONFIG_CPU_IDLE_GOV_MENU=y CONFIG_DT_IDLE_STATES=y # ARM CPU Idle Drivers CONFIG_ARM_CPUIDLE=y CONFIG_ARCH_NEEDS_CPU_IDLE_COUPLED=n # CPU Frequency scaling CONFIG_CPU_FREQ_GOV_COMMON=y CONFIG_CPU_FREQ_STAT=y CONFIG_CPU_FREQ_STAT_DETAILS=y CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND=y CONFIG_CPU_FREQ_GOV_PERFORMANCE=y CONFIG_CPU_FREQ_GOV_POWERSAVE=y CONFIG_CPU_FREQ_GOV_USERSPACE=y CONFIG_CPU_FREQ_GOV_ONDEMAND=y CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y # CPUFreq Driver Options CONFIG_CPUFREQ_DT=y CONFIG_ARM_BIG_LITTLE_CPUFREQ=n CONFIG_ARM_KIRKWOOD_CPUFREQ=n CONFIG_ARM_OMAP2PLUS_CPUFREQ=n CONFIG_ARM_TI_CPUFREQ=y CONFIG_QORIQ_CPUFREQ=n # AMx3 Power Config Options CONFIG_MAILBOX=y CONFIG_WKUP_M3_RPROC=m CONFIG_SOC_TI=y CONFIG_SOC_BRCMSTB=n CONFIG_WKUP_M3_IPC=m CONFIG_AMX3_PM=m CONFIG_SRAM=y CONFIG_TI_EMIF_SRAM=m CONFIG_SUNXI_SRAM=n CONFIG_PM_DEVFREQ=n # K2G Power config options # CONFIG_MAILBOX is enabled in AMx3 CONFIG_TI_MESSAGE_MANAGER=y CONFIG_TI_SCI_PROTOCOL=y CONFIG_TI_SCI_PM_DOMAINS=y CONFIG_TI_SCI_CLK=y # Enable Reset Controllers CONFIG_RESET_CONTROLLER=y CONFIG_RESET_TI_SYSCON=y CONFIG_RESET_TI_SCI=y # CPUFreq and OPP drivers CONFIG_OPP_DOMAIN_TI=y # Thermal CONFIG_THERMAL=y CONFIG_THERMAL_OF=y CONFIG_THERMAL_WRITABLE_TRIPS=y CONFIG_THERMAL_DEFAULT_GOV_STEP_WISE=y CONFIG_THERMAL_GOV_FAIR_SHARE=y CONFIG_THERMAL_GOV_STEP_WISE=y CONFIG_THERMAL_GOV_BANG_BANG=y CONFIG_THERMAL_GOV_USER_SPACE=y CONFIG_THERMAL_GOV_POWER_ALLOCATOR=y CONFIG_CPU_THERMAL=y CONFIG_TI_SOC_THERMAL=y CONFIG_TI_THERMAL=y CONFIG_OMAP4_THERMAL=y CONFIG_OMAP5_THERMAL=y CONFIG_DRA752_THERMAL=y # Since HWMON is needed by Sensors.. CONFIG_HWMON=y CONFIG_SENSORS_TMP102=y CONFIG_SENSORS_GPIO_FAN=y # Enable the reset framework CONFIG_POWER_RESET=y CONFIG_POWER_SUPPLY=y # Pinctrl CONFIG_PINCTRL_TI_IODELAY=y CONFIG_PINCTRL_SINGLE=y # # Multifunction device drivers CONFIG_MFD_CORE=y CONFIG_MFD_AS3711=n CONFIG_MFD_AS3722=n CONFIG_PMIC_ADP5520=n CONFIG_MFD_AAT2870_CORE=n CONFIG_MFD_ATMEL_FLEXCOM=n CONFIG_MFD_ATMEL_HLCDC=n CONFIG_MFD_BCM590XX=n CONFIG_MFD_AXP20X=n CONFIG_MFD_AXP20X_I2C=n CONFIG_MFD_CROS_EC=n CONFIG_MFD_CROS_EC_I2C=n CONFIG_MFD_CROS_EC_SPI=n CONFIG_MFD_ASIC3=n CONFIG_PMIC_DA903X=n CONFIG_MFD_DA9052_SPI=n CONFIG_MFD_DA9052_I2C=n CONFIG_MFD_DA9055=n CONFIG_MFD_DA9062=n CONFIG_MFD_DA9063=n CONFIG_MFD_DA9150=n CONFIG_MFD_DLN2=n CONFIG_MFD_MC13XXX_SPI=n CONFIG_MFD_MC13XXX_I2C=n CONFIG_MFD_HI6421_PMIC=n CONFIG_HTC_EGPIO=n CONFIG_HTC_PASIC3=n CONFIG_HTC_I2CPLD=n CONFIG_LPC_ICH=n CONFIG_LPC_SCH=n CONFIG_INTEL_SOC_PMIC=n CONFIG_MFD_JANZ_CMODIO=n CONFIG_MFD_KEMPLD=n CONFIG_MFD_88PM800=n CONFIG_MFD_88PM805=n CONFIG_MFD_88PM860X=n CONFIG_MFD_MAX14577=n CONFIG_MFD_MAX77686=n CONFIG_MFD_MAX77693=n CONFIG_MFD_MAX77843=n CONFIG_MFD_MAX8907=n CONFIG_MFD_MAX8925=n CONFIG_MFD_MAX8997=n CONFIG_MFD_MAX8998=n CONFIG_MFD_MT6397=n CONFIG_MFD_MENF21BMC=n CONFIG_EZX_PCAP=n CONFIG_MFD_VIPERBOARD=n CONFIG_MFD_RETU=n CONFIG_MFD_PCF50633=n CONFIG_MFD_PM8XXX=n CONFIG_MFD_PM8921_CORE=n CONFIG_MFD_RDC321X=n CONFIG_MFD_RTSX_PCI=n CONFIG_MFD_RT5033=n CONFIG_MFD_RTSX_USB=n CONFIG_MFD_RC5T583=n CONFIG_MFD_RK808=n CONFIG_MFD_RN5T618=n CONFIG_MFD_SEC_CORE=n CONFIG_MFD_SI476X_CORE=n CONFIG_MFD_SM501=n CONFIG_MFD_SKY81452=n CONFIG_MFD_SMSC=n CONFIG_ABX500_CORE=n CONFIG_AB3100_CORE=n CONFIG_MFD_STMPE=n CONFIG_STMPE_I2C=n CONFIG_STMPE_SPI=n CONFIG_MFD_SYSCON=y CONFIG_MFD_TI_AM335X_TSCADC=m CONFIG_MFD_LP3943=n CONFIG_MFD_LP8788=n CONFIG_MFD_OMAP_USB_HOST=y CONFIG_MFD_PALMAS=y CONFIG_TPS6105X=n CONFIG_TPS65010=n CONFIG_TPS6507X=n CONFIG_MFD_TPS65086=n CONFIG_MFD_TPS65090=y CONFIG_MFD_TPS65217=y CONFIG_MFD_TPS65218=y CONFIG_MFD_TPS6586X=y CONFIG_MFD_TPS65910=y CONFIG_MFD_TPS65912_I2C=n CONFIG_MFD_TPS65912_SPI=n CONFIG_MFD_TPS80031=n CONFIG_TWL4030_CORE=n CONFIG_TWL4030_POWER=n CONFIG_MFD_TWL4030_AUDIO=n CONFIG_TWL6040_CORE=y CONFIG_MFD_WL1273_CORE=n CONFIG_MFD_LM3533=n CONFIG_MFD_TI_LP873X=y CONFIG_MFD_TI_LP87565=y CONFIG_MFD_TC3589X=n CONFIG_MFD_TMIO=n CONFIG_MFD_T7L66XB=n CONFIG_MFD_TC6387XB=n CONFIG_MFD_TC6393XB=n CONFIG_MFD_VX855=n CONFIG_MFD_ARIZONA_I2C=n CONFIG_MFD_ARIZONA_SPI=n CONFIG_MFD_WM8400=n CONFIG_MFD_WM831X_I2C=n CONFIG_MFD_WM831X_SPI=n CONFIG_MFD_WM8350_I2C=n CONFIG_MFD_WM8994=n CONFIG_MFD_VEXPRESS_SYSREG=n # Regulators CONFIG_REGULATOR=y CONFIG_REGULATOR_FIXED_VOLTAGE=y CONFIG_REGULATOR_DEBUG=n CONFIG_REGULATOR_VIRTUAL_CONSUMER=n CONFIG_REGULATOR_USERSPACE_CONSUMER=n CONFIG_REGULATOR_ACT8865=n CONFIG_REGULATOR_AD5398=n CONFIG_REGULATOR_ANATOP=n CONFIG_REGULATOR_AS3711=n CONFIG_REGULATOR_AS3722=n CONFIG_REGULATOR_AXP20X=n CONFIG_REGULATOR_BCM590XX=n CONFIG_REGULATOR_DA9210=n CONFIG_REGULATOR_DA9211=n CONFIG_REGULATOR_FAN53555=n CONFIG_REGULATOR_GPIO=y CONFIG_REGULATOR_ISL9305=n CONFIG_REGULATOR_ISL6271A=n CONFIG_REGULATOR_LP3971=n CONFIG_REGULATOR_LP3972=n CONFIG_REGULATOR_LP872X=n CONFIG_REGULATOR_LP8755=n CONFIG_REGULATOR_LP873X=y CONFIG_REGULATOR_LP87565=y CONFIG_REGULATOR_LTC3589=n CONFIG_REGULATOR_MAX14577=n CONFIG_REGULATOR_MAX1586=n CONFIG_REGULATOR_MAX8649=n CONFIG_REGULATOR_MAX8660=n CONFIG_REGULATOR_MAX8907=n CONFIG_REGULATOR_MAX8952=n CONFIG_REGULATOR_MAX8973=n CONFIG_REGULATOR_MAX77686=n CONFIG_REGULATOR_MAX77693=n CONFIG_REGULATOR_MAX77802=n CONFIG_REGULATOR_MT6311=n CONFIG_REGULATOR_PALMAS=y CONFIG_REGULATOR_PBIAS=y CONFIG_REGULATOR_PFUZE100=n CONFIG_REGULATOR_PWM=n CONFIG_REGULATOR_RK808=n CONFIG_REGULATOR_S2MPA01=n CONFIG_REGULATOR_S2MPS11=n CONFIG_REGULATOR_S5M8767=n CONFIG_REGULATOR_TI_ABB=y CONFIG_REGULATOR_TPS51632=n CONFIG_REGULATOR_TPS62360=y CONFIG_REGULATOR_TPS65023=y CONFIG_REGULATOR_TPS6507X=y CONFIG_REGULATOR_TPS65090=y CONFIG_REGULATOR_TPS65217=y CONFIG_REGULATOR_TPS65218=y CONFIG_REGULATOR_TPS6524X=y CONFIG_REGULATOR_TPS6586X=y CONFIG_REGULATOR_TPS65910=y CONFIG_REGULATOR_TWL4030=n CONFIG_REGULATOR_VEXPRESS=n # Crypto Modules CONFIG_CRYPTO_DEV_OMAP=m CONFIG_CRYPTO_DEV_OMAP_SHAM=m CONFIG_CRYPTO_DEV_OMAP_AES=m CONFIG_CRYPTO_DEV_OMAP_DES=m CONFIG_CRYPTO_USER_API_HASH=m CONFIG_CRYPTO_USER_API_SKCIPHER=m CONFIG_CRYPTO_SHA1_ARM_NEON=m CONFIG_CRYPTO_SHA256_ARM=m CONFIG_CRYPTO_SHA512_ARM=m CONFIG_CRYPTO_AES_ARM_BS=m # # RTC drivers # CONFIG_RTC_DRV_ABB5ZES3=n CONFIG_RTC_DRV_ABX80X=n CONFIG_RTC_DRV_DS1307=m CONFIG_RTC_DRV_DS1374=n CONFIG_RTC_DRV_DS1672=n CONFIG_RTC_DRV_DS3232=n CONFIG_RTC_DRV_HYM8563=n CONFIG_RTC_DRV_MAX6900=n CONFIG_RTC_DRV_RS5C372=n CONFIG_RTC_DRV_ISL1208=n CONFIG_RTC_DRV_ISL12022=n CONFIG_RTC_DRV_ISL12057=n CONFIG_RTC_DRV_X1205=n CONFIG_RTC_DRV_PALMAS=m CONFIG_RTC_DRV_PCF2127=n CONFIG_RTC_DRV_PCF8523=n CONFIG_RTC_DRV_PCF8563=n CONFIG_RTC_DRV_PCF85063=n CONFIG_RTC_DRV_PCF8583=n CONFIG_RTC_DRV_M41T80=n CONFIG_RTC_DRV_BQ32K=n CONFIG_RTC_DRV_TPS6586X=m CONFIG_RTC_DRV_TPS65910=m CONFIG_RTC_DRV_TWL92330=y CONFIG_RTC_DRV_TWL4030=n CONFIG_RTC_DRV_S35390A=n CONFIG_RTC_DRV_FM3130=n CONFIG_RTC_DRV_RX8581=n CONFIG_RTC_DRV_RX8025=n CONFIG_RTC_DRV_EM3027=n CONFIG_RTC_DRV_RV3029C2=n CONFIG_RTC_DRV_RV8803=n CONFIG_RTC_DRV_M41T93=n CONFIG_RTC_DRV_M41T94=n CONFIG_RTC_DRV_DS1305=n CONFIG_RTC_DRV_DS1343=n CONFIG_RTC_DRV_DS1347=n CONFIG_RTC_DRV_DS1390=n CONFIG_RTC_DRV_MAX6902=n CONFIG_RTC_DRV_R9701=n CONFIG_RTC_DRV_RS5C348=n CONFIG_RTC_DRV_DS3234=n CONFIG_RTC_DRV_PCF2123=n CONFIG_RTC_DRV_RX4581=n CONFIG_RTC_DRV_MCP795=n CONFIG_RTC_DRV_CMOS=n CONFIG_RTC_DRV_DS1286=n CONFIG_RTC_DRV_DS1511=n CONFIG_RTC_DRV_DS1553=n CONFIG_RTC_DRV_DS1685_FAMILY=n CONFIG_RTC_DRV_DS1742=n CONFIG_RTC_DRV_DS2404=n CONFIG_RTC_DRV_STK17TA8=n CONFIG_RTC_DRV_M48T86=n CONFIG_RTC_DRV_M48T35=n CONFIG_RTC_DRV_M48T59=n CONFIG_RTC_DRV_MSM6242=n CONFIG_RTC_DRV_BQ4802=n CONFIG_RTC_DRV_RP5C01=n CONFIG_RTC_DRV_V3020=n CONFIG_RTC_DRV_ZYNQMP=n CONFIG_RTC_DRV_OMAP=m CONFIG_RTC_DRV_SNVS=n CONFIG_RTC_DRV_HID_SENSOR_TIME=n # WatchDog CONFIG_WATCHDOG=y CONFIG_WATCHDOG_CORE=y CONFIG_WATCHDOG_NOWAYOUT=n # Watchdog Device Drivers CONFIG_SOFT_WATCHDOG=n CONFIG_GPIO_WATCHDOG=n CONFIG_XILINX_WATCHDOG=n CONFIG_CADENCE_WATCHDOG=n CONFIG_DW_WATCHDOG=n CONFIG_OMAP_WATCHDOG=m CONFIG_TWL4030_WATCHDOG=m CONFIG_MAX63XX_WATCHDOG=n CONFIG_ALIM7101_WDT=n CONFIG_I6300ESB_WDT=n CONFIG_BCM7038_WDT=n CONFIG_MEN_A21_WDT=n # No Staging drivers please CONFIG_STAGING=n # GPIO CONFIG_GPIOLIB=y CONFIG_GPIO_SYSFS=y CONFIG_DEBUG_GPIO=y # GPIO disable unused options CONFIG_GPIO_DWAPB=n CONFIG_GPIO_EM=n CONFIG_GPIO_GENERIC_PLATFORM=n CONFIG_GPIO_XILINX=n CONFIG_GPIO_TPS6586X=n # Enable options to facilitate testing CONFIG_CRYPTO_TEST=m CONFIG_RTC_DEBUG=y CONFIG_THERMAL_EMULATION=y # OPTEE Driver CONFIG_TEE=y CONFIG_OPTEE=y ################################################## # TI RPMsg/IPC Config Options ################################################## # HwSpinLock CONFIG_HWSPINLOCK=y CONFIG_HWSPINLOCK_OMAP=y # Mailbox CONFIG_OMAP2PLUS_MBOX=y # IOMMU CONFIG_IOMMU_SUPPORT=y CONFIG_OMAP_IOMMU=y CONFIG_OMAP_IOMMU_DEBUG=y # Remoteproc CONFIG_REMOTEPROC=m CONFIG_OMAP_REMOTEPROC=m CONFIG_KEYSTONE_REMOTEPROC=m CONFIG_DA8XX_REMOTEPROC=m CONFIG_PRUSS_REMOTEPROC=m # RPMsg CONFIG_RPMSG_VIRTIO=y CONFIG_RPMSG_PROTO=y CONFIG_RPMSG_RPC=y CONFIG_RPMSG_PRU=y # DSP Memory Mapper for Keystone MPM CONFIG_KEYSTONE_DSP_MEM=m # UIO Module CONFIG_UIO=m ################################################## # TI Connectivity Configs ################################################## # Disable unused I2C options CONFIG_I2C_MUX=n CONFIG_I2C_DESIGNWARE_PLATFORM=n CONFIG_I2C_GPIO=n CONFIG_I2C_RK3X=n CONFIG_I2C_XILINX=n # I2C GPIO expanders CONFIG_GPIO_PCF857X=y CONFIG_GPIO_TPIC2810=m #Networking drivers CONFIG_NET_VENDOR_TI=y CONFIG_KEYSTONE_NAVIGATOR_QMSS=y CONFIG_KEYSTONE_NAVIGATOR_DMA=y CONFIG_TI_KEYSTONE_NETCP=y CONFIG_TI_KEYSTONE_NETCP_ETHSS=y CONFIG_TI_DAVINCI_EMAC=y CONFIG_TI_DAVINCI_MDIO=y CONFIG_TI_DAVINCI_CPDMA=y CONFIG_TI_CPSW_PHY_SEL=y CONFIG_TI_CPSW_ALE=y CONFIG_TI_CPSW=y CONFIG_TI_CPTS=y # non-TI Net vendors CONFIG_NET_DSA_BCM_SF2=n CONFIG_B53=n CONFIG_SYSTEMPORT=n CONFIG_NET_VENDOR_3COM=n CONFIG_NET_VENDOR_ADAPTEC=n CONFIG_NET_VENDOR_AGERE=n CONFIG_NET_VENDOR_ALTEON=n CONFIG_NET_VENDOR_AMAZON=n CONFIG_NET_VENDOR_AMD=n CONFIG_NET_VENDOR_ARC=n CONFIG_NET_VENDOR_ATHEROS=n CONFIG_NET_VENDOR_BROCADE=n CONFIG_NET_VENDOR_CAVIUM=n CONFIG_NET_VENDOR_CHELSIO=n CONFIG_NET_CADENCE=n CONFIG_BCMGENET=n CONFIG_NET_VENDOR_CIRRUS=n CONFIG_NET_VENDOR_CISCO=n CONFIG_NET_VENDOR_DEC=n CONFIG_NET_VENDOR_DLINK=n CONFIG_NET_VENDOR_EMULEX=n CONFIG_NET_VENDOR_EZCHIP=n CONFIG_NET_VENDOR_EXAR=n CONFIG_NET_VENDOR_FARADAY=n CONFIG_NET_VENDOR_HISILICON=n CONFIG_NET_VENDOR_HP=n CONFIG_IGB=n CONFIG_NET_VENDOR_I825XX=n CONFIG_NET_VENDOR_MELLANOX=n CONFIG_NET_VENDOR_MICROCHIP=n CONFIG_NET_VENDOR_MYRI=n CONFIG_NET_VENDOR_NATSEMI=n CONFIG_NET_VENDOR_NETRONOME=n CONFIG_NET_VENDOR_NVIDIA=n CONFIG_NET_VENDOR_OKI=n CONFIG_NET_VENDOR_8390=n CONFIG_NET_VENDOR_QLOGIC=n CONFIG_NET_VENDOR_QUALCOMM=n CONFIG_NET_VENDOR_REALTEK=n CONFIG_NET_VENDOR_RENESAS=n CONFIG_NET_VENDOR_RDC=n CONFIG_NET_VENDOR_ROCKER=n CONFIG_NET_VENDOR_SAMSUNG=n CONFIG_NET_VENDOR_SILAN=n CONFIG_NET_VENDOR_SIS=n CONFIG_NET_VENDOR_SEEQ=n CONFIG_NET_VENDOR_STMICRO=n CONFIG_NET_VENDOR_SUN=n CONFIG_NET_VENDOR_SYNOPSYS=n CONFIG_NET_VENDOR_TEHUTI=n CONFIG_NET_VENDOR_VIA=n CONFIG_NET_VENDOR_WIZNET=n #Wireless LAN CONFIG_WLCORE=m CONFIG_WLCORE_SDIO=m CONFIG_WL18XX=m #MDIO phys CONFIG_MARVELL_PHY=y CONFIG_MICREL_PHY=y # unused PHY drivers CONFIG_BROADCOM_PHY=n CONFIG_ICPLUS_PHY=n #PRU MII PHYs for Industrial Boards CONFIG_DP83848_PHY=y # Enable phy for DRA72 evm CONFIG_DP83867_PHY=y #MTD CONFIG_OMAP_GPMC=y CONFIG_MTD_NAND_OMAP2=y CONFIG_MTD_NAND_OMAP_BCH=y CONFIG_MTD_NAND_OMAP_BCH_BUILD=y CONFIG_MTD_TESTS=m CONFIG_MTD_CMDLINE_PARTS=y #PCIE CONFIG_PCI=y CONFIG_PCI_ENDPOINT=y CONFIG_PCI_ENDPOINT_CONFIGFS=y CONFIG_PCI_EPF_TEST=y CONFIG_PCI_ENDPOINT_TEST=m CONFIG_PCI_DRA7XX=y CONFIG_PCI_DRA7XX_HOST=y CONFIG_PCI_DRA7XX_EP=y CONFIG_PCI_KEYSTONE_EP=y #These drivers have been used with DRA7x/AM57x PCIe RC with some success CONFIG_NET_VENDOR_BROADCOM=y CONFIG_NET_VENDOR_MARVELL=y CONFIG_NET_VENDOR_INTEL=y CONFIG_TIGON3=m CONFIG_SKGE=m CONFIG_E1000=m CONFIG_E1000E=m CONFIG_IWLWIFI=m CONFIG_IWLDVM=m CONFIG_IWLMVM=m #Generic Phys CONFIG_PHY_TI_KEYSTONE_SERDES=y # Networking CONFIG_HSR_PRP=y CONFIG_NF_CONNTRACK=m CONFIG_NF_CONNTRACK_IPV4=m CONFIG_IP_NF_IPTABLES=m CONFIG_IP_NF_ARPTABLES=m CONFIG_IP_NF_ARPFILTER=m CONFIG_IP_NF_ARP_MANGLE=m CONFIG_IP_NF_FILTER=m CONFIG_IP_NF_NAT=m CONFIG_NF_NAT_IPV4=m CONFIG_IP_NF_TARGET_MASQUERADE=m CONFIG_BRIDGE=m CONFIG_XFRM_USER=m CONFIG_NET_KEY=m CONFIG_INET=y CONFIG_INET_AH=m CONFIG_INET6_AH=m CONFIG_INET6_IPCOMP=m CONFIG_INET6_XFRM_TUNNEL=m CONFIG_INET6_TUNNEL=m CONFIG_INET_ESP=m CONFIG_INET_IPCOMP=m CONFIG_INET_XFRM_MODE_TRANSPORT=m CONFIG_INET_XFRM_MODE_TUNNEL=m CONFIG_INET_XFRM_MODE_BEET=m CONFIG_IPV6_TUNNEL=m CONFIG_NETFILTER=y CONFIG_NETFILTER_XTABLES=m CONFIG_NETFILTER_XT_TARGET_CLASSIFY=m CONFIG_NETFILTER_XT_TARGET_IDLETIMER=m CONFIG_NETFILTER_XT_TARGET_MARK=m CONFIG_NETFILTER_XT_MATCH_COMMENT=m CONFIG_NETFILTER_XT_MATCH_CPU=m CONFIG_NETFILTER_XT_MATCH_IPRANGE=m CONFIG_NETFILTER_XT_MATCH_LENGTH=m CONFIG_NETFILTER_XT_MATCH_LIMIT=m CONFIG_NETFILTER_XT_MATCH_MAC=m CONFIG_NETFILTER_XT_MATCH_MARK=m CONFIG_NETFILTER_XT_MATCH_MULTIPORT=m CONFIG_NETFILTER_XT_MATCH_PKTTYPE=m CONFIG_NETFILTER_XT_MATCH_POLICY=m CONFIG_NETFILTER_XT_MATCH_SCTP=m CONFIG_BRIDGE_NF_EBTABLES=m CONFIG_BRIDGE_EBT_BROUTE=m CONFIG_BRIDGE_EBT_T_FILTER=m CONFIG_BRIDGE_EBT_T_NAT=m CONFIG_BRIDGE_EBT_802_3=m CONFIG_BRIDGE_EBT_AMONG=m CONFIG_BRIDGE_EBT_ARP=m CONFIG_BRIDGE_EBT_IP=m CONFIG_BRIDGE_EBT_IP6=m CONFIG_BRIDGE_EBT_LIMIT=m CONFIG_BRIDGE_EBT_MARK=m CONFIG_BRIDGE_EBT_PKTTYPE=m CONFIG_BRIDGE_EBT_STP=m CONFIG_BRIDGE_EBT_VLAN=m CONFIG_BRIDGE_EBT_ARPREPLY=m CONFIG_BRIDGE_EBT_DNAT=m CONFIG_BRIDGE_EBT_MARK_T=m CONFIG_BRIDGE_EBT_REDIRECT=m CONFIG_BRIDGE_EBT_SNAT=m CONFIG_BRIDGE_EBT_LOG=m CONFIG_BRIDGE_EBT_NFLOG=m CONFIG_NET_SCHED=y CONFIG_NET_SCH_CBQ=m CONFIG_NET_SCH_HTB=m CONFIG_NET_SCH_HFSC=m CONFIG_NET_SCH_PRIO=m CONFIG_NET_SCH_MULTIQ=m CONFIG_NET_SCH_RED=m CONFIG_NET_SCH_SFB=m CONFIG_NET_SCH_SFQ=m CONFIG_NET_SCH_TEQL=m CONFIG_NET_SCH_TBF=m CONFIG_NET_SCH_GRED=m CONFIG_NET_SCH_DSMARK=m CONFIG_NET_SCH_NETEM=m CONFIG_NET_SCH_DRR=m CONFIG_NET_SCH_MQPRIO=m CONFIG_NET_SCH_CHOKE=m CONFIG_NET_SCH_QFQ=m CONFIG_NET_SCH_CODEL=m CONFIG_NET_SCH_FQ_CODEL=m CONFIG_NET_SCH_INGRESS=m CONFIG_NET_CLS=y CONFIG_NET_CLS_BASIC=m CONFIG_NET_CLS_TCINDEX=m CONFIG_NET_CLS_ROUTE4=m CONFIG_NET_CLS_FW=m CONFIG_NET_CLS_U32=m CONFIG_CLS_U32_MARK=y CONFIG_NET_CLS_RSVP=m CONFIG_NET_CLS_RSVP6=m CONFIG_NET_CLS_FLOW=m CONFIG_NET_EMATCH=y CONFIG_NET_EMATCH_STACK=32 CONFIG_NET_EMATCH_CMP=m CONFIG_NET_EMATCH_NBYTE=m CONFIG_NET_EMATCH_U32=m CONFIG_NET_EMATCH_META=m CONFIG_NET_EMATCH_TEXT=m CONFIG_NET_CLS_ACT=y CONFIG_NET_ACT_POLICE=m CONFIG_NET_ACT_GACT=m CONFIG_GACT_PROB=y CONFIG_NET_ACT_MIRRED=m CONFIG_NET_ACT_IPT=m CONFIG_NET_ACT_NAT=m CONFIG_NET_ACT_PEDIT=m CONFIG_NET_ACT_SIMP=m CONFIG_NET_ACT_SKBEDIT=m CONFIG_NET_ACT_CSUM=m CONFIG_NET_CLS_IND=y CONFIG_NET_SCH_FIFO=y CONFIG_IP_SCTP=m CONFIG_VLAN_8021Q=m CONFIG_IP_MULTICAST=y #PRUSS Ethernet driver CONFIG_TI_PRUETH=m #MMC/SD support CONFIG_MMC=y CONFIG_MMC_SDHCI=y CONFIG_MMC_SDHCI_PLTFM=y CONFIG_MMC_OMAP_HS=y CONFIG_MMC_SDHCI_OMAP=y CONFIG_MMC_DW=n #SPI CONFIG_SPI_CADENCE_QUADSPI=y CONFIG_SPI_TI_QSPI=y #Disable unused SPI controllers CONFIG_SPI_BITBANG=n CONFIG_SPI_CADENCE=n CONFIG_SPI_ROCKCHIP=n CONFIG_SPI_XILINX=n CONFIG_SPI_SPIDEV=n #Disable SPI NOR 4K SECTORS CONFIG_MTD_SPI_NOR_USE_4K_SECTORS=n #SPI GPIO expanders CONFIG_GPIO_PISOSR=m #SATA CONFIG_SATA_AHCI_PLATFORM=m CONFIG_SATA_AHCI=m CONFIG_ATA=m #USB gadgets CONFIG_USB_GADGET=m CONFIG_USB_AUDIO=m CONFIG_USB_ETH=m CONFIG_USB_G_NCM=m CONFIG_USB_GADGETFS=m CONFIG_USB_FUNCTIONFS=m CONFIG_USB_FUNCTIONFS_ETH=y CONFIG_USB_FUNCTIONFS_RNDIS=y CONFIG_USB_FUNCTIONFS_GENERIC=y CONFIG_USB_MASS_STORAGE=m CONFIG_USB_G_SERIAL=m CONFIG_USB_MIDI_GADGET=m CONFIG_USB_G_PRINTER=m CONFIG_USB_CDC_COMPOSITE=m CONFIG_USB_G_ACM_MS=m CONFIG_USB_G_MULTI=m CONFIG_USB_G_MULTI_CDC=y CONFIG_USB_G_HID=m CONFIG_USB_G_DBGP=m CONFIG_USB_G_WEBCAM=m CONFIG_USB_GADGET_STORAGE_NUM_BUFFERS=32 CONFIG_USB_ZERO=m CONFIG_USB_CONFIGFS=m CONFIG_USB_CONFIGFS_SERIAL=y CONFIG_USB_CONFIGFS_ACM=y CONFIG_USB_CONFIGFS_OBEX=y CONFIG_USB_CONFIGFS_NCM=y CONFIG_USB_CONFIGFS_ECM=y CONFIG_USB_CONFIGFS_ECM_SUBSET=y CONFIG_USB_CONFIGFS_RNDIS=y CONFIG_USB_CONFIGFS_EEM=y CONFIG_USB_CONFIGFS_MASS_STORAGE=y CONFIG_USB_CONFIGFS_F_LB_SS=y CONFIG_USB_CONFIGFS_F_FS=y CONFIG_USB_CONFIGFS_F_UAC1=y CONFIG_USB_CONFIGFS_F_UAC2=y CONFIG_USB_CONFIGFS_F_MIDI=y CONFIG_USB_CONFIGFS_F_HID=y CONFIG_USB_CONFIGFS_F_UVC=y CONFIG_USB_CONFIGFS_F_PRINTER=y # USB DWC3 CONFIG_USB_DWC3=m CONFIG_USB_DWC3_DUAL_ROLE=y CONFIG_USB_DWC3_OMAP=m CONFIG_USB_DWC3_PCI=n CONFIG_USB_DWC2=n CONFIG_USB_CHIPIDEA=n #USB PHY CONFIG_NOP_USB_XCEIV=m #USB MUSB CONFIG_USB_MUSB_HDRC=m CONFIG_USB_MUSB_DUAL_ROLE=y CONFIG_USB_MUSB_OMAP2PLUS=m CONFIG_USB_MUSB_AM35X=m CONFIG_USB_MUSB_DSPS=m CONFIG_USB_MUSB_AM335X_CHILD=m CONFIG_TI_CPPI41=y CONFIG_USB_TI_CPPI41_DMA=y CONFIG_AM335X_CONTROL_USB=y CONFIG_AM335X_PHY_USB=y #USB EHCI CONFIG_USB=m CONFIG_USB_EHCI_HCD=m CONFIG_USB_EHCI_PCI=m CONFIG_USB_EHCI_HCD_OMAP=m #USB Networking CONFIG_USB_USBNET=m CONFIG_USB_NET_DRIVERS=m CONFIG_USB_NET_SMSC95XX=m #USB testing CONFIG_USB_TEST=m #USB Serial CONFIG_USB_ACM=m CONFIG_USB_SERIAL=m # Extcon drivers CONFIG_EXTCON=m CONFIG_EXTCON_PALMAS=m CONFIG_EXTCON_USB_GPIO=m # PWM CONFIG_PWM_TIECAP=y CONFIG_PWM_TIEHRPWM=y CONFIG_PWM_TIPWMSS=y # 1-wire Bus Masters CONFIG_W1=m CONFIG_HDQ_MASTER_OMAP=m # Matrix keypad CONFIG_KEYBOARD_MATRIX=m #Touchscreen/ADC CONFIG_TOUCHSCREEN_TI_AM335X_TSC=m CONFIG_TI_AM335X_ADC=m #CAN CONFIG_CAN=m CONFIG_CAN_C_CAN=m CONFIG_CAN_C_CAN_PLATFORM=m CONFIG_CAN_M_CAN=m # Rotary Encoder CONFIG_INPUT_GPIO_DECODER=m # Filesystem extra options CONFIG_EXT4_FS_POSIX_ACL=y CONFIG_EXT4_FS_SECURITY=y CONFIG_CIFS=m CONFIG_CIFS_STATS=y CONFIG_CIFS_XATTR=y CONFIG_CIFS_POSIX=y CONFIG_CIFS_ACL=y ################################################## # TI Audio/Display config options ################################################## CONFIG_CMA_SIZE_MBYTES=24 # backlight CONFIG_LEDS_CLASS=y CONFIG_LEDS_TLC591XX=y CONFIG_BACKLIGHT_PWM=y CONFIG_BACKLIGHT_GPIO=y CONFIG_BACKLIGHT_LED=y # fbdev CONFIG_FB_SSD1307=y # drm CONFIG_DRM=y # SGX driver needs legacy support CONFIG_DRM_LEGACY=y CONFIG_DRM_VM=y # Disable unneeded features CONFIG_VGA_ARB=n CONFIG_DRM_I2C_ADV7511=n CONFIG_DRM_NOUVEAU=n CONFIG_DRM_EXYNOS=n CONFIG_DRM_PANEL_SIMPLE=n CONFIG_DRM_PANEL_SAMSUNG_S6E8AA0=n CONFIG_DRM_NXP_PTN3460=n CONFIG_DRM_PARADE_PS8622=n CONFIG_DRM_STI=n CONFIG_LCD_CLASS_DEVICE=n # tilcdc CONFIG_DRM_I2C_NXP_TDA998X=y CONFIG_DRM_TILCDC=y # omapdrm CONFIG_DRM_OMAP=y CONFIG_DRM_OMAP_WB=y CONFIG_OMAP2_DSS=y CONFIG_OMAP2_DSS_DEBUGFS=y CONFIG_OMAP2_DSS_DPI=y CONFIG_OMAP2_DSS_VENC=n CONFIG_OMAP4_DSS_HDMI=y CONFIG_OMAP5_DSS_HDMI=y CONFIG_OMAP2_DSS_SDI=n CONFIG_OMAP2_DSS_DSI=n CONFIG_TI_DSS6=y CONFIG_DRM_OMAP_PANEL_DPI=y CONFIG_DRM_OMAP_CONNECTOR_HDMI=y CONFIG_DRM_OMAP_CONNECTOR_DVI=y CONFIG_DRM_OMAP_DRA7EVM_ENCODER_TPD12S015=y CONFIG_DRM_OMAP_ENCODER_TPD12S015=y CONFIG_DRM_OMAP_ENCODER_SII9022=y CONFIG_DRM_OMAP_ENCODER_TC358768=y CONFIG_DRM_OMAP_ENCODER_TFP410=y # sound CONFIG_SOUND=y CONFIG_SND=y CONFIG_SND_SOC=y CONFIG_SND_OMAP_SOC=y CONFIG_SND_EDMA_SOC=y CONFIG_SND_DAVINCI_SOC_MCASP=y CONFIG_SND_AM33XX_SOC_EVM=m CONFIG_SND_SIMPLE_CARD=m CONFIG_SND_SOC_TLV320AIC31XX=m CONFIG_SND_SOC_TLV320AIC3X=m CONFIG_SND_SOC_HDMI_CODEC=m CONFIG_SND_OMAP_SOC_HDMI_AUDIO=m # Disable what we don't want in our config CONFIG_SND_ARM=n CONFIG_SND_SPI=n CONFIG_SND_PCI=n CONFIG_SND_ATMEL_SOC=n CONFIG_SND_SOC_FSL_SAI=n CONFIG_SND_OMAP_SOC_OMAP3_PANDORA=n CONFIG_SND_SOC_AK4642=n CONFIG_SND_SOC_SGTL5000=n CONFIG_SND_SOC_STI_SAS=n CONFIG_SND_SOC_WM8978=n # v4l2 CONFIG_MEDIA_SUPPORT=y CONFIG_MEDIA_CAMERA_SUPPORT=y CONFIG_MEDIA_CONTROLLER=y CONFIG_VIDEO_V4L2_SUBDEV_API=y CONFIG_V4L_PLATFORM_DRIVERS=y CONFIG_VIDEO_AM437X_VPFE=m CONFIG_VIDEO_TI_CAL=m CONFIG_VIDEO_TI_VIP=m CONFIG_V4L_MEM2MEM_DRIVERS=y CONFIG_VIDEO_TI_VPE=m CONFIG_MEDIA_SUBDRV_AUTOSELECT=n CONFIG_VIDEO_OV2659=m CONFIG_VIDEO_OV1063X=m CONFIG_VIDEO_MT9T11X=m CONFIG_GPIO_PCA953X=m CONFIG_VIDEO_OV490=m CONFIG_MEDIA_USB_SUPPORT=y CONFIG_USB_VIDEO_CLASS=m CONFIG_USB_VIDEO_CLASS_INPUT_EVDEV=y # Touchscreen CONFIG_TOUCHSCREEN_EDT_FT5X06=m CONFIG_TOUCHSCREEN_PIXCIR=m CONFIG_TOUCHSCREEN_GOODIX=m CONFIG_HID_MULTITOUCH=m ################################################## # TI Base OMAP generation SoCs generic default ################################################## CONFIG_KEYSTONE2_DMA_COHERENT=n CONFIG_ARCH_OMAP=y CONFIG_ARCH_OMAP2PLUS=y CONFIG_OMAP_INTERCONNECT_BARRIER=y CONFIG_ARM_PSCI=n # Maximum Number of processors CONFIG_NR_CPUS=2 # Kexec CONFIG_KEXEC=y # EDAC CONFIG_EDAC=y CONFIG_EDAC_TI=m ################################################## # TI DRA7 specific config options ################################################## # Supported ARM CPUs CONFIG_ARCH_MULTI_V6=n CONFIG_ARCH_MULTI_V7=y CONFIG_ARCH_MULTI_V6_V7=n CONFIG_CPU_V6=n # Enable CONFIG_SMP CONFIG_SMP=y # Disable Socs other than DRA7 CONFIG_ARCH_OMAP2=n CONFIG_ARCH_OMAP3=n CONFIG_ARCH_OMAP4=n CONFIG_SOC_OMAP5=n CONFIG_SOC_AM33XX=n CONFIG_SOC_AM43XX=n CONFIG_SOC_DRA7XX=y CONFIG_ARCH_KEYSTONE=n CONFIG_ARM_LPAE=y CONFIG_TI_PTP_BC=y CONFIG_TI_1PPS_DM_TIMER=y ################################################## # Real Time Linux Configs ################################################## CONFIG_PREEMPT=y CONFIG_PREEMPT_RT_BASE=y CONFIG_PREEMPT_RT_FULL=y #Disable PM features CONFIG_CPU_IDLE=n CONFIG_CPU_FREQ=n CONFIG_SUSPEND=n CONFIG_HOTPLUG_CPU=y # SCHED_DEBUG provides a lot of additional options for scheduler # tuning in /proc/sys/kernel/ and allows to see scheduler statistic in # /proc/sched_debug # CONFIG_SCHED_DEBUG # --- RCU optimization options to reduce OS jitter # RCU_BOOST : This option boosts the priority of preempted RCU readers that # block the current preemptible RCU grace period for too long. # This option also prevents heavy loads from blocking RCU # callback invocation for all flavors of RCU # CONFIG_RCU_BOOST=n # RCU_NOCB_CPU : Use this option to reduce OS jitter for aggressive HPC or # real-time workloads. It can also be used to offload RCU # callback invocation to energy-efficient CPUs in battery-powered # asymmetric multiprocessors. # CONFIG_RCU_NOCB_CPU=y # RCU_NOCB_CPU_ALL: his option forces all CPUs to be no-CBs CPUs. # The rcu_nocbs= boot parameter will be ignored. All CPUs' RCU callbacks will # be executed in the context of per-CPU rcuo kthreads created for # this purpose. # CONFIG_RCU_NOCB_CPU_ALL=y ############################################## # # Kernel options needed for systemd enabled TI SDKs # See https://cgit.freedesktop.org/systemd/systemd/tree/README#n38 for details # ############################################## CONFIG_DEVTMPFS=y CONFIG_DEVTMPFS_MOUNT=y CONFIG_CGROUPS=y CONFIG_CGROUP_FREEZER=y CONFIG_CGROUP_DEVICE=y CONFIG_CGROUP_CPUACCT=y CONFIG_BLK_CGROUP=y CONFIG_CGROUP_PIDS=y CONFIG_CGROUP_PERF=y CONFIG_INOTIFY_USER=y CONFIG_SIGNALFD=y CONFIG_TIMERFD=y CONFIG_EPOLL=y CONFIG_NET=y CONFIG_SYSFS=y CONFIG_PROC_FS=y CONFIG_FHANDLE=y # udev will fail to work with the legacy sysfs layout: CONFIG_SYSFS_DEPRECATED=n # Legacy hotplug slows down the system and confuses udev: CONFIG_UEVENT_HELPER_PATH="" # Userspace firmware loading is not supported and should # be disabled in the kernel: CONFIG_FW_LOADER_USER_HELPER=n # Some udev rules and virtualization detection relies on it: # Only for UEFI based systems # http://cateee.net/lkddb/web-lkddb/DMI.html CONFIG_DMIID=n # Support for some SCSI devices serial number retrieval, to # create additional symlinks in /dev/disk/ and /dev/tape: CONFIG_BLK_DEV_BSG=y # Required for PrivateNetwork and PrivateDevices in service units: # Note that systemd-localed.service and other systemd units use # PrivateNetwork and PrivateDevices so this is effectively required. CONFIG_NAMESPACES=y CONFIG_NET_NS=y CONFIG_DEVPTS_MULTIPLE_INSTANCES=y # Optional but strongly recommended options: those are nice to have and # indeed recommended, but not necessarily systemd required. These to be # enabled in corresponding domain fragments since they are not specific # to supporting systemd. CONFIG_SECCOMP=y # for kcmp syscall CONFIG_CHECKPOINT_RESTORE=y # Required for CPUShares= in resource control unit settings CONFIG_CGROUP_SCHED=y CONFIG_FAIR_GROUP_SCHED=y # Required for CPUQuota= in resource control unit settings CONFIG_CFS_BANDWIDTH=y # For systemd-bootchart, several proc debug interfaces are required: # Systemd-debug.cfg? CONFIG_SCHEDSTATS=y CONFIG_SCHED_DEBUG=y # We recommend to turn off Real-Time group scheduling in the # kernel when using systemd. RT group scheduling effectively # makes RT scheduling unavailable for most userspace, since it # requires explicit assignment of RT budgets to each unit whose # processes making use of RT. As there's no sensible way to # assign these budgets automatically this cannot really be # fixed, and it's best to disable group scheduling hence. CONFIG_RT_GROUP_SCHED=n # Note that kernel auditing is broken when used with systemd's # container code. When using systemd in conjunction with # containers, please make sure to either turn off auditing at # runtime using the kernel command line option "audit=0", or # turn it off at kernel compile time using: CONFIG_AUDIT=n