in doc spruem2a, Dm648 supports only 16-bit adress,because it uses a 16-bit-long register for memory adress;
in the meanwhile, in the erf spraaj1d, 24-bit SPI address mode is valid.
I wonder that dm648 is able to boot from spi in 24-bit address mode. Only if it supports 24-bit address, SPI memory space
is enough for the application image.
Only values of 0x02
(16-bit SPI EEPROM) or 0x03 (24-bit SPI EEPROM/Flash) are acceptable.