Other Parts Discussed in Thread: ADS1606,
What would be the best way to connect an ADS1606 to the AM5728 while using as little as possible glue logic?
I see the GPMC as one option, but in the future I would like to be able to connect 3 of these ADCs, and with the GPMC PCB routing becomes a bit complicated, since the 16 bits of data will have to be connected in parallel.
Would it be possible to configure the VIP to get data from the ADS1606? To have the VIP read a 16 bit word on each pixel clock and store it in a buffer, working without a horizontal or vertical sync lines?
I have a AM572x EVM I'm working with and plan to make a daughter board with the ADC (instead of the LCD module), so if the suggested interfaces were available on the AM572x GP EVM expansion connectors, that would be even more helpful.
Maybe there is and example project available somewhere that shows the AM5728 getting data from an ADC at several MSPS?