Tool/software: Linux
Hello experts
Hardware: Beaglebone black
Software : latest TI SDK
I am trying to operate the UART in 3000000 baud rate
my Question:
Do i need to do any changes in software to achieve this baudrate ?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hello experts
Hardware: Beaglebone black
Software : latest TI SDK
I am trying to operate the UART in 3000000 baud rate
my Question:
Do i need to do any changes in software to achieve this baudrate ?
Regards
I derived my information from table 19-25, on page 4344 where this baud rate is not in the list, will check again for this difference in the tables.
Forgot to mention that I'm looking at
https://www.ti.com/lit/ug/spruh73p/spruh73p.pdf
Hi Nick,
What do you mean you don't see any data? You don't see data on the uart bus analyzer or the receiving application?
Do you see data in any lower baud rate?
yes i dont see any data and in the
kernel config
Device Drivers --->
Character devices --->
Serial drivers --->
"8250/16550 and compatible serial support" i see this driver is enabled can you please confirm if this driver support 3Mbps
and by the way we are using the TI SDK version : Processor SDK Linux for AM335x v04.00.00.04 Download i know this is 3 version old but still
Please the attached C code it works fine for all baud rate less than 230400 and when i increase the baudrate to 3000000 it does not work
#include <stdio.h> /* Standard input/output definitions */ #include <string.h> /* String function definitions */ #include <unistd.h> /* UNIX standard function definitions */ #include <fcntl.h> /* File control definitions */ #include <errno.h> /* Error number definitions */ #include <termios.h> /* POSIX terminal control definitions */ #include <sys/types.h> #include <sys/time.h> #include <sys/select.h> #include <signal.h> #include <pthread.h> #define TIMEVAL struct timeval //globals: int bRunning=1; int bRun=1; //static const char *pHelloToken="hey laptop i just got: "; //FD: int ttyFD=-1; //global for this module pthread_t thrid; //open-tuning: int tty_open(const char *pDevName, unsigned int nBaud) { int fd; struct termios options; //open: fd = open(pDevName, O_RDWR | O_NOCTTY | O_NDELAY); if(-1 == fd) return fd; //tune: fcntl(fd, F_SETFL, 0); tcgetattr(fd, &options); options.c_cflag &= ~PARENB; options.c_cflag &= ~CSTOPB; options.c_cflag &= ~CSIZE; options.c_cflag |= CS8; if(cfsetispeed(&options, nBaud)<0) //B115200); //B3000000); { printf("failed to set input speed to %d\n", nBaud); } if(cfsetospeed(&options, nBaud)<0) //B115200); //B3000000); { printf("failed to set output speed to %d\n", nBaud); } /*options.c_cflag &= ~CBAUD; //Remove current BAUD rate options.c_cflag |= BOTHER; //Allow custom BAUD rate using int input options.c_ispeed = 3000000; //Set the input BAUD rate options.c_ospeed = 3000000; //Set the output BAUD rate*/ options.c_cflag |= (CLOCAL | CREAD); options.c_cflag |= (CLOCAL | CREAD); // options.c_cflag &= ~CNEW_RTSCTS; options.c_lflag &= ~(ICANON | ECHO | ECHOE | ISIG); //raw mode!!! options.c_iflag &= ~(IXON | IXOFF | IXANY); //no soft flow options.c_oflag &= ~OPOST; //raw output also tcsetattr(fd, TCSAFLUSH, &options); return fd; //!!!!!! } int tty_blread(int nFD, char *pBuf, int nBufSize, int tmt_mS) { fd_set fd; TIMEVAL tv; int bytes_read; //read all from port: bytes_read=0; FD_ZERO(&fd); tv.tv_sec = 0; tv.tv_usec =tmt_mS*1000; //mS FD_SET(nFD, &fd); if(0==select(nFD+1, &fd, NULL, NULL, &tv)) //wait for data return bytes_read; bytes_read+=read(nFD, pBuf+bytes_read, nBufSize-bytes_read); return bytes_read; } void *upd_loop(void *parg) { int nRead; char in_buf[1024]; if(ttyFD<0) { pthread_exit(0); } printf("entering listening thread...\n"); while(bRun){ nRead=tty_blread(ttyFD, in_buf, sizeof(in_buf), 500); if(nRead>0) { #ifdef DIAG_MSG in_buf[nRead-1]='\0'; printf("->%s", in_buf); printf("\r\n"); #endif } usleep(100000); } printf("exiting listening thread...\n"); pthread_exit(0); } int init_at_comm(void) { return pthread_create(&thrid, NULL, upd_loop, NULL); } void destroy_at_comm(void) { bRun=0; pthread_join(thrid, NULL); } static void sigexit_handler(int signum) { bRunning=0; } int main(void) { struct termios tios; speed_t ispeed; speed_t ospeed; signal(SIGQUIT, sigexit_handler); signal(SIGINT, sigexit_handler); signal(SIGTERM, sigexit_handler); ttyFD=tty_open("/dev/ttyS1", 3000000); //B9600); if(ttyFD<0) { printf("failed to open ttyS1\n"); return 1; } tcgetattr(0, &tios); ispeed = cfgetispeed(&tios); ospeed = cfgetospeed(&tios); printf("baud rate in: %d\n", tios.c_ispeed); printf("baud rate out: %d\n", tios.c_ospeed); init_at_comm(); while(bRunning) { usleep(50000); } destroy_at_comm(); close(ttyFD); return 0; }
even if i use this linux-serial-test -y 0x55 -z 0x0 -p /dev/ttyS1 -b 3000000 as mentioned in this link (https://github.com/cbrake/linux-serial-test/blob/master/linux-serial-test.c) still i do not see the baud of 3000000 i think it is issue with the kernel serial drivers can you please help check if this driver support 3000000 baud rate