Part Number: TMDXIDK5728
Tool/software: Linux
Hello,
I am running the newest Linux SDK on a SD card and I am root debugging through my JTAG to USB XDS100v2. I have a PCAN Connector attached to my J38 CAN header pins. I am able to send CAN frames FROM the EVM to the PCAN. I am not able to send frames TO the EVM from the PCAN.
I am using "candump any" as the command. I also have tried "candump -s 0 -l any" to turn off silent mode. I know my bitrate settings are fine due to being able to get the frames out of the EVM. When I attempt to send different frames from the PCAN interface, nothing shows up in the Serial PuTTY window and the BUS status goes to BUS HEAVY, indicating an ACK error.
Using "cansend can0 123#12.13.14.15.16.17.18.19" works fine. I get the frame in the PCAN.
Please help me to figure out how to remedy this error. I am wondering if it's a similar issue to the SDK-RTOS CAN problem, where the signal wasn't reaching the header pin.
Thank you,
Alec