This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM6528: WKUP-uart access from A53

Part Number: AM6528

Tool/software: Linux

HI

Can the WKUP_UART be used by linux running on the A53? Do we have any linux examples for this?

Also can the MCU-UART (this is part of the MCU block) be used by the A53 running linux? If yes i assume it is already part of the linux release? 

Any example or how to setup the dts for these 2 uarts would be great.

We need to have 4 UARTS that can be controlled by the A53 running linux. There are 3 as part of the A53 so need one more.

Thanks