Part Number: 66AK2G12
Hi,
My customer forgot to apply the following directions for some differential clock inputs on their custom board:
5.9.3.2 Optional LVDS Clock Inputs Not Used
Some *_P/N signals are pulled up/down with 10kΩ rather than 130Ω. I know the recommendation is still following the datasheet, but just in case, i would like to confirm that, is there any possibilities to have fatal problem in the device point of view if they leave the current connection ? Can you share the reason for using 130Ω?
Best Regards,
NK