Part Number: AM3352
My customer want to use ROM ECC NAND boot, but forgot to pull down SYSBOOT[9], left it un-pulled/floating, but it still can boot from NAND, did not find issue so far, and measured on SYSBOOT[9] is LOW, want to make sure whether it is internal pulled down in default, as this product deployed in field already, and volume is big, fell upset about the stability, so want to ask for confirmation.