Part Number: AM5728
Other Parts Discussed in Thread: PMP, DRA752
Tool/software: Linux
I have a AM5728 custom board.
I split the sd card's partition into two partitions via create-sdcard.sh provided by sdk (8GB capacity).
The following dt and pinmux have been modified for custom boards.
software-dl.ti.com/.../Foundational_Components_U-Boot.html
I built u-boot and the kernel as shown in the above guide and copied the image to the sd card.
But I can not move from u-boot to the kernel.
Could you tell me why?
------------------------------------------------------------------
SDK = ti-processor-sdk-linux-rt-am57xx-evm-05.03.00.07
u-boot = u-boot-2018.01+gitAUTOINC+313dcd69c2-ge2bc936055
kernel = linux-rt-4.14.79+gitAUTOINC+a72bf1418c-ga72bf1418c
cross compiler = arm-linux-gnueabihf-gcc
------------------------------------------------------------------
1. console
MMC read: dev # 1, block # 10518528, count 2097152 ... �
U-Boot SPL 2018.01-00569-g7d9bc2b3c2-dirty (May 28 2019 - 15:41:00)
DRA752-GP ES2.0
Trying to boot from MMC1
no pinctrl state for default mode
no pinctrl state for default mode
U-Boot 2018.01-00569-g7d9bc2b3c2-dirty (May 28 2019 - 15:41:00 +0900)
CPU : DRA752-GP ES2.0
Model: TI AM5728 IDK
Board: AM572x IDK REV
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Warning: fastboot.board_rev: unknown board revision
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Could not get PHY for ethernet@48484000: addr 0
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** File not found boot.scr **
** Unrecognized filesystem type **
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** File not found /boot/fitImage **
Trying to boot Linux from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** File not found /boot/fitImage **
Trying to boot Android from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
MMC read: dev # 1, block # 10518528, count 2097152 ... 2097152 blocks read: OK
mmc - MMC sub system
Usage:
mmc info - display info of the current MMC device
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt
mmc rescan
mmc part - lists available partition on current mmc device
mmc dev [dev] [part] - show or set current mmc device [partition]
mmc list - lists available devices
mmc hwpartition [args...] - does hardware partitioning
arguments (sizes in 512-byte blocks):
[user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
[gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
[check|set|complete] - mode, complete set partitioning completed
WARNING: Partitioning is a write-once setting once it is set to complete.
Power cycling is required to initialize partitions after set to complete.
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
mmc rst-function dev value
- Change the RST_n_FUNCTION field of the specified device
WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
mmc setdsr <value> - set DSR register value
Wrong Image Format for bootm command
ERROR: can't get kernel image!
=>
2.printenv
arch=arm
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=am57xx
board_name=am572x_idk
boot_fdt=try
boot_fit=0
boot_part=9
bootargs=androidboot.serialno=0f00200e1b340122 console=ttyS2,115200 androidboot.console=ttyS2 androidboot.hardware=am57xevmboard
bootcmd=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;echo Booting into fastboot ...; fastboot 1; fi;if test ${boot_fit} -eq 1; then run u
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=fitImage
bootm_size=0x10000000
bootpart=1:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO1,115200n8
cpu=armv7
devnum=1
devtype=mmc
dfu_alt_info_emmc=rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x200;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image1
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x200;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;1
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
dfu_bufsiz=0x10000
dofastboot=0
emmc_android_boot=echo Trying to boot Android from eMMC ...; run update_to_fit; setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 1; setenv fdt_part 3; setenv boot_part 9; setenv ;
emmc_linux_boot=echo Trying to boot Linux from eMMC ...; setenv mmcdev 1; setenv bootpart 1:2; setenv mmcroot /dev/mmcblk0p2 rw; run mmcboot;
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbooten;
ethaddr=94:e3:6d:4a:fe:f2
eval_bootargs=setenv bootargs androidboot.serialno=0f00200e1b340122 console=ttyS2,115200 androidboot.console=ttyS2 androidboot.hardware=am57xevmboard
fastboot.cpu=DRA752
fastboot.secure=GP
fdt_addr_r=0x88000000
fdt_part=3
fdt_size=200000
fdt_start=a08000
fdtaddr=0x88000000
fdtcontroladdr=fdf187d8
fdtfile=am572x-idk.dtb
findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-evm.dtb; fi;if test $board_name = dra72x-revc; then setenv fdtfile dra72-
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage
fit_loadaddr=0x87000000
idk_lcd=no
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
kernel_addr_r=0x82000000
loadaddr=0x87000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_mmc; bootm ${loadaddr}#${fdtfile};
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
machid=fe6
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test ${boot_fit} -eq 1; then run loadfit; else run mmc;
mmcdev=1
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the;
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext4 rootwait
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
nfsopts=nolock
partitions=uuid_disk=${uuid_gpt_disk};name=bootloader,start=384K,size=1792K,uuid=${uuid_gpt_bootloader};name=rootfs,start=2688K,size=-,uuid=${uuid_gpt_rootfs}
partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=1792K,uuid=${uuid_gpt_bootloader};name=environment,size=128K,uuid=${uuid_gpt_environ}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
rootpath=/export/rootfs
scriptaddr=0x80000000
scsidevs=0
serial#=0f00200e1b340122
soc=omap5
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@4806c000
stdin=serial@4806c000
stdout=serial@4806c000
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usbtty=cdc_acm
vendor=ti
ver=U-Boot 2018.01-00569-g7d9bc2b3c2-dirty (May 28 2019 - 15:41:00 +0900)
vram=16M
Environment size: 8012/131067 bytes