This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: TIDL .y file

Other Parts Discussed in Thread: AM5708

Hi,

How is the .y file made?

  • Good question. This file can be either .y or .raw image format. To create this, you can use the convert tool through imageMagick. For example, converting from png to raw:
    'convert input_image.png -interlace plane RGB:output_image.raw'

    This command should work in the same way for a .y file, just exchange the file extension. If you didn't train the network on 224x224 images, make sure the inWidth, inHeight and dimensions of .raw (or .y) image matches the dimensions of the images you trained with.
  • Hi,

    This is the single input image in a format that is used for training the network model. It is used to derive the quantization parameters for dynamic quantization feature. You can learn about dynamic quantization here -

  • My apologies, I left out a step because I needed to confirm it. TIDL will do a conversion to BGR (rather than RGB) image format when using the model, but this conversion is not done automatically on the sample image or raw input images. To fix this, you'll need to convert the image to BGR format before converting to raw. Instead of the single command I used before, please use the two I am posting below.

    convert $input_filename -separate +channel -swap 0,2 -combine -colorspace sRGB ./sample_bgr.png

    convert ./sample_bgr.png  -interlace plane BGR:sample_img.raw

  • Hi

         First thank you,  after i command the above two, and i  got the .raw file.

        But when i command  the following :

    tidl_model_import.out /home/lab/Documents/sdk5.03/linux-devkit/sysroots/x86_64-arago-linux/usr/share/ti/tidl/uti
    ls/test/testvecs/config/import/caffe/tidl_import_alex66.txt

    and the result :


    Name of the Network : CaffeNet
    Num Inputs : 0
    Input layer(s) not Available.. Assuming below one Input Layer !!Unsuported Layer Type : Input !!!! assuming it as pass through layer
    [libprotobuf FATAL /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-tidl-import/01.01.00.00-r0/recipe-sysroot-native/usr/include/google/protobuf/repeated_field.h:1478] CHECK failed: (index) < (current_size_):
    terminate called after throwing an instance of 'google::protobuf::FatalException'
    what(): CHECK failed: (index) < (current_size_):
    Aborted (core dumped)

     the last   words indicate : "CHECK failed: (index) < (current_size_):,", i don't know the reason,what should i  do?

  • Hi,

    Are you trying to do an implementation of AlexNet? This is not supported by us because there is not a 'Normalize' layer in TIDL.

  • Yes,indeed. I actually use the  AlexNet model . Here is the  my situation , i already  trained two models for  a  image classification  task , the one  is AlexNet model, it's accuracy  almost have  99.9%. The another one is  ShuffleNet, although it's  training  faster  than AlexNet  about 5 times, but it's  accuracy  only have  90%.

     On this website :http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_TIDL.html#verified-networks-topologies  it's said  support  Caffe-Jacinto11  model,  how it's accuracy may only have  80 %( i didn't  run this model and  just saw it on the  website like  github ,maybe it is higher now ) .

    My purpose is   use a model  that can run on  TIDL  through the AM5708 to inference the result , not  use TI  devcie translator tool  that model   can  fit  TIDL  (like Caffe-Jacinto11 ) is very well , however  the accuracy  shouldn't be  too low,   what  should  i do , can you  give me some advice  ,thanks  a lot.

  • [libprotobuf ERROR google/protobuf/text_format.cc:288] Error parsing text-format caffe.NetParameter: 356:25: Message type "caffe.LayerParameter" has no field named "shuffle_channel_param".
    ERROR: Reading text proto file
    Name of the Network : ShuffleNet V2 
    Num Inputs : 1 
    Unsuported Layer Type : ConvolutionDepthwise !!!! assuming it as pass through layer
    Unsuported Layer Type : ConvolutionDepthwise !!!! assuming it as pass through layer
    Unsuported Layer Type : ShuffleChannel !!!! assuming it as pass through layer
    Num of Layer Detected : 14 
    0, TIDL_DataLayer , data 0, -1 , 1 , x , x , x , x , x , x , x , x , 0 , 0 , 0 , 0 , 0 , 1 , 3 , 224 , 224 , 0 ,
    1, TIDL_ConvolutionLayer , conv1 1, 1 , 1 , 0 , x , x , x , x , x , x , x , 1 , 1 , 3 , 224 , 224 , 1 , 24 , 112 , 112 , 8128512 ,
    2, TIDL_PoolingLayer , pool1 1, 1 , 1 , 1 , x , x , x , x , x , x , x , 2 , 1 , 24 , 112 , 112 , 1 , 24 , 56 , 56 , 677376 ,
    3, TIDL_UnSuportedLayer , resx1_match_DWconv 1, 1 , 1 , 2 , x , x , x , x , x , x , x , 3 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 , 0 ,
    4, TIDL_BatchNormLayer , resx1_match_DWconv_bn 1, 1 , 1 , 3 , x , x , x , x , x , x , x , 3 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 , 75264 ,
    5, TIDL_BatchNormLayer , resx1_match_DWconv_scale 1, 1 , 1 , 3 , x , x , x , x , x , x , x , 4 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 , 75264 ,
    6, TIDL_ConvolutionLayer , resx1_match_conv 1, 1 , 1 , 4 , x , x , x , x , x , x , x , 5 , 1 , 24 , 56 , 56 , 1 , 122 , 56 , 56 , 9182208 ,
    7, TIDL_ConvolutionLayer , resx1_conv1 1, 1 , 1 , 2 , x , x , x , x , x , x , x , 6 , 1 , 24 , 56 , 56 , 1 , 122 , 56 , 56 , 9182208 ,
    8, TIDL_UnSuportedLayer , resx1_conv2 1, 1 , 1 , 6 , x , x , x , x , x , x , x , 7 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 , 0 ,
    9, TIDL_BatchNormLayer , resx1_conv2_bn 1, 1 , 1 , 7 , x , x , x , x , x , x , x , 7 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 , 382592 ,
    10, TIDL_BatchNormLayer , resx1_conv2_scale 1, 1 , 1 , 7 , x , x , x , x , x , x , x , 8 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 , 382592 ,
    11, TIDL_ConvolutionLayer , resx1_conv3 1, 1 , 1 , 8 , x , x , x , x , x , x , x , 9 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 , 46676224 ,
    12, TIDL_ConcatLayer , resx1_concat 1, 2 , 1 , 5 , 9 , x , x , x , x , x , x , 10 , 1 , 122 , 56 , 56 , 1 , 244 , 56 , 56 , 1 ,
    13, TIDL_UnSuportedLayer , shuffle1 1, 1 , 1 , 10 , x , x , x , x , x , x , x , 11 , 1 , 244 , 56 , 56 , 1 , 244 , 56 , 56 , 0 ,
    Total Giga Macs : 0.0748

    Processing config file ./tempDir/qunat_stats_config.txt !
    0, TIDL_DataLayer , 0, -1 , 1 , x , x , x , x , x , x , x , x , 0 , 0 , 0 , 0 , 0 , 1 , 3 , 224 , 224 ,
    1, TIDL_ConvolutionLayer , 1, 1 , 1 , 0 , x , x , x , x , x , x , x , 1 , 1 , 3 , 224 , 224 , 1 , 24 , 112 , 112 ,
    2, TIDL_PoolingLayer , 1, 1 , 1 , 1 , x , x , x , x , x , x , x , 2 , 1 , 24 , 112 , 112 , 1 , 24 , 56 , 56 ,
    3, TIDL_ReshapeLayer , 1, 1 , 1 , 2 , x , x , x , x , x , x , x , 3 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 ,
    4, TIDL_BatchNormLayer , 1, 1 , 1 , 3 , x , x , x , x , x , x , x , 3 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 ,
    5, TIDL_BatchNormLayer , 1, 1 , 1 , 3 , x , x , x , x , x , x , x , 4 , 1 , 24 , 56 , 56 , 1 , 24 , 56 , 56 ,
    6, TIDL_ConvolutionLayer , 1, 1 , 1 , 4 , x , x , x , x , x , x , x , 5 , 1 , 24 , 56 , 56 , 1 , 122 , 56 , 56 ,
    7, TIDL_ConvolutionLayer , 1, 1 , 1 , 2 , x , x , x , x , x , x , x , 6 , 1 , 24 , 56 , 56 , 1 , 122 , 56 , 56 ,
    8, TIDL_ReshapeLayer , 1, 1 , 1 , 6 , x , x , x , x , x , x , x , 7 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 ,
    9, TIDL_BatchNormLayer , 1, 1 , 1 , 7 , x , x , x , x , x , x , x , 7 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 ,
    10, TIDL_BatchNormLayer , 1, 1 , 1 , 7 , x , x , x , x , x , x , x , 8 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 ,
    11, TIDL_ConvolutionLayer , 1, 1 , 1 , 8 , x , x , x , x , x , x , x , 9 , 1 , 122 , 56 , 56 , 1 , 122 , 56 , 56 ,
    12, TIDL_ConcatLayer , 1, 2 , 1 , 5 , 9 , x , x , x , x , x , x , 10 , 1 , 122 , 56 , 56 , 1 , 244 , 56 , 56 ,
    13, TIDL_ReshapeLayer , 1, 1 , 1 , 10 , x , x , x , x , x , x , x , 11 , 1 , 244 , 56 , 56 , 1 , 244 , 56 , 56 ,
    14, TIDL_DataLayer , 0, 1 , -1 , 11 , x , x , x , x , x , x , x , 0 , 1 , 244 , 56 , 56 , 0 , 0 , 0 , 0 ,

    TIDL returned with error code : -1100, refer to interface header file for error code details

    Error at line: 1596 : in file src/tidl_tb.c, of function : test_ti_dl_ivison 
    End of config list found !

    It's seems  to be  unsupported  the " convolutionDepthwise " layer,  but this time  it's better than Alexnet,  because it produce    configFileslist.txt, qunat_stats_config.txt, temp_net.bin,  three  files   under the  tempDir  folder,  and tidl_net_shffle.bin, tidl_param_shuffle.bin under the  tidl_models folder,   can i  think it works ?

    Besides , if it doesn't works,  can  i just delete  the  ConvolutionDepthwise “”  layer on the  Shufflenet , or  delete the "Normalize " layer  on the Alexnet ,    so that  can  fit   the  TIDL; Or  is there  any  method   to  improve the  caffe_ jacinto11  's  accuracy  reach the 90%,  thanks  a lot .

  • It seems both of those networks include layers unsupported by TIDL. It is worth noting that running deep learning models on an embedded platform will require sacrifices in accuracy for the network to produce results quickly enough to be actionable. This is briefly explained before the list of verified network topologies. The set of verified topologies are chosen with this in mind.

    Removing a normalization layer might be fine for Alex net, though I wouldn't recommend it. I would expect the shuffle layer to be important for ShuffleNet though. You can try removing these, but I would not expect great results. The tidl_net*.bin and tidl_param*.bin were created I see, but they probably did not finish. I would be surprised if those worked.

    I'm not sure I understand what you mean by:

    "My purpose is   use a model  that can run on  TIDL  through the AM5708 to inference the result , not  use TI  devcie translator tool  that model   can  fit  TIDL  (like Caffe-Jacinto11 ) is very well , however  the accuracy  shouldn't be  too low,   what  should  i do , can you  give me some advice  ,thanks  a lot."

    particularly the part on not using the device translator tool. When you train one of these models, you'll need to convert it into a pair of binaries describing the network and weights for it to run on through TIDL on an embedded platform. This is a requirement if you wish to run this on an AM57X processor.

    My recommendation would be to use one of the topologies verified for TIDL or to find another suitable network that only contains supported layers.

  • Hi,

      Thank you so much  for your explanation , after  read  you replay , i know i need  the device translator tool  to convert the model  into a pair of binaries which describing the network and  weights for  it to run on through TIDL on an embedded platform.

    Today , i try  to install the  Caffe-Jacinto  ,   after  changed  the files "Makefile"  ,"Makefile.config"   and  during the  installation  some problem already  be fixed  through  searching the web,   but   the following  problems  appear   3 times :

    CXX examples/siamese/convert_mnist_siamese_data.cpp
    CXX .build_release/src/caffe/proto/caffe.pb.cc
    AR -o .build_release/lib/libcaffe-nv.a
    LD -o .build_release/lib/libcaffe-nv.so.0.17.0
    CXX/LD -o .build_release/tools/upgrade_net_proto_binary.bin
    CXX/LD -o .build_release/tools/compute_image_mean.bin
    CXX/LD -o .build_release/tools/caffe.bin
    CXX/LD -o .build_release/tools/upgrade_solver_proto_text.bin
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionGroupCount'
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionMathType'
    collect2: error: ld returned 1 exit status
    Makefile:654: recipe for target '.build_release/tools/compute_image_mean.bin' failed
    make: *** [.build_release/tools/compute_image_mean.bin] Error 1
    make: *** Waiting for unfinished jobs....
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionGroupCount'
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionMathType'
    collect2: error: ld returned 1 exit status
    Makefile:654: recipe for target '.build_release/tools/upgrade_solver_proto_text.bin' failed
    make: *** [.build_release/tools/upgrade_solver_proto_text.bin] Error 1
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionGroupCount'
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionMathType'
    collect2: error: ld returned 1 exit status
    Makefile:654: recipe for target '.build_release/tools/caffe.bin' failed
    make: *** [.build_release/tools/caffe.bin] Error 1
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionGroupCount'
    .build_release/lib/libcaffe-nv.so: undefined reference to `cudnnSetConvolutionMathType'
    collect2: error: ld returned 1 exit status
    Makefile:654: recipe for target '.build_release/tools/upgrade_net_proto_binary.bin' failed
    make: *** [.build_release/tools/upgrade_net_proto_binary.bin] Error 1
    lab@lab-System-Product-Name:/home/caffeinstall/caffe$

    Until now , i can't find  the  reason  and  don't know  how to  solve this ,  would you like  help me  ?   Thank   you advance ;

                                                                                                                                                                          Warm regards

  • Hi

          There is  one thing  im not sure. Can i use  the version of 3.4 opencv   .Or must  3.1 opencv version. Thank you advance.