This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Hi,
we found two modules on apps folder, one is mcal and other one is autosar_ipcin and autosar_ipcout, From our point of view these two modules used for exchanging the messages in between the cores is that Correct? According to the source code the mcal fits on ipu2(secondary) or ipu1_1 and autosar_ipcin & out fits on ipu1_0 (primary).
Kindly correct us if we are wrong at the assumption.
Thanks
Prakash
Hi Prakash,
can you check this Application Note and see if it clarifies your questions about MCAL/AutoSAR integration:
Regards,
Yordan
Hi Yordan,
Thanks for the application note, it was really helpful. At this moment we don't have idea to integrate the autosar stack and we planned to write some software on ipu1_1 in tda3x. So we need to send some custom messages inbetween the cores ipu1_0 to ipu1_1 and ipu1_1 to ipu1_0. Our questions can we reuse the autosar & mcal modules according to our needs?
if possible can you explain in short about these two modules (autosar ipc & mcal)? if there is any document Kindly point us.
Thanks
Prakash M
Hi Prakash,
can you check if you can use IPCLib for your usecase, please refer vision_sdk\docs\FeatureSpecificUserGuides\AppNote_IpcLib.pdf
Regards,
Yordan
Hi Yordan,
If we understood correct, the autosar IPC are implemented on top of IPClib modules. we seen some ipclib api are present in autosar modules.
Regards
Prakash
Hi Prakash,
TI provides IPC as an CDD MCAL and this can inter-operate with IPCLib of PDK/VisionSDK. With autosar_ipcin/ autosar_ipcout links on VisionSDK allows one to establish a communication channel between core hosting AUTOSAR and core hosting VisionSDK.
In the usecase vip_single_cam_view_autosar_app an message would be sent from IPU 1 0 (hosting VisionSDK) to IPU 2 0 hosting MCAL demo application.
Regards, Sujith