This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Dear TI officer:
I have a TDA2x development board and an OPT8241-CDK-EVM.
Can I put the OPT8241-CDK-EVM 's SDK: Voxel SDK on the TDA2 development board compiler and execute the OPT8241 application?
Thanks.
Hi Finley,
I am not too familiar with the Voxel SDK. I believe if this is C code and library which can be compiled for the cores on TDA2 SoC and have no dependency on any specific OS functions which is not provided as part of TI RTOS, it should be okay.
Thanks and Regards,
Piyali
Dear Piyali:
Thank you for your response
Voxel SDK dependency on PCL-1.7.2, libusb-1.0-0-dev, libudev-dev, linux-libc-dev, G++ 4.8 or later
on Ubuntu 14.04
Can it compile and run on TDA2 Linux ?
Thanks
Hi Finley,
I had tried running the PCL a long time back on the Linux on TDA2 and it was working fine. I believe you need to make sure your filesystem has the right libraries to support this. I will also let one of our Linux experts to have a look at your requirements to confirm this is indeed supported.
Thanks and Regards,
Piyali
Hi Finley,
The latest Linux SDK release, that can be used with TDA2, is 5.00.
This has support for point-cloud-dev and all other libraries that you mentioned. Please try it out and see if you can get the Voxel SDK working.
If not, we will have to look at the issues and see how we can enable you from there.
Regards
Karthik
Dear Piyali and Karthik,
Thank you for your response,
i will try OPT8241 on TDA2x.
thanks