Tool/software: Linux
Hello:
Background
We'are working on VisionSDK 3.05, for the QT environment we copy from PSDKLA 3.4.3 which the QT version is 5.6.
To support the full-screen and position control on QT application, we should select the ivi-shell in weston which require the QT version is newer than 5.7
we saw the PSDKLA 5.00 support the QT 5.9
PSDKLA 5.00
http://processors.wiki.ti.com/index.php?title=Processor_SDK_Linux_Automotive_Release_Notes
Component | Version |
---|---|
Linux Kernel | 4.14.79+ (2018 LTS) |
U-Boot | 2018.01+ |
Yocto Project | 2.4 (Rocko) |
Linaro Toolchain (gcc) | 7.2.1 hard-float |
Qt | 5.9.7 |
Wayland | 2.0 |
GStreamer | 1.12 |
PSDKLA 3.04
processors.wiki.ti.com/index.php
Component | Version |
---|---|
Linux Kernel | 4.4.84+ (2016 LTS) |
U-Boot | 2016.11+ |
Yocto Project | 2.1 (Krogoth) |
Linaro Toolchain (gcc) | 5.3 2016.02 hard-float |
Qt | 5.6 |
Wayland | 1.9 |
GStreamer | 1.6 |
Question
- Can we directly copy the QT library from PSDLA 5.0 to VisionSDK 3.5
- If not, how can we upgrade QT on visionsdk to 5.9.7?
Thanks.