Part Number: AM5718
Tool/software: Linux
Hi everyone,
I'm facing the same problem as this post said,
It can boot from SD card normally, the sf command works ok.
BUT after burn the MLO and u-boot.bin to the QSPI Flash, it cann't go to u-boot stage.
The error message is same as the post, I don't know how to fix this issue.
Anyone can give me some help?
Thanks very much!
DRA722-GP ES2.0
Trying to boot from SPI
Invalid bus 0 (err=-19)
Failed to initialize SPI flash at 0:0 (error -19)
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###