Greetings,
While following the traces between the DM355 and the DDR memory on my evalulation kit, I realized that the trace connecting DDR_DQGATE0 and DDR_DQGATE1 has does back and forth multiple times. However, on pages 3 and 4 in SPRAAR3 Application report, it mentions that is should be routed like the data lines and back. Can someone explain this please? And why is the distance between the DM355 and DDR is what it is and not as close as possible on par to what is recommended? I would have placed them much closer together, but I am not an expert so I may be missing a thing or two. Any clarification is greatly appreciated.
Thank you,
A