Other Parts Discussed in Thread: AM5718
Hi TI:
Some of our AM5718 main boards can't power up sometimes.
It will block on "start kernel".
MLO I/O re-calibration failed too.
Can you help to analyze root cause?
Thanks
Fail Log:
U-Boot SPL 2017.01-gf8adbe225f (Aug 28 2019 - 00:07:55)
DRA722-GP ES2.0
IODELAY: Isolation of Device IOs failed
Trying to boot from MMC2
U-Boot 2017.01-gf8adbe225f (Aug 28 2019 - 00:07:55 +0000)
CPU : DRA722-GP ES2.0
Model: TI AM572x EVM Rev A3
Board: RV700
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1, OMAP SD/MMC: 2
Writing to MMC(1)... done
Writing to redundant MMC(1)... done
Hit any key to stop autoboot: 0
MMC: no card present
switch to partitions #0, OK
mmc1(part 0) is current device
active partition:
1
==>Load Kernel
391736 bytes read in 43 ms (8.7 MiB/s)
SD/MMC found on device 1
** File not found boot.scr **
** File not found uEnv.txt **
3973576 bytes read in 109 ms (34.8 MiB/s)
101626 bytes read in 14 ms (6.9 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe4000, end 8ffffcf9 ... OK
Starting kernel ...
DarkHou