Why does page 20 of the Gerber pdf for the DM6467T EVM (aka Spectrum Digital HD1080P) specify the following controlled impedances?
Note 16: "Controlled Impedance of 50 ohms to be matched on all signal layers, on 5 mil lines." This does make some sense to me, but I've never had to specified controlled impedance before. Any insight?
Note 17: "5.1 mil traces on layer 12 to be 45 ohm, single ended and 90ohm differential." What are these signals and why are they special?
Note 18: "5.1 mil traces on layers 1 and 3 to be 50 ohm, single ended and 100 ohm differential". What are these signals and why are they special?
Most especially, why the specified difference here in Note 18 versus Note 17? I find DDR routing on all three of these layers but also on others. So Notes 17 and 18 must refer to either special DDR lines or something going elsewhere, like ATA (hard disk), PCI, or VLYNQ perhaps.
ref: http://support.spectrumdigital.com/boards/evmdm6467t/revc/files/Davincihd1080p_EVM_Gerber_revc.pdf
Thanks,
Helmut