This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have questions about SPI timing.
Our board has SPI interface between MCU domain of TDA4 and AP domain of TDA4. (MOSI : F25-->V25, MISO : W24-->F28, CS : F27-->W27, CLK : F26-->W29)
1) This interface's setup time(SPI_D valid before SPI_CLK active edge) is sholud be longer than 2.9ns according to datasheet(Table 5-75. Timing Requirements for SPI).
As I attached (1.spi-i-48mhz-cs-time, 2.spi-i-48mhz-mode0-fail, 3. spi-i-48mhz-mode2-ok), our interface can't meet the setup time when clk is 48MHz. (spi-i-48mhz-mode0-fail).
Surely, we can change the mode, and we can meet the setup time by setting mode2 (spi-i-48mhz-mode2-ok), 24MHz is also ok.
Q) Could we change the timing of MOSI or MISO?(ex. change some registers) Should it work normally at 48MHz?
2) Delay time (SPI_CSi active to SPI_CLK first edge, SPI_CLK last edge to SPI_CSi inactive) looks so long. (please see the spi-i-48mhz-cs-time)
Q) Is it normal?
Please give me a comment!
Thanks,
Manwoo Kim
Hi Manwoo Kim,
1. I don't know for a register for MOSI timing. The main issue here, I think, is that 48 MHz is the max frequency and this implies the PCB must be carefully designed .
2. I think this is is normal if SINGLE mode (one master, one slave) was chosen in software.
Also, didn't you consider use the internal connected MCSPIs? MCSPI4 has a permanent connection to MCU_MCSPI2 and MCSPI3 can optionally be muxed to MCU_MCSPI1 internally. Please refer to Figure 12-313. MCSPI Overview in TRM.
Regards,
Stan
Hi, Stan.
Thanks for your reply.
Does "Don't know for a register for MOSI timing" mean there is no register for MOSI/MISO timing?
Thanks,
Manwoo Kim
I've scrolled through MCSPI registers and PADCONF registers. I didn't find a setting to improve timing in MCSPI, but in the PADCONF registers for CLK and MOSI pins, you can try change the Drive Strength setting. I.e. bits 20:19 DRV_STR. I see it is 0x0 by default, so you can increase it gradually to see if any improvement. I don't know however if this will work in this case.
Regards,
Stan
Manwoo,
Have you taken the action proposed by Stan to check if drive strength affects setup time? Also, I noticed that in image 2, the setup time is measured from MISO=90%, but in image 2 it is measured from MISO=50%. Timings in the data sheet are based on 50% levels.
-Zack
Hi, Stan.
Thanks for your reply.
I will try to do your solution, and then notice you.
Thanks,
Manwoo Kim