This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: UART Boot Issue on custom board based on AM5728

Part Number: AM5728


Hi,

We have designed a custom board based on AM5728, 1GB DDR3L (Only 1 EMIF Interface used). P/N of DDR3 Used is MT41K512M16HA107:IT.

We are trying to boot through UART mode, as the board has provisions to boot only through

1. UART

2. mSATA

Steps followed:

1. sent u-boot-spl.bin file through debug UART3 port successfully. But received @VA!VA!VA! at the terminal. No "CCCC" seen on terminal. Can you please suggest why this behavior has been observed?

The Baud rate settings are 11.5kbps, No parity, No flow control.

2. Transfer of u-boot-file through Y-MODEM failed.

3. Configured DDR3L GEL files according to our custom board designed (file has been attached)EMIF_RegisterConfig_v1.xlsx, We aren't sure if the values that we have generated through the EMIF_Tool_Config is correct.

Please suggest us how to configure boot through UART and also configuration of DDR3L