This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: query for TDA4 camera feature

Part Number: TDA4VM

Hi TI,

I have several questions for TDA4.
please let me know about uncertainties.

1) The description of camera shows "One 4MP camera or eight 2MP camear streams" in page "CSI_RX_IF_feature".
what is the hz for this streams ? 1x 4MP @ 60hz and 8x 2MP @ 60hz ??

2) CSI 1.3+
I saw the expression "MIPI CSI2 v1.3+, mipi CSI2 v2.0".
what is the meaning of the "MIPI CSI2 v1.3+ (plus)", is this spec version ?

3) Dependency for same time RX x2 (*)
when I wanna use 4 Lane x2.5 Gbps (full bandwidth) on 2x input, (e.g> 3840x2160 @ 50hz x2)
can I use this feature except any dependency ? or do I just use the resolution, following the datasheet,
only support one 4M image or 8x 2MP images ?

Thanks,