This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I am doing my design based on AM437X_INDUTRIAL_EVM
I am copying and pasting the tracks between the MPU and the RAM.
But I have the following question:
In the AM437X_INDUTRIAL_EVM it has two RAM memories; my custom project has a single RAM, so:
When I copy and paste the tracks should I just remove the excess of the tracks connecting to the 2 RAMs or should I retune the tracks?
I have no doubts with my electrical scheme, my doubt is routing the RAM.
Thanks very much
Hi,
albgarc2014 said:When I copy and paste the tracks should I just remove the excess of the tracks connecting to the 2 RAMs or should I retune the tracks?
You might need to do both. Follow the guidelines in section 5.12.8.2.1 of the AM437x Datasheet Rev. E.