This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to connect a external ram to AM5718. When i check datasheet i saw, it supports DDR3-1333 (667 MHz) 2GB. But i want to connect DDR3L (800MHz) 2GB. So i see that, they work different clock frequency and i have question about this.
Can i connect it ? Does it work with AM5718?
Best regards.
Hi,
All DDR3 higher speed grades work at lower clock frequencies too. This is a JEDEC requirement.