This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir/Madam,
I am using TMS320C6678 along with DDR3 [4 Nos] i.e x64bit Data wide with 666MHz Operating. speed
I have PCB space constraints, So i may not be able to place the DDR3s in flyby topology as per "SPRABI1C"
So can i place these DDR3 in clamshell topology ?
PS: Anyways we shall carry out Signal Integrity analysis for the same.
Shekhar,
We very strongly recommend that you implement the SDRAM all on one side of the board and on the same side as the C6678. There are many benefits from this implementation regarding routing and via stub management. Even if you implement SDRAMs both top and bottom, they must appear electrically in a fly-by arrangement without any branching of the ADDR / CMD / CNTRL / CLK routes terminated to VTT. Customers that attempt SDRAM placement on both sides normally have significant stability issues and have to operate the DDR3 interface at a sub-optimal rate to obtain robust operation. Also note that simulation of via structures in high performance interfaces like DDR3 are very difficult and often do not correlate with actual signal integrity.
Tom
HI Tom,
Thank you for your feedback.
My one query is, why not Xilinx FPGA's and other NXP Processors do not restrict the usage of Clamshell topology for DDR3/DDR4.
ANd we have proven even Xilinx Zynq Ultrascale+ DDR4@1600Mbps with Clamshell topology
Why TI's processor have such restrictions ?
Shekhar,
I cannot explain how these other devices achieve this functionality. I speculate that these are newer devices that have additional functionality which either requires additional power consumption or are more expensive.
Tom