This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
While the figure of Synchronous Single "Read" for non-multiplexed mode is discribed, the figure of Synchronous Single "write" for non-multiplexed mode is not discribed.
We would like to read and write access to non-multiplexed device with "single" read/write mode.
Is this possible? Is there the access mode?
Thanks.
Hi,
Synchronous Single write is possible but the timing diagram was not included in the data manual. This is an error in the manual but you can use the read access as an example. The timing for the data valid from the falling edge is F15 in the table, similar to the burst mode.
Regards, Bill
Hi,
Thank you for your answer.
By the way, according to the Table 2-1. Device Memory Map in the TRM, address area of GPMC_0_DATA is described as 00 3000 0000 - 00 3FFF FFFF.
When we want to read/write data of the external NOR Flash memory which is connected to GPMC, ARM and DSP should access to this area (00 3000 0000 - 00 3FFF FFFF).
(The behavior of GPMC address bus pin is accordance with this address information accessed.)
Is this comprehension correct?
Thanks.
Hi,
That is correct but remember that the address range in question is addressing bytes. If you are using a 16bit NOR flash one less address bit would be represented outside the 66AK2G12.
Regards, Bill