Part Number: 66AK2G12
Hi,
I would like to know about GPMC for Synchronous Multiple (Burst) Read/write access.
I am supposed to use external Synchronous memory device.
As is the case of Figure 7-178. Synchronous Multiple (Burst) Read (GPMCFCLKDIVIDER = 1) in the TRM,
if GPMCFCLKDIVIDER = 1 and RDACCESSTIME >= 3 then,
it is impossible to select 16 words burst setting, isn't it?
Because WEOFFTIME, OEOFFTIME, CSRDOFFTIME and CSRDOFFTIME are up to 31 "GPMC_FCLK" cycles (not 31 "GPMC_CLK" cycles).
So, if GPMCFCLKDIVIDER = 1 then, I guess the number of "GPMC_CLK" cycle is up to 16 and it is impossible to select 16 words burst setting.
Is this correct?
Regards.