Part Number: AM3356
Hi Experts,
Customer is developing their system with AM3356BZCZA80(Linux SDK version:06_03_00_106)/TPS65910AA1RSLR. In their current system, Cortex-A8 is working at 600MHz/VDD_CORE=1.1V. Recently, their End-customer is requesting to reduce bootup/startup time. Therefore, customer is considering they would like to operate at 800HMz from powerup. After bootup/startup, customer is also considering that the operating clock frequency is changed to 600MHz dynamically, because of reducing power-consumption.
According to Datasheet " Table 5-7. VDD_MPU OPPs for ZCZ Package". If Cortex-A8 is operating at 800MHz, customer has to supply not "VDD_MPU = 1.1V" but "VDD_MPU = 1.26V". it means, it seems that customer needs to control PMIC.
Customer is asking if TI Linux SDK is supporting the above control(CPU speed/VDD_MPU voltage)? Is it possible to change CPU speed/VDD_MPU voltage dynamically? Can I have your Expert's advice/comments on this, please?
If there is any solution which reduces bootup/startup time, could you share it, please?
Best regards,
Miyazaki