This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What's the pin status( high impedance?) when power up for AM3354BZCZA100? I pull down 10k resistor at pin C16, but there is 0.9V at this pin when power up, this will make the NPN on when power on. it is so strange.
is anyone can help?
HI Nick
software is IAR.
when this happen, the initialization is not finished. when finished, the output is OK.
Jian, check the AM335x datasheet https://www.ti.com/lit/gpn/am3354 Table 4-1 for pin C16. It shows High-z during reset (Ball Reset State) and High-impedance with an active pull up after reset (Ball Reset Rel State). The internal pull resistor value can vary quite a bit depending on process, but rule of thumb is typically it is around 30K. You will need a stronger on board pull down to overcome this (<5K), or choose a different GPIO that doesn't have a pull enabled in Reset Rel State.
Regards,
James.
Hi,
I am using gpio2_21 pin as input in my am335x ZCZ package. In hardware i am getting the signal as 1 and 0
But using with this declaration in my dts and using system calls is getting always 0.
Please check the below declaration to read the gpio in am335x and suggest me.
declaration in DTS file:-
am33xx_pinmux: pinmux@44e10800 {
pinctrl-names = "default";
pinctrl-0 = <&mygpio1_pins_default>;
mygpio1_pins_default: mygpio1_pins_default {
pinctrl-single,pins = <
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* (M16) gmii1_rxd0.gpio2[21] */
>;
};
};
#gpio as Input gpio2_21 = 85
echo '85' > /sys/class/gpio/export
echo "in" > /sys/class/gpio/gpio85/direction
cat /sys/class/gpio/gpio85/value
please find the below circuit to read the input signal.
Regards,
lofna
Hi
First make sure the two resistors are solder well. For PIN M16, It shows "L" during reset (Ball Reset State) and "L" with an active pull down after reset (Ball Reset Rel State). you can try changing 10k to 4.7k. if this doesn't solve this, check your code again.
regards
wang jian