This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
After translation of the AM5728 ibis model, there are multiple models to choose from in the ibis file name in the SI model browser. How to choose the correct model?
[Pin] signal_name model_name R_pin L_pin C_pin
Y10 ATESTV NC
G19 DCAN1_RX Selector_10 0.142301 1.81835E-09 4.38728E-13
G20 DCAN1_TX Selector_10 0.137913 1.91785E-09 4.43391E-13
|*****************************************************************************************
| Usage I/O#1.8/3.3###BC1833DV40DCPBFBP1811_SSCEV.PAD
| Base model BC1833DV40DCPBFBP1811_SSCEV
|*****************************************************************************************
[Model Selector] Selector_10
Model_736 I/O,1.8V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40D_V_10P_!SC1_1P8
Model_737 I/O,1.8V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40D_V_10P_SC1_1P8
Model_738 I/O,1.8V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40D_V_5P_!SC1_1P8
Model_739 I/O,1.8V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40D_V_5P_SC1_1P8
Model_740 I/O,3.3V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40D_V_10P_!SC1_3P3
Model_741 I/O,3.3V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40D_V_10P_SC1_3P3
Model_742 I/O,3.3V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40D_V_5P_!SC1_3P3
Model_743 I/O,3.3V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40D_V_5P_SC1_3P3
Hi,
The models differ for slew rate, voltage tolerance, and IO voltage level.
If the IO voltage is 1.8V, then you should select one of the models 736-739. Use models 740-743 for IO voltage of 3.3V.
You should check the datasheet for voltage tolerance. Models 738,739,742,743 correspond to 5%. The others are 10%.
Lastly, models 736,738,740,742 correspond to fast slew rate. The others correspond to slow slew rate.
Thanks,
Kevin