Hello,
Recently I moved to SDK 7.1 and followed the instructions mentioned in the original question for changing UART2 to UART7 on SDK 7.1. However, I don't see any log on UART7. It works on SDK 7.0 but I couldn't make it work on SDK 7.1.
Some of the things I observed are.
Changing UART instance to "7U" doesn't make any difference. "make ethfw_all" doesn't compile this code. Whereas on SDK 7.0 making the same change does take effect.
#if defined(SOC_J7200) #define ENET_UTILS_MCU2_0_UART_INSTANCE (3U) #else #define ENET_UTILS_MCU2_0_UART_INSTANCE (7U) #endif
Also I added "TISCI_DEV_UART7" in this code with no luck.
void EnetBoard_initEthFw(void) { Board_initCfg boardCfg = 0U; Board_STATUS status; uint32_t i, moduleCnt, appFlags; uint32_t clkModuleId[] = { TISCI_DEV_DDR0, TISCI_DEV_TIMER12, TISCI_DEV_TIMER13, TISCI_DEV_UART7, };
Any help would be great here.
Thanks,
Satish